2025-12-05 6:13 AM
Hello,
Where can I view the commands sent and received from the ST67W611M1 using the SPI and UART? The datasheet doesn't provide this information. I couldn't find any other documents describing the command system on the ST67W611M1 page.
Solved! Go to Solution.
2025-12-05 6:21 AM
The list of commands, responses, etc. is available at ST67W611M1 AT Command - stm32mcu.
As a side note, the UART interface is not used for interaction with the module from the application - it is only used for firmware update, RF testing. I'd suggest exploring the Wiki pages in general, e.g. to learn more ST67W611M1 Hardware setup - stm32mcu.
2025-12-05 6:21 AM
The list of commands, responses, etc. is available at ST67W611M1 AT Command - stm32mcu.
As a side note, the UART interface is not used for interaction with the module from the application - it is only used for firmware update, RF testing. I'd suggest exploring the Wiki pages in general, e.g. to learn more ST67W611M1 Hardware setup - stm32mcu.