2022-09-30 9:01 AM
In the Data Sheet for the ST8034P the following is not clear about the ST8034PQR
Context is migrating a design from ST8034ATDT to ST8034PQR. The old design uses the fXTAL/2 functionality of table 13, with CLKDIV=1. ST8034P has no CLKDIV input. But it's untold if the behavior is that of CLKDIV=1 or CLKDIV=0.
A clue that fCLK = fCLKIN is that both have the same maximum frequency (26 MHz). But then, I wonder how the 45/55% duty cycle for CLK in table 8 is obtained without some slightly tighter duty cycle spec on CLKIN.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.