2019-03-04 9:19 PM
I found that I can make vendor model client with BluenrgMesh_SetRemoteData(), BluenrgMesh_ReadRemoteData() functions using BlueNRG embedded SDK.
However, these functions looks only for vendor models. Are there any APIs to make standard models client like Generic On/Off, Sensor models?
I mean for example I'd like to prepare Generic On/Off "Physical" Switch to control lighting which has Generic On/Off server model (Not iOS/Android APP).
2019-03-11 3:29 AM
KIndly look in this function BluenrgMesh_ModelsCommand()
You can see implementation of Generic_Publish()
Please use latest SDK V1.07 from the web. Thanks
Let us know if it helps
2019-03-12 7:12 PM
Hello, alok.
Thanks for your reply. I find new SDK V1.07 is released and I have checked the Generic_Publish(). That's what I need.
I noticed BluenrgMesh_SetRemoteData() is finally called in Generic_Publish(). I didn't know it can be used for all models. I also find Generic Level Client implementation in Appli_IntensityControlPublishing(). They're helpful.