2015-11-27 6:14 AM
Hi,
I got a problem while using STEVAL-IDB002V1 eval. kit. It is not entering into DFU mode if i follow the procedure as per the documentation (because led is not blinking). Thanks in advance. Regards , Ratheesh T2015-12-01 3:37 AM
Dear Customer,
The STM32L is preprogrammed with a DFU firmware that allows the downloading of a firmware image without the use of a programmer. If an user accidentally erases DFU firmware, he can reprogram it through STLink using the hex image DFU_Bootloader.hex available on DK SW package, firmware folder. Regards, GM2015-12-07 10:17 PM
Hi Marchese.Graziella,
I tried that by using STlink but it is also not working. I have attached the log window which shows some warning ________________ Attachments : dfu.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I19T&d=%2Fa%2F0X0000000bn9%2FAMh8S54cAc_PFwlp5NqQmIS_eciOdCffiDX0IrXPKpU&asPdf=false2015-12-09 10:18 PM
Hi,
Thank you... Problem Solved First i tried IAR compiler and ST link debugger for flashing DFU image file (not solved, that was my 2nd post) After that i tried ST link utility exe (downloader) and ST link debugger to flash DFU image it solved my issue . i.e now it can enter into DFU modeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.