cancel
Showing results for 
Search instead for 
Did you mean: 

Advertising stops after modifying the advertising data

RAdam.1
Associate III

Using a BlueNRG-LP

I am wanting the advertising packet to show the battery level and some other changing data - pretty normal for a BLE device. So I have it advertising normally and I call this function every 10 seconds. This however seems to just stop advertising altogether.

I have tried disabling advertising, changing it and re-enabling but that has the same effect. The data length doesnt change - just the contents

Any suggestions?

void BluetoothUpdateAdvertisement(uint8_t Role, uint8_t Battery)

{

tBleStatus ret;

if (APP_FLAG(SET_CONNECTABLE))

{

adv_data[AD_MFRDATA_STATUS] = Role;

adv_data[AD_MFRDATA_BATT] = Battery;

ret = aci_gap_set_advertising_data(0, ADV_COMPLETE_DATA, sizeof(adv_data), adv_data);

printf("Update advertising data %02X\n", ret); 

}

}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
paolonegrini9
Associate II

Did you solve the problem !?!?1

I'm facing with the same issue!!