cancel
Showing results for 
Search instead for 
Did you mean: 

About BlueNRG-1 pairing

Guo Rongbo
Associate
Posted on May 03, 2017 at 11:18

Hello,

        My question is about BlueNRG-1 .

I want to design a about bluetooth master and slave Fixed PIN pairing.

But the Fixed PIN seems to be no effect.

Specific how should do?Thanks !

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 05, 2017 at 10:02

Dear Customer,

as example you can see the scripts: Security_PassKeyEntry_Master_Role.py and Security_PassKeyEntry_Slave_Role.py, that you can find inside last installation package.

To use fixed pin, you have to modify lightly these scripts, for example in the  ACI_GAP_SET_AUTHENTICATION_REQUIREMENT command, you have to set the field Use_Fixed_Pin = 0x00 (fixed pin ) instead of 0x01 (requested pin).

Regards,