cancel
Showing results for 
Search instead for 
Did you mean: 

Inquiry About VL53L5CX Gesture Recognition Implementation on STM32N657

dw1
Associate III

Dear ST Support Team,

I hope this message finds you well.

I am currently working on a project where I aim to implement gesture recognition using the VL53L5CX sensor. However, I noticed in the official documentation that the supported cores for gesture recognition do not include the M55 (which is the core of my STM32N657 microcontroller).

Could you please advise if there are alternative methods to achieve gesture recognition with the VL53L5CX on this platform? For example:

  1. Are there any software libraries or algorithms compatible with the STM32N657 that I could utilize?

  2. Would it be possible to port the existing gesture recognition functionality to the M55 core?

  3. Are there other recommended approaches or workarounds to accomplish this?

I would greatly appreciate any guidance or resources you could provide to help me proceed with this implementation.

Thank you in advance for your time and support.

Best regards,
dw1

0 REPLIES 0