2018-11-27 3:55 AM
Hi guys, i'm working with the GNSS expansion board X-NUCLEO-GNSS1A1, plugged to STM32F411RE Nucleo board. I looked inside the X-Cube GNSS1 expansion software package, which provides also some ready-to-be-built examples. I've chosen the simpler one, "GetPos", and after building and running a serial terminal, i see from the menu that the "wakeupstatus" is always "0". I've tried to add some code that set the wakeup pin, but nothing changes.
I've used the following configuration of the jumper:
J2 open
J3 closed
J4 closed
J5 open
J6 closed
J7 open
J8 open
J9 closed
J10 open
J11 open
J12 open
J13 closed
J14 closed
J15 closed
Any suggestions?
2018-11-27 4:43 AM
Ciao Stefano
Wakeup signal can be routed on:
in your case J9 is ok.
In the Tese-LIV3F the wakeup signal (pin-5) is an Input-signal used to wakeup the module from Standby.
If you see the led D2, (the Red led) blinking, this means the module is already running and this could explain why the Wake-Up signal is doing nothing.
To test the wakeup you should move the module in standby (for example you can use the NMEA command: "$PSTMFORCESTANDBY,00010" which forces the module to sleep 10 seconds) and while the module is sleeping you can wakeup the module toggling the wakeup-pin.
Hope this helps.
Regards
Francesco
2018-11-27 7:01 AM
Ciao Francesco and Stefano,
In the Jumper configuration, J11 (SCL) and J12 (SDA) has to be closed.