2025-09-14 11:26 PM
Hello, I am using Teseo-LIV4F for some time. Do you also notice that the sat count drop from the start, i.e. from 27 sats down to ~18-19 over some time (~15 min)? It is reproducible here, a soft reset bring it up again and it goes down again over the next 15 mins.
2025-10-02 8:04 AM
Hi,
What you are observing is not normal behavior.
Can you please share a log ? This will give me a good sense of CN0 levels and the azimuth and elevation of satellites.
I am assuming you have enabled GPS, GAL and BD constellation.
Also, could you please let me know what are your testing conditions? If you can post a picture of your antenna placement and test conditions that would be helpful.
2025-10-09 11:33 PM - edited 2025-10-09 11:34 PM
@GalaxyQuest thanks for your reply. In general the satcount drop seems to be normal at the Teseo LIV4F because it startet with L1 only and then switch to L1 and L5 which result in a lower satcount because of the limitation in total available tracking channels of the receiver.