| Subject | Author | Posted | |
|---|---|---|---|
|
Hi, I’m planning to use the EVLSTGAP3SXS-H eval board for testing at around 40 A. The MOSFETs are ...
| 2025-05-13 9:12 AM | ||
|
We are trying to build 30W PFC circuit using L6562 in fixed off time(FOT) mode ref AN1792 in this c...
| 2025-05-12 2:46 AM | ||
|
Here is my hardware design.
The output with load goes high during chip reset. When I cancel the r...
| 2025-05-05 8:00 PM | ||
|
Hello. I have a problem with this IC. I can read cell voltages perfectly. but when I initiate cell...
| 2025-05-05 5:37 AM | ||
|
Dear All, I have created a new schematic for a project I am working on, using the POE Dual Active ...
| 2025-04-24 7:25 AM | ||
|
Hi, We have designed PFC using L6562 referring application note AN2761 on that the auxiliary windi...
| 2025-04-22 5:50 AM | ||
|
Hi. I am using the L6599AD without PFC. Previously, the DIS pin was connected to the DELAY pin...
| 2025-03-26 3:45 PM | ||
|
Hello, I have developed a custom board using the STPM33 to measure power consumption. The schemati...
| 2025-03-25 3:21 PM | ||
|
What is the difference between Thermal Suddown and Thermal Rest?
| 2025-03-11 4:49 PM | ||
|
Hello ST Team and Community, I am currently testing the IGBT STGP10M65DF2 in PSpice to verify the ...
| 2025-03-11 4:01 AM | ||
|
Hello Everyone, I am working on T-type PFC and I refer STSW-PFCBIDIR. May I know the reference ...
| 2025-03-10 8:53 PM | ||
|
hello comunity, i want design a motor controller with the stspin32g4. i have a question about the...
| 2025-02-27 3:51 AM | ||
|
Hello, I whant to build a 3 phase meter from the EVALSTPM-3PHISO. The Data that is computed sho...
| 2025-02-26 5:22 AM | ||
|
Does the VN5T016AH-E handle short circuits with extremely low inductance/resistance without damage ...
| 2025-02-25 9:37 PM | ||
|
Hello all, I am writing to inquire about a DC motor driver solution suitable for our applicatio...
| 2025-02-25 7:42 AM | ||
|
I believe the VCX comparator is designed to clamp the maximum primary current, but there is no equa...
| 2025-02-24 1:37 AM | ||
|
Currently we use a PowerStep01 in StepClock configuration the current controller (CM_VM Bit set)....
| 2025-02-19 7:12 AM | ||
|
Dear Madam/Sir, We are using powerStep01 and must implement motor "hardstop" purely in hardware (n...
| 2025-02-13 10:25 PM | ||
|
Hi, I’m seeking advice on selecting the appropriate battery monitoring IC for a project involving ...
| 2025-02-09 10:38 PM | ||
|
Hi,
not sure if this is the right section, but:
I have been given an AET-MOT-2DC70S1 motor cont...
| 2025-02-03 7:49 AM |