| Subject | Author | Posted | |
|---|---|---|---|
|
I am trying to set-up power management for a USB charging point using an STUSB4710 (i.e. dropping t...
| 2024-02-16 11:55 AM | ||
|
Hello, I'm developing a project on a NUCLEO WL55JC1 board. I require Bluetooth communication betwee...
| 2024-02-15 9:23 AM | ||
|
1.Is there a Demo board for STOTG04? If so where can I procure it? 2.It is given in the datasheet ...
| 2024-02-02 8:56 PM | ||
|
Hi, I ask for the following issue. I am testing the STEVAL-IDB008V1 board, the BLE RemoteControl ...
| 2024-02-02 12:52 PM | ||
|
Hello, i used the CubeMX to generate the example code for the X-Nucleo-BNRG2A1 board. The Example w...
| 2024-02-02 10:38 AM | ||
|
Hi, We are looking for a Bluetooth module that support Classic audio in Hands Free Profile Audio G...
| 2024-01-31 6:40 AM | ||
|
I have STEVAL-CCC002V1 with STUSB1600A controled with STM32F103 over I2C. Samsung Galaxy Tab connec...
| 2024-01-31 3:55 AM | ||
|
Mode 2 Can read and write sensor data directly through the psi5 operation register?
| 2024-01-29 5:24 PM | ||
|
I'm searching for detailed information on the Serial Peripheral Interface (SPI) protocol used by th...
| 2024-01-29 1:07 AM | ||
|
Can Mode 2 of the L9663 read the sensor data directly with the MCU? Or do we go through SPI?
| 2024-01-28 6:42 PM | ||
|
I am using the blue-nrg-lps,but when i test the hid example project , it cannot work in win11,but i...
| 2024-01-26 5:26 PM | ||
|
Hello All, I am new to Bluetooth and would like to use the BlueNRG M2 as a hosted network co-proce...
| 2024-01-23 7:14 AM | ||
|
Hi. We are trying to measure analog values using BlueNRG-2. We want to calculate the accuracy, bu...
| 2024-01-19 10:29 PM | ||
|
Hi ST Community, I use the X-CUBE-BLE1 library and the SensorApp application, and I can understand...
| 2024-01-18 11:15 AM | ||
|
I am programming stm32411CeU Blackpill- i want to make connection between the Stm32 and Pc Vi...
| 2024-01-10 6:41 AM | ||
|
Hi, I'm new with this development board. My target is to use the S2-LP DK Application to configure...
| 2024-01-10 4:59 AM | ||
|
Where can I get the detailed technical manual of STSAFE-VJ100-CCC, such as the definition of chip p...
| 2024-01-10 12:22 AM |