| Subject | Author | Posted | |
|---|---|---|---|
|
I have an X-Nucleo-67W61M1 with a Nucleo-WB55RG host board. I was following this link for how to do...
| 2026-01-15 2:56 AM | ||
|
Hello ST Community, I am working with NUCLEO-WBA55CG and encountering a startup issue when using t...
| 2026-01-13 10:21 PM | ||
|
FUS and BLE update. I would like to know if it is possible to update FUS (1.2.0)(2.1.0) and BLE (1...
| 2026-01-13 5:35 AM | ||
|
This https://blog.st.com/stm32wl5x-stm32wl5m/ seems to suggest that the wireless module could be ei...
| 2026-01-12 4:39 PM | ||
|
Hello. I got my hands on a wba55cg nucleo board and i'm currently studying about ble. I want to ...
| 2026-01-12 3:33 AM | ||
|
I am using LPTIM for pulse counting in ultra low power (stop 2) mode for STM32wl55jc. Now, the prob...
| 2026-01-12 1:23 AM | ||
|
On a custom board, I would like to use the BlueNRG GUI (v.4.7.1) to run the tests described in AN48...
| 2026-01-09 7:58 AM | ||
|
Hello ST Community, I am currently designing a board based on the STM32WL55 and I am aiming to opt...
| 2026-01-08 6:55 AM | ||
|
Hello ST Community,
I am working with the NUCLEO-WL55JC1 and the official Sigfox_PushButton examp...
| 2026-01-06 1:01 PM | ||
|
I want to measure current draw on a Nucleo-WBA65RI board using a Nordic PPK2 power profiler. I put ...
| 2026-01-04 3:11 AM | ||
|
le_advertising_event = (hci_le_advertising_report_event_rp0 *) p_meta_evt->data; int8_t rssiValue ...
| 2025-12-30 8:31 AM | ||
|
Hello, I’m working with STM32WB55CGU (UQFN68) on a WeAct WB55 board and trying to achieve ultra-lo...
| 2025-12-29 10:44 AM | ||
|
I have a stable BLE application on STM32WB55RG. The application uses a Custom Template, has one ser...
| 2025-12-23 4:48 AM | ||
|
Hi there, i am planning to create a "smart light" (on/off) which is compatible with philips hue wi...
| 2025-12-22 7:15 AM | ||
|
Dear Community Members, I am trying to control / communicate-with X-NUCLEO-BNRG2A1 via NUCLEO-STM3...
| 2025-12-21 8:39 PM | ||
|
Hello, I am setting up a P-NUCLEO-LRWAN3 kit and experiencing issues with serial communication to ...
| 2025-12-21 7:12 AM | ||
|
Dear ST Community Members, I bought X-NUCLEO-BNRG2A1 (497-X-NUCLEO-BNRG2A1-ND) and X-NUCLEO-67W61M...
| 2025-12-19 10:38 PM | ||
|
Hi, I need help with latest X-NUCLEO-BNRG2A1 board firmware/software. The schematic available on ...
| 2025-12-17 10:49 PM | ||
|
Hi , we are using LORA , 22 dBm , 3.3V system , TX and RX path are connected via RF SWITCH on Boar...
| 2025-12-16 9:08 PM | ||
|
The parameters for the AT+TCONF are shown differently in your example to where you show the breakd...
| 2025-12-15 11:53 PM |