cancel
Showing results for 
Search instead for 
Did you mean: 

Toolchain not detected by Cube AI studio v1.2

stm-trt
Associate

Hello,

I am trying to create a project with Cube AI studio v1.2.

My toolchain and libraries are well detected with Cube AI studio v1.1, and I can create a project.

However, it is not the case for the Cube AI studio v1.2. The toolchain paths seem valid, but when creating a project no IDE is proposed at all, as shown in the attached image.

 

Could you help me please ? No debug logs are generated.

 

Versions :

  • Cube AI studio : 1.2
  • CubeMX : 6.17
  • CubeIDE: 2.1.1
  • CubeProgrammer : 2.22.0
  • EdgeAICore : 4.0

 

1 ACCEPTED SOLUTION

Accepted Solutions
stm-trt
Associate

Thank you for your response.

 

Updating proxy settings on each involved application has actually solved my problem.

I guess it couldn't download any updates, hence this bug. It has also solved the unwritten log files bug.

 

I have added the versions of each tools in the initial post, just if needed for the other users.

 

Thank you very much for your help !

 

 

View solution in original post

2 REPLIES 2
hamitiya
ST Employee

Hello @stm-trt ,

Could you share what are the dependencies version you have for 

- STM32CubeIDE

- STM32CubeMX

You also mentioning that  you don't have any logs. Does it mean that the folder C:\Users\<username>\.stm32cubeaistudio\logs is empty ?

If yes, could you check that all instances of STM32Cube AI Studio are killed in the Task Manager and the folder .stm32cubeaistudio is writable ? 

 

 

Best regards,

Yanis


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
stm-trt
Associate

Thank you for your response.

 

Updating proxy settings on each involved application has actually solved my problem.

I guess it couldn't download any updates, hence this bug. It has also solved the unwritten log files bug.

 

I have added the versions of each tools in the initial post, just if needed for the other users.

 

Thank you very much for your help !