2019-01-05 6:42 PM
I tried Cube AI like youtube https://youtu.be/grgNXdkmzzQ. But I got some difficulties.
I use Cube MX 5.0.1,Cube AI 3.3.0.
1. Invalid Network Error
In mcu selection, I selected Github Model file and pushed analyze button in the funtion item. Then I got Invalid network error and difficult to analyze the model.
In the youtube, here : https://youtu.be/grgNXdkmzzQ?t=217
2. Unable check AI in the Pinout & Configuration Setting
I selected F7 MCU. But the item of Artificial intelligence doesn’t appear in the Application software. I tried to display the item by checking AI in the additional software. But the item doesn’t appear in the Application.
In the youtube, here : https://youtu.be/grgNXdkmzzQ?t=316
Anyone has solutions?
Thank you.
2019-01-07 5:26 AM
Hi,
Could you provide us the complete output log and the CubeMX log while reproducing the error ?
(CubeMX log is located at: C:\Users\[username]\.stm32cubemx\STM32CubeMX.log)
Thank you
2019-01-07 8:32 AM
I get the same error when I try and analyse the HAR-CNN-Keras Model from Github: This is the relevant snippet from the STM32CubeMX.Log file:
2019-01-07 16:23:57,845 [INFO] McuExtendedFiltersManager:82 - Reset MCU extended filter: Artificial Intelligence
2019-01-07 16:24:12,555 [ERROR] AIPython:88 - Error: no directory found: C:/Users/another/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/3.3.0/Utilities/windows
2019-01-07 16:24:12,555 [INFO] AIPython:100 - Command: C:/Users/another/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/3.3.0/Utilities/windows/generatecode --auto -c C:/Users/another/AppData/Local/Temp/mxAI11374476597176510148740718862498/config.ai
2019-01-07 16:24:12,565 [INFO] AIPython:153 - Exception in python generation: java.io.IOException: Cannot run program "C:/Users/another/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/3.3.0/Utilities/windows/generatecode" (in directory "C:\Users\another\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\3.3.0\Utilities\windows"): CreateProcess error=2, The system cannot find the file specifiedThe console in STM32CubeMX shows:
Command: Command: C:/Users/another/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/3.3.0/Utilities/windows/generatecode --auto -c C:/Users/another/AppData/Local/Temp/mxAI11374476597176510148740718862498/config.ai
 Invalid networkThe following path has no files or directories present:
C:\Users\another\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\3.3.0The parent directory includes the 3.3.0 folder and what looks like an extraction of the the install pack in a TMPUPD folder.
Hope this figures out what the problem is..
Jonathan
2019-01-07 8:43 AM
Copying the contents of :
C:\Users\another\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\TMPUPD_7987620512652994028\Utilities
To:
C:\Users\te192188\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\3.3.0\Utilities
Seems to resolve the problem running analyse. It looks like the installer hasn't worked correctly.
2019-01-07 9:18 AM
I also don't see the "Additional Software" option on the LHS after enabling the AI Application and AI Core settings. From these messages in the log I guess other parts of the install also failed:
2019-01-07 17:13:51,330 [INFO] UITreeTableRework:854 - In
2019-01-07 17:13:51,337 [ERROR] Mcu:515 - ThirdParty IPModes/IPconfigs doesn't exist for :C:/Users/another/.stm32cubemx/plugins/thirdparty/db//STMicroelectronics/X-CUBE-AI/3.3.0/STMicroelectronics.X-CUBE-AI.3.3.0_Modes.xml
2019-01-07 17:14:50,608 [INFO] UITreeTableRework:854 - In
2019-01-07 17:14:50,608 [ERROR] Mcu:515 - ThirdParty IPModes/IPconfigs doesn't exist for :C:/Users/another/.stm32cubemx/plugins/thirdparty/db//STMicroelectronics/X-CUBE-AI/3.3.0/STMicroelectronics.X-CUBE-AI.3.3.0_Modes.xml2019-01-08 2:01 AM
There are effectively problems during the installation, try deleting X-Cube-AI from CubeMX, then go to "C:\Users\[username]\STM32Cube\Repository\Packs\STMicroelectronics" and check that X-Cube-AI is no more present (delete it if present). Be sure that no process is using the directory and try re-installing the X-Cube-AI from CubeMX
Additionally what you can try is a manual installation by downloading the plugin here (bottom of the page) : https://www.st.com/en/embedded-software/x-cube-ai.html
Then go to Help > Embedded Software Packages Manager and click on "From Local" to browse the file you just get
Hope this can help
2019-01-08 5:38 AM
Thank you.
CubeMX log is here.
2019-01-07 22:29:32,388 [ERROR] AIPython:88 - Error: no directory found: C:/Users/***/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/3.3.0/Utilities/windows
 
2019-01-07 22:29:32,407 [INFO] AIPython:100 - Command: C:/Users/***/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/3.3.0/Utilities/windows/generatecode --auto -c C:/Users/***/AppData/Local/Temp/mxAI21338039797414705533947946921371644/config.ai
 
2019-01-07 22:29:32,431 [INFO] AIPython:153 - Exception in python generation: java.io.IOException: Cannot run program "C:/Users/***/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/3.3.0/Utilities/windows/generatecode" (in directory "C:\Users\***\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\3.3.0\Utilities\windows"): CreateProcess error=2, cannot find files.
 
2019-01-07 22:29:32,663 [INFO] New_gui_TipPanel:170 - scale :0.21235194585448391
 
2019-01-07 22:29:36,157 [INFO] ApiDb:186 - Save user favorites file C:\Users\***/.stm32cubemx/favorites.mcus.txt: 0 item(s)
 
2019-01-07 22:29:36,159 [INFO] ApiDb:191 - User favorites MCUs=[]
 
2019-01-07 22:29:36,165 [INFO] ApiDb:186 - Save user favorites file C:\Users\***/.stm32cubemx/favorites.boards.txt: 0 item(s)
 
2019-01-07 22:29:36,166 [INFO] ApiDb:191 - User favorites Boards=[]From the log, the probrem may be the instalation fail of the ai pack.
The dedicated folder doesn't exit and I reinstalled it again.
But I got the error again.
Finally, I succeeded the execution.
The solution is deleting X-Cube-AI folder completely and reinstalling it again.
Thank you.
2019-02-25 3:55 PM
Also seeing the same error shown in the CubeMX dialog, but have a different log remark:
[INFO] AIPython:108 - INVALID MODEL: Model saved with Keras 2.2.4-tf but <= 2.2.4 is supported
It appears the latest Keras version appends "tf" unfortunately, and the code may not handle that properly?
2019-02-26 5:44 AM
You are right for this problem, in the next version of the pack this problem will be fixed
2019-10-17 5:18 AM
Hi everyone, i am having a similar issue , i get a invalid network error window once i start to analyze. Please find below the log:
2019-10-17 17:35:39,958 [INFO] AIPython:126 - Command used: C:/Users/Preeti/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/3.4.0/Utilities/windows/generatecode --auto -c C:/Users/Preeti/AppData/Local/Temp/mxAI117732111163906505095478914033096/config.ai
2019-10-17 17:35:39,974 [INFO] AIPython:196 - Exception in python generation: java.io.IOException: Cannot run program "C:/Users/Preeti/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/3.4.0/Utilities/windows/generatecode" (in directory "C:\Users\Preeti\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\3.4.0\Utilities\windows"): CreateProcess error=216, This version of %1 is not compatible with the version of Windows you're running. Check your computer's system information to see whether you need a x86 (32-bit) or x64 (64-bit) version of the program, and then contact the software publisher