2020-03-17 5:52 AM
Hello,
I created a CNN model used Keras with tensorflow
here's the model
model = models.Sequential()
model.add(layers.Conv2D(32, (3, 3), activation='relu', input_shape=(32, 32,1)))
model.add(layers.MaxPooling2D((2, 2)))
model.add(layers.Conv2D(64, (3, 3), activation='relu'))
model.add(layers.MaxPooling2D((2, 2)))
model.add(layers.Conv2D(64, (3, 3), activation='relu'))
model.add(layers.Flatten())
model.add(layers.Dense(32, activation='relu'))
model.add(layers.Dense(4))when I test the model on Python using model.evaluate()
I get the following results
loss: 0.0086 - accuracy: 0.9955
but when I test on STM32 , using the code creaded from CUBE-MX-AI :
I get always result of negative value from -15 to -23 for the 1st output and 0's for the last three outputs.
after commented the code of randomizing the input data in MX_X_CUBE_AI_Process()
the result is some negative value for 1st output and 0's for the last three outputs.
I can't understand why I didn't get the same result as testing on python .