2025-11-17 8:11 AM
Hi,
I have build a custom model based on st yolox model.
This model have an input of 480x480. Intput int8 and output float.
Five classes for vehicles detection
Quantized and tested on stm32N6570-DK.
Now i'm trying to add my model on this st example
https://github.com/STMicroelectronics/STM32N6-GettingStarted-ObjectDetection/tree/main
I'm following this tutorial to deploy my model
https://github.com/STMicroelectronics/STM32N6-GettingStarted-ObjectDetection/blob/main/README.md#application-build-and-run---dev-mode
I'm using stm32cubdeIDE to program the card
After i programmed the network_data.hex, i'm trying to deploy and debug the application.
But i have this error at this step : app_postprocess_init
The parameters
Do you have en idea how i can resolve this ?
2025-12-12 6:36 AM
@mls, yes I think, except if I did a mistake...
Your model are best_model_PerChannel_quant_int8_float32_random_1 and best_model_PerChannel_quant_int8_int8_random_1 correct?
Could you try to clone the repository again to make sure we are aligned?
Have a good day,
Julian