2018-08-19 8:45 PM
SPC5 Studio for SPC560D-DIS board, LINFLEX0 configured as UART, Tx is okay but Rx ISR is not getting called. I am using the auto generated Serial Test application which creates IRQ handlers in "spc5_linflex.c". I have break points set in both Tx and Rx IRQ handlers, only Tx IRQ gets hit. I can see the RX data coming into BDRM buffer and UARTSR DRF (data receive flag) is also set. Please help.
2018-08-29 1:47 AM
Hello,
are you using spc5studio 5.8.1?
If not please update your version of SPC5Studio to 5.8.1 and let us know if the problem still exist.
Regards