2014-05-23 10:21 AM
Can anybody offer any knowledge of using STANDBY mode?
I am putting the chip in STANDBY and it appears to go there, as the processor goes dormant until I cause a wakeup event. But the current draw on the VDD_LV power-input (2.1v) is ridiculously high (~100ma). I've confirmed that the power is not going out the ports - those are all ok - it appears to be going to core/peripherals (hence VDD_LV). Following the spec carefully, with weeks of scrutiny and experimentation. Can give more details if anybody has experience here... tnx, -mark #powerconsumption-power-standbySolved! Go to Solution.
2014-05-27 1:58 AM
Hello Mark ,
sorry for our late answer.you can check in the chapter : (cf reference manual of SPC564B70 (Bolero))Table 88. Low-Power Peripheral Configuration Registers (ME_LP_PC0…7) Field DescriptionsPeripheral control during STANDBY0 Peripheral is frozen with clock gated1 Peripheral is activeAnd your peripheral control registers are maybe badly configured. Best regards Erwan YVIN2014-05-27 1:58 AM
Hello Mark ,
sorry for our late answer.you can check in the chapter : (cf reference manual of SPC564B70 (Bolero))Table 88. Low-Power Peripheral Configuration Registers (ME_LP_PC0…7) Field DescriptionsPeripheral control during STANDBY0 Peripheral is frozen with clock gated1 Peripheral is activeAnd your peripheral control registers are maybe badly configured. Best regards Erwan YVIN