2019-05-29 2:09 AM
Hello
Is there any specific reason behind putting this delay, if yes than what it is?
I want to manage time in my application so i tried to reduce the delay but in that case I am not able to transmit data properly.
below is the given function
sd_lld_write(&SD1,CMD2,(uint16_t)(sizeof(CMD2)/sizeof(CMD2[0])));
osalThreadDelayMilliseconds(200);
Solved! Go to Solution.
2019-06-28 5:34 AM
Hello rewatee ,
it is better to use the Runtime IO component in SPC5Studio
Best Regards
Erwan
2019-06-28 5:34 AM
Hello rewatee ,
it is better to use the Runtime IO component in SPC5Studio
Best Regards
Erwan
2019-07-16 5:19 AM
Hello Erwan
I am facing same problem with the Runtime IO component as well. I have set the configuration parameter in Runtime io environment.
I am using "function ioWrite(int fd, const void *buf, size_t count)" for data transmission.
can you please provide some sample code?
Regards
Rewatee