2019-07-17 5:29 AM
Is it possible to compile the application only with Gcc (free) so do not use GHS or Hightec and flash and run the compiled code?
I can tolerate that this compiler is not efficient as those not free.
Solved! Go to Solution.
2019-07-17 6:50 AM
Yes , it is possible for you to use gcc (free) for SPC5 Family
The compiler is available on the update site (SPC5Studio Update site)
http://spc5tools.spc5studio.com
you should download from SPC5Studio Tools suite
Best regards
Erwan
2019-07-17 6:50 AM
Yes , it is possible for you to use gcc (free) for SPC5 Family
The compiler is available on the update site (SPC5Studio Update site)
http://spc5tools.spc5studio.com
you should download from SPC5Studio Tools suite
Best regards
Erwan