2017-02-08 5:18 AM
Hello,
I am trying to use C++ in the SPC560Bxx mcu using SPC5 Studio and the free gcc vle toolchain (4.9.2).
However, it looks like constructors aren't called as I expected.
In the following example, I expect to end up in the first case of the if statement, but I end up in the else case.
class Foo {
public:
int val;
Foo() {
val = 42;
}
void do_something() {
if (val == 42) {
printf('I expect to end up here');
} else {
printf('But I end up here');
}
}
};
static Foo myObject; // this ought to call the Foo's constructor
int main(void) {
...
myObject.do_something();�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
...
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
From what I understand this is because the crt0.s doesn'tinitialize the static objects on startup.
Does anyone have a solution to my problem or aworking c++ example they can share?
#spc560b54l5 #c++11 #c++ #gcc2017-02-09 11:08 PM
To answer my own question, I found out that if I left the .ctors section during linking and then called each constructor, my problem seems to be solved.
I had to add the following in the ld-script:
/* .ctors are used for c++ constructors */
.ctors :
{
PROVIDE(__ctors_start__ = .);
KEEP(*(SORT(.ctors.*)))
KEEP(*(.ctors))
PROVIDE(__ctors_end__ = .);
} >flash
�?�?�?�?�?�?�?�?
and then using the following __late_init function, which is called before main():
void __late_init() {
extern void (*__ctors_start__[])(void) __attribute__((weak));
extern void (*__ctors_end__[])(void) __attribute__((weak));
int count = __ctors_end__ - __ctors_start__;
int i;
for (i = 0; i < count; i++) {
__ctors_start__[i]();
}
}
�?�?�?�?�?�?�?�?�?�?
Note that this only solves the construction of global objects.
2017-02-10 1:40 AM
Hello Gustav ,
I have tried yesterday to port a C Test Application on C++ Test Application in SPC5Studio
SPC560Dxx OS-Less Test Application for Discovery
Compilation is ok but i have a coredump on clock init.
i had forgotten to update my linker file.
Anyway, i will reactive a change request to create a C++ Test Application from SPC5Studio.
I will take some time.
Do not hesitate to contribute on this subject on
Best regards
Erwan