cancel
Showing results for 
Search instead for 
Did you mean: 

Can i use 1CH. audio out with stereo provision IC ?

panneerrajan_g
Associate II
Posted on December 15, 2015 at 07:57

Hi,

Can i use single output only with stereo output provision?

for eg:

TDA7297 is 2+15W stereo IC,  But i want single (mono) out only with 15W,

Can i use single channel only?

reaming channel should connect or make it floating /open?

if open means, Its create any problem. Pls suggest me
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Nickname1623_O
Associate II
Posted on December 15, 2015 at 08:23

hi Panneerr,

of course , you can just use one amplifier of stereo amplifier .

and you should connected non-used channel input coupling cap to ground  to avoid resonance .

by the way , due to non-used channel are in active status , so power dissipation will higher than mono amplifier IC .

Thanks ,

YT

panneerrajan_g
Associate II
Posted on December 17, 2015 at 07:02

Hi Yun Tao,

Thank you,

Coupling capacitor require any specified value for unused input channel connect to ground.

can i connect 0.1uF 25V ceramic disc capacitor?

Pls. suggest