2015-04-21 8:23 AM
Hello,
I want to save between 1 and 5 noises or sounds as reference, whenever;Nr1 noise is played (source can be input of speakers) the relay needs to be switched 1 timeNr2 noise is played (source can be input of speakers) the relay needs to be switched 2 timesNr3 noise is played (source can be input of speakers) the relay needs to be switched 3 timesNr4 noise is played (source can be input of speakers) the relay needs to be switched 4 timesNr5 noise is played (source can be input of speakers) the relay needs to be switched 5 timesI dont want to use microphone as transduser because the enviroment is very noisy. I need to gather the analogue sound signal from the inputs of the speakers.I cannot use PC or OS based programs.Any ideas what is the best solution?Many thanksBest RegardsAlkan #audio-comparing-and-switching