2015-05-08 2:17 PM
Hello, I am designing an Audio Amplifier that is capable of connecting to 4 ohm, 6 ohm and 8 ohm speakers. I need to be able to run at an output of 25W at 25V so I decided to go with the TDA7492P. For reference, I have puchased the 50W and 20W Evaluation Boards and everything is great so far.
Question: The reference design of the 20W Amp shows the following image.2015-05-10 6:21 PM
hello engineer X ,
the filter LC parameter will affect frequency response of class D amplifier ,due to the filter is LCR filter in fact. so when the load impedance had been changed , the LC parameters should be changed to provide a flat response within audio band. if you used LC fitler for 8 ohm , and connected 4 ohm load, you will found 2~3 dB attenuation around 20Khz . so if you'd like to support 4~8 ohm load , it's better to choose LC parameters for 6 ohm load . and another improtant thing is output current capability of amplifier , if you are going to deliver 25W 1%THD @ 4 ohm load , 16 V supply is enough , but if you are using 8 ohm load , it's better to provide 22V supply . due to TDA7492P is slug down package , so the disspation power will be transferred to ambnient from PCB, in case you need to deliver high output power continously , it's better to choose TDA7492 , it's slug up version and external heatsink willl help to keep IC runing with high output power . thanks to consider ST device .