Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).
Most recent activity
When I want to detect the variables of 2-d array, found it have not be support in this tool, just support for 1-d array, can anyone help to check it whether is my omission or this function is not existed.
Hi all,trying to download a copy of your STM32CubeMonitor-RF, I am a little confused about SW revisions.According to your download site it should be 2.5.0:But it looks as if the downloaded executable still is revision 2.4.0. Setup wizard reports this:Also the installed SW says 2.4.0:Could you please have a look and / or provide a link for the latest 2.5.0?Thank you and kind regardsGotthard
Dear all, is it possible to change the Y scale for Chart? In the information panel I can see group[Home] Chartorder4width"7"height"5"chartType"line"curveType"linear"duration"10"ymin""ymax"", but in the Properties tab I can see only group, size, chart type, curve type, duration and name... Scale is missed.
..
I have successfully built and downloaded the motor control application using ST motor control workbench and the CubeIDE etc and can connect to flash and step through my program. However when it comes to using CubeMonitor i get an error giving "not connected ! Unknown JTAG chain (16)"In the config screen i can flash the LED on the board ... I have tried both protocols SWD and and JTAG .. Can i use monitor with the BG431B-ESC1 board ?Many thanks if youve got this far ....
Hello,Is it possible to monitor local variables using STM32CubeMonitor?
I tried to get the variable "g_counter1" in 80 micro-seconds for the STM-Studio Example project using CubeMX_ver.5.6.0 and EWARM_ver.8.42.1.But the result was not as good as the attachment below.-STM32_CubeMonitor_Result_dashboard_g_counter1.PNG-Log_myVariables_2020-04-29_14h35m16s.zip (Log_myVariables_2020-04-29_14h35m16s.stcm)In the first place, can CubeMonitor be obtained in 80 microseconds?In addition,MCU: STM32G0431KB(NUCLEO-G431KB)This setting information is the following attached file.-STM32_CubeMonitor_Setup1_Block_diagram.PNG-STM32_CubeMonitor_Setup2_Variable_AquisitionParameters.PNG-STM32_CubeMonitor_Setup3_Probe_Protocol_Frequency.PNGThe setting value of this source code is the following attached file.-STM32_CubeMonitor_SourceCode1_dataAqc.c.PNG-STM32_CubeMonitor_SourceCode2_dataAqc.h.PNGThank you for your guidance.
I am looking to get a good power consumption measurement of my STM32L011K4. I bought the Nucleo-LPM01A for that. However, the project I've loaded onto my L011K4 does not load when in USB mode. I've checked the user manual UM2243, but that described only how to measure the power of the MCU as use case.What should/can I do?
During testing I frequently make changes to the source and re-compile it using "STM32CubeIde". Now, when trying to add/remove a variable from the watchlist ("variables" node in STM32CubeMon), I get the following message and my previous selection is gone."The variable list has been updated because the executable file *** has changed."So even the list of available variables has not changed (and I think even their address is still the same), I have to redo the selection.So is there a way to tell STM32CubeMon to update the symbol table and thereby keep the old selection?Kind regards,Thomas
I am using keil compiler and loading the .axf file.Other than global variable which are arrays no other global variables are visible in the variable list for selection.What i am missing here?
I am using keil asIDE and would like to use the capabilities of Cube Monitor for debugging. I could not figure out how to import keil project, or any of the generated files into Cube monitor. Looking for inputs and references.
Hi all,I have a data streaming firmware and to keep the stream alive I must reset a counter before it reaches a fixed value.Is there a way to perform this operation with CubeMonitor while monitoring other values?Thank youWalter
Hi,I'm trying to plot different values on different plot charts because they live in a very different scale, but it seems that the "Single value" subplot is not working.If I remove it the plot charts show all the values correctly.Any idea?Thank youWalter
Hi I am trying to use the Write Panel Mode in my flow to inject values into my target device (via the STM link).I have setup the Write Panel Node (following the nodes instructions) and the Node works as expected, whereby I can enter values into the variable spaces on the dashboard and when I hit the 'write' key it send it to my target and updates the values.What I wanted to know, is there a way to programatically trigger the 'Write' from the node red flow instead of using the dashboard button??This is my example flow.The 'inject vals' node is a basic node red 'inject' node. I was hoping to use this node to write values into the 'Write panel' node and get it tp send the values to the target without havind to press the 'write' button on the bashboard.Any help is appreciatedCheersMichael
Hello, I wondered if you will add the ability to import/add new nodes to the STM32CubeMonitor system from the Node Red Library (https://flows.nodered.org/)?After all this is one of the strengths of the Node Red system to enable the use of collabrative built nodes. Many thanksMichael
(Windows 10 x64, TrueStudio v9.1.0, STM32CubeMonitor v1.0.0)
Hey allI've been having issues filtering out values from my processing module1) for the second graph and gauge i went in and modified it to look like thisi wanted to extract a variable out of my list called sum so in the varfilter i placed sum as a string input but when i go to deploy, nothing comes out of it.any ideas ?attached the whole thing in a zip
Hi,if i record the power everything looks good like:but, if i zoom in/out or press "Show All" it looks like this:Anyone else using this feature?
The process is as follows:config the variables node ,choose the axf executable filespitch on Expand Variable Listwaiting for the file parsing,and then the software breakdown
The new STM32CubeMonitor software tool from STMicroelectronics displays runtime variables of STM32 applications in real time while enabling developers to customize the graphical visualization in their OS environment of choice (Windows®, Linux, or MacOS®).You can find the presentation and software at : www.st.com/stm32cubemonitorThe reference documentation and setup instructions are available in stm32mcu wiki : https://wiki.st.com/stm32mcu/wiki/STM32CubeMonitor:STM32CubeMonitor_overviewIf you have questions or want to share feedback, please post in this forum, and set the tag STM32CubeMonitor.
The cube monitor can't find my target board,but the KEIL did it.what should I do? Thank you ~~
Using the same .elf file for several projects using f303, f301, f407 and f779 MCUs, all work on the first 2 machines but although the Ubuntu 19.10 sees the STLink OK (the area I thought most likely to fail) the selection of the .elf file results in no variables being shown at all.Is a system function being used to examine the .elf file that is missing in the latest *buntu ?I've tried checking for dependencies missing (apt -f install) but nothing apparent.Cheers
ST Community highlights – April to June 2026
Already have an account? Login
No account yet? Create an account
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.