WATCH ON-DEMAND | STM32 Summit 2026
Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
Most recent activity
I am working on a custom board with STM32MP133A cpu and Kingston EMMC08G-ML36 EMMC. The board boots fine from the EMMC, however if the board resets due to kernel panic and/or watchdog timeout it fails to boot from EMMC and enters DFU mode (where it hangs indefinitely). It looks like that after unexpected reset EMMC stays in 8-bit bus width and boot-rom fails to load the TF-A. The current workaround is to set bus-width to 1 in both u-boot and linux device trees. Is this boot-rom behavior described somewhere?Is there any way to reliably reset bus-width from 8 to 1 in case of unexpected STM32MP133A reset? Or to get out of DFU mode after some timeout, although in this case bus-width still has to be reset to 1 somehow?
Hello,I’m working with an STM32MP255 and want to access GPIOs from the Cortex-M33 coprocessor (not from the A-core/Linux side). I’m trying to understand the correct workflow and configuration steps so M33 firmware can drive/read GPIO pins. Specifically:1. Are there any reference examples or official documentation showing how to assign GPIO pins to the Cortex-M33 coprocessor (M33 execution context) using device tree and RIFSC configuration on STM32MP255 / STM32MP2 devices?2. Is there a step-by-step for RIFSC/firewall, resource assignment, or device tree overlays that shows how to move ownership of a GPIO from the Linux/A-core domain to the M33?3. I’m using STM32CubeIDE to build the M33 firmware. Under SystemCore → GPIO there is no checkbox to select the Cortex-M33 execution context for a GPIO. Is that expected? If so, how should I configure ownership (is it a device tree / RIFSC setting rather than a CubeIDE option)?
Due to the high cost of RAM. I wonder if ST have plans or other information about which 4GB RAM vendors fits MP25x products?I know that ST have information about other RAM vendors on their wiki. Only one 4GB vendor is mention there.I bought the 4GB RAM MT53E1G32D2FW-046 WT:C (single rank) from here when it cost 20 USD.https://www.aliexpress.com/item/1005009146059053.html but its seems to only having the DDR density to 8bits (2 GB). Perhaps it was only a 2GB or MT53E1G32D2FW-046 WT:B (dual rank)I'm still looking for other RAM vendors that can offer 4GB solutions for the MP25x. Question:Can ST write a criteria what a RAM memory need to have to fit MP25x? Do the RAM need to follow a specific RAM standard? What do I need to know to know if the RAM memory fits the MP25x?
Hi everyone,I am encountering an issue while trying to flash OpenSTDroid onto my STM32MP257F-DK board.I downloaded the Starter Package from the official website and used STM32CubeProgrammer for the installation. However, the flashing process consistently fails during the final stages.Could anyone provide the correct flashing procedure or suggest what might be causing this error? Below are the details of my setup:Starter Package Source: STM32MP2DroidSta | Product - STMicroelectronicsSTM32CubeProgrammer Error Screenshot: Thank you in advance for your help!
In my custom FSBL on an STM32MP135AAE3, everything runs great except anytime I try to modify one of the GIC flags it pretty much ignores me completely (when I read it back, my changed bits aren't changed). I'm guessing this is some kind of trust zone or secure state or similar situation.BTW, when I run my FSBL by setting the chip to serial boot and uploading it that way, it runs great, so I know the code is solid.What do I need to change so my FSBL has full privileges? Is there a document that talks about this?
Does the stm32mp157 have an ESV or is there one in progress?
Hello everybody.On STM32MP2, is it possible to operate only the M33 like a microcontroller, without booting the A35? Also, if only the M33 is operated, can major peripherals such as I2C and Ethernet be controlled from the M33? (I assume that PCIe would be difficult...)
I am building a custom Yocto image for STM32MP1 (STM32MP157) using ST OpenSTLinux (dunfell-based) and I am facing a persistent U-Boot build failure.Environment:SoC: STM32MP157 (custom board)Yocto: ST OpenSTLinux (dunfell)U-Boot: v2020.10-stm32mp-r2.2Recipe: u-boot-stm32mpMachine: stm32mp1 Issue:During bitbake u-boot-stm32mp, the build fails in do_compile with the following error:.../tmp-glibc/work-shared/stm32mp1/uboot-source is not clean,please run 'make mrproper'This error is triggered by U-Boot’s internal check that aborts when generated files are found in the shared source tree. Observations:The error occurs even after running:bitbake -c clean u-boot-stm32mpThe failure persists until I manually remove:tmp-glibc/work-shared/stm32mp1/uboot-source and then run:bitbake -c cleansstate u-boot-stm32mp At some point earlier, I ran make menuconfig manually in the U-Boot source to inspect SPI configuration, which may have introduced .config or include/config/* into the sh
I've got an STM32MP135AAE3 for which I'm writing my own FSBL. It's basically working!There are two scenarios:1) Chip set to serial boot; the BootROM wakes up and I use STM32_Programmer_CLI.exe to send it my FSBL which it stores in SYSRAM, BootROM then passes execution to my FSBL2) Chip set to boot from eMMC; BootROM wakes up, sees my FSBL in eMMC, copies it from eMMC to SYSRAM, passes execution to itIt would be helpful for my FSBL to know which scenario it is, and according to STM32 MPU ROM code overview I should be able to inspect the first 512 bytes SRAM2 for a bunch of boot information as defined in this H file. It also says SRAM2 is for "ROM code secure data" and SRAM1 is for "ROM code non-secure data" and I'm running in non-secure mode so maybe it's actually SRAM1 for me?In any case, I've got my LD file set up so nobody touches the first 512 bytes of either SRAM1 or SRAM2:MEMORY { SYSRAM (rwx) : ORIGIN = 0x2FFE0000, LENGTH = 128K SRAM1 (rwx) : ORIGIN = 0x3
Hello,unlike the STM32MP157F-DK2 the STM32MP257F-DK is not equipped with an Touch/LCD.Is it possible to use an identical/similar LCD with the STM32MP257F-DK (that means: are the appropriate connections on the board)?Marc
Linux kernel, Yocto project, etc. each has their LTS strategy, does ST has similar plan for its OpenSTLinux?
Hi,I am trying to understand and test secure boot on STM32MP1. I was able to compile and boot unsigned tf-a. boot failed as expected as it is not verified.generated keys.Now how to burn these below hash file? can we burn into flash and test without using OTP for development and POC?publicKeyhash.binThank you.
Hello Team,I am currently working on QuadSPI with MDMA, but I am unable to locate the driver code for this functionality.Could you please provide the required driver code?For reference, I am working on the STM32MP133F series.Regards,Sreedhar Kaduru
Hello,Is there a list of supported/recommended displays that are compatible with the DSI connector CN4 on STM32MP157D-DK1 please?Kind regards,Al
I've got a custom board with an STM32MP135AAE3 talking to an eMMC (THGBMTG5D1LBAIL if it makes a difference). I've discovered that if I write from SYSTEM to the eMMC using DMA (HAL_MMC_WriteBlocks_DMA) it works fine, but if I use anything in RAM (SRAM1, SRAM2, or SRAM3) as the source, the DMA fails immediately.If it helps, the SDMMC2 registers inside SDMMC2_IRQHandler() are: STA=0x8001010; DCOUNT=0x200; DCTRL=0x90; IDMACTRL=0x1; MASK=0x11AIs this a known limitation of the IDMA? If not, is it something I'm somehow initializing incorrectly?
Hi,We are trying to make use of the ethernet interface in this fashion:- The board is a custom one with a soldered module from Karo, the qsmp-2550, that includes an stm32mp255fa.- The eth2 is connected to a PHY (TI DP83869HM) in RGMII.- The PHY is then configured to output Base100-FX to an SFP cage.- There is no CLK125, we use ck_ker_eth2 configured at 125Mhz (confirmed in /sys/kernel/debug/clk/stm32_clk_summary), we use the `st,ext-phyclk` DT property.The PHY is reachable via mdio using the CLI from mdio-tools and seem to be working as intended.We checked that the PHY sends the correct clock, the RX one, with a scope: it does.Then when enabling the link using `ip link set up eth0` we are greeted with:```root@qsmp-2550:~# ip link set up eth0[ 16.583371] stm32-dwmac 482d0000.eth2 eth0: Register MEM_TYPE_PAGE_POOL RxQ-0[ 16.586971] stm32-dwmac 482d0000.eth2 eth0: Register MEM_TYPE_PAGE_POOL RxQ-1[ 17.123948] stm32-dwmac 482d0000.eth2 eth0: PHY [stmmac-1:00] driver [TI DP83869] (irq=
I have built a custom board by using STM32MP257F and I want to boot on USART6. I have not succeed to boot on USART6 when I compile my own fsbla by change the device tree of TF-A.I got a suggestion from ST Dev team to run this ROM tracedump wiki-stm32mp-addons/MP2RomTracesDump at 6.1.0 · STMicroelectronics/wiki-stm32mp-addons · GitHub and it gave me a positive output on USART6. The soldering was OK. The BootROM was OK and the UART6 was alive. This is the output from my USART6.=================================================== == STM32MP25 cut2.x bootrom display traces V1.01 == == Date of compilation : Jun 26 2024 - 11:25:23 == =================================================== Executed on Cortex A35 - Aarch64 Successfully booted on interface SD instance 1 Reset reason : POR reset Chip state : CLOSED_UNLOCKED ================================================================== Bootrom traces ================================================================== [INFO] -
Hello, I am working with an STM32MP135f-dk device running Linux and trying to evaluate the possibility of using the USART peripheral in synchronous mode (TX/RX + CK). From a hardware point of view, the STM32 USART clearly supports synchronous operation. However, when using the standard STM32 USART Linux kernel driver, the peripheral is only exposed as a /dev/ttySTM* device and operates strictly in asynchronous (UART) mode. As far as I can see, the current driver does not enable or drive the CK clock signal, which makes true synchronous USART communication impossible under Linux, even though the underlying hardware is a USART. My questions are:1. Is this limitation expected by design in the current STM32 Linux USART driver? 2. Has anyone successfully implemented synchronous USART on STM32 under Linux, for example by: Extendimg the existing driver, writing a custom kernel driver, or using an alternative ?
Dear All,I have a total of 8 boards with eMMC from Alliance Memory. All of them boot from SDCard and work well. On 4 of them eMMC is detected correctly and boots fine with 50Mhz/8bit/ddr speed.4 boards are failing in exactly the same manner, that is: EXTCSD/CID registers have some wrong values and eMMC is discovered as 128MB (instead of ~4GB), with with wrong manuf. ID and manufacturer code. Writing gives io-error (timeout) - reading returns "ER18" ascii code every 512bytes.I have lowered down params of sdmmc interface down to: 400kHz / 1 bit / no-ddr, with different slew-rates on IO ports without a success. I've observed these changes on an oscilloscope and also with simple logic analyzer on lower speeds/1bit bus. Failure is persistent between restarts and also between boards. I have also manipulated series resistors and pull-up resistors.Normally I'd expect some layout issues, but this failure mode is really stable and I am looking for other ideas. I can't imagine tha
Please check STM32MP157F-DK2 no function issue after STM32MP157F-DK2.#1. After receiving the STM32MP157F-DK2 board, I connected a 5V/3A Type-C Power Adapter to CN6 and verified Linux boot and operation. LCD operation.#2. Updated the Linux image on the SD card using STM32Cube Programmer on a Windows PC.Following the procedure in the link below, successfully updated the Linux flash image to the SD card using FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv via STM32Cube Programmer on the Windows PC.https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image#3. Turn SW1 BOOT0 and BOOT2 back ON, connect the USB Cable to the ST-LINK (CN11) on the PC, and connect the 5V/3A Type-C Power Adapter to CN6 to boot the stm32mp157f-dk2 board.#4. UART logs output normally, but the message "ERROR USB TYPE-C connection in unattached mode" appears and Linux does not boot. - The same Type-C Power Adapter used in #1 above was
Hello,I am working with an STM32MP151 and I would like to start the Cortex-M4 core as early as possible during the boot sequence.The main requirement is to run a real-time task on the M4 that reads an analog input (ANA0 – ADC channel) with minimal startup latency.In my current setup, the ADC channel is first owned by the Cortex-A7 Linux kernel and is explicitly released and reassigned to the Cortex-M4 via the Linux device tree (by disabling the ADC node for A7 and assigning it to the M4).Additionally, if I stop the system in boot mode and manually start the Cortex-M4, I am able to successfully debug the M4 firmware and correctly read the ADC value.My goal is to have the M4 firmware start automatically in the same early boot conditions, without requiring a manual boot/debug sequence.I would like to understand:At which earliest boot stage the Cortex-M4 can be releasedWhether the Cortex-M4 can be started independently from the Linux boot on the Cortex-A7Thank you in advance for your suppo
Hello,Currently I'm working on a project that requires a synchronized clock signal between multiple devices connected through Ethernet.The logic solution for this is PTP, and using linuxptp I was able to archive synchronous PPS on PG8 pin between devices with a jitter smaller than 1us for 1Hz. Now the problem is that the requirement for PPS frequency is not 1Hz but a OR between a 100Hz and 1.25Hz (see attached image). From documentation, flexible PPS output may be the solution and started testing it by generating the 100Hz signal. Here is were I found the issue, after program PPSCMD[3:0] with start I notice that the 100Hz signal starts to drift slowly (around 20us/s).Now strange part is if I use fixed PPS (bit PPSEN0 of MACPPSCR cleared) with any frequency (1Hz to 16kHz with digital rollover) there is no drift. From my understanding the reference clock for pps is the same as system time thus adjusted by ptp protocol for maintaining synchronization.Is my assumption corre
Hello!I am in the progress of setting up a Yocto based build for a custom board based on a STM32MP157C. I am using "vanilla" Yocto scarthgap with the respective ST meta layer: https://github.com/STMicroelectronics/meta-st-stm32mp meaning I created a custom machine and am patching my own device trees into the meta-st-stm32mp layer.Currently I am trying to port my device trees for TF-A , OPTEE, U-Bboot and Linux, that were originally created for an SDK based build, to the new environment. I am using the regular "optee" bootscheme in my custom maschine.conf with EMMC as boot device.The build already succeeds but when I try to program the contents of my .tsv via Cube32Programmer I get a "iwdg1" reset when the bootfs is downloaded:UPLOAD ... done Ctrl+C to exit ... #DOWNLOAD ... OK Ctrl+C to exit ... # UPLOAD ... done Ctrl+C to exit ... # UPLOAD ... done Ctrl+C to exit ... ###D/TC:0 gic_native_itr_handler:678 Special interrupt 1023 D/TC:0 gic_native_itr_handler:678 Special interru
Hello, I am trying to load an .elf file on the M33 core on my stm32mp257f processor. When I launch the remote core using remoteproc I get the following errors. root@stm32mp257f-hydra-mx:~# echo -n /home/root > /sys/module/firmware_class/parameters/path root@stm32mp257f-hydra-mx:~# echo Sparta.elf > /sys/class/remoteproc/remoteproc0/firmware root@stm32mp257f-hydra-mx:~# echo start > /sys/class/remoteproc/remoteproc0/state [ 119.336297] remoteproc remoteproc0: powering up m33 [ 119.511444] remoteproc remoteproc0: Booting fw image Sparta.elf, size 6237772 [ 119.513130] remoteproc remoteproc0: unsupported fw ver: 0 [ 119.518401] remoteproc remoteproc0: no resource table found for this firmware E/TC:0 stm32_iac_itr:192 IAC exceptions [159:128]: 0x200 E/TC:0 stm32_iac_itr:197 IAC exception ID: 137 E/TC:0 stm32_risaf_dump_erroneous_data:256 DUMPING DATA FOR risaf@420d0000 E/TC:0 stm32_risaf_dump_erroneous_data:257 ================================================
Hi,I am trying to work with the USART6 which is connected to is connected to PF13 (TX) and PF14 (RX) on the extended GPIO.It looks like the SCRIF does not allow access to this USART, wven though the OPTEE configuration seems to enable it:from optee/...core/.../stm32mp257f-ev1-ca35tdcid-rif.stdi:...IFPROT(STM32MP25_RIFSC_USART6_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIF_UNUSED, RIF_SEM_DIS, RIF_CFDIS)...but when I boot the board I can see this:cat /sys/kernel/debug/stm32_firewall/rifsc | grep USART| USART1 || 31 || NSEC || NPRIV || enabled || enabled || 0 || 0x0 || USART2 || 32 || NSEC || PRIV || enabled || disabled || 1 || 0x0 || USART3 || 33 || NSEC || NPRIV || enabled || enabled || 0 || 0x0 || USART6 || 36 || NSEC || NPRIV || enabled || disabled || 2 || 0x0 | From what I understand it means the CID is 2 which means access to this USART can be done only from the M33 micro. Is that correct?How can I solve this? I am struggeling with Yocto for a while with no su
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.