Skip to main content
Lead
Feb 17, 2026 10:15 AM UTC
Solved

Lack of other 4GB RAM alternatives for MP25x

Due to the high cost of RAM. I wonder if ST have plans or other information about which 4GB RAM vendors fits MP25x products?

I know that ST have information about other RAM vendors on their wiki. Only one 4GB vendor is mention there.

I bought the 4GB RAM MT53E1G32D2FW-046 WT:C (single rank) from here when it cost 20 USD.

https://www.aliexpress.com/item/1005009146059053.html but its seems to only having the DDR density to 8bits (2 GB). Perhaps it was only a 2GB or MT53E1G32D2FW-046 WT:B (dual rank)

I'm still looking for other RAM vendors that can offer 4GB solutions for the MP25x. 

Question:

Can ST write a criteria what a RAM memory need to have to fit MP25x? Do the RAM need to follow a specific RAM standard? What do I need to know to know if the RAM memory fits the MP25x?

 

PatrickF
PatrickFBest answer
ST Employee
Feb 23, 2026 4:32 PM UTC

Hi,

Btw, did you look to use 2 x DDR4 16-bits 16Gbits (as on STM32MP257F-EV1) ?
Might offer more manufacturer choices and so lower price or better availability (LPDDR4 32-Gbits single-rank is almost limited to Micron as far as I know).

Furthermore, DDR4 timings are usually slightly more robust than LPDDR4 (at the expense of more power rails and PCB terminations).

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

10 replies

Erwan SZYMANSKI
ST Technical Moderator
Feb 18, 2026 9:51 AM UTC

Hello @DMårt ,
Maybe this Application Note could help you to get DDR criteria accepted for STM32MP2x designs: https://www.st.com/resource/en/application_note/an5723-guidelines-for-ddr-configuration-on-stm32mp2-mpus-stmicroelectronics.pdf

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
DMårtAuthor
Lead
Feb 18, 2026 10:39 AM UTC

Thank you @Erwan SZYMANSKI for the reply.

So, dual channel e.g MT53E1G32D2FW-046 WT:B can work with MP25x?

If a RAM follows JEDEC standard, it's compatible with MP25x?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
PatrickF
ST Employee
Feb 23, 2026 1:47 PM UTC

Hi,

maybe a mixed-up with dual-channel (STM32MP25 has 2 x 16bits channels in lockstep mode to form a 32 bits memory) and dual-rank (2 x chip select per channel, which is not supported by STM32MP25).

The MT53E1G32D2FW-046 WT:B (dual channel, dual rank per channel) could work with STM32MP25, but with half of the size accessible (i.e. 16Gbits).

The MT53E1G32D2FW-046 WT:C (dual channel, single rank per channel) will work with STM32MP25, with full size accessible (i.e. 32Gbits).

 

Regards.

 

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
PatrickF
PatrickFBest answer
ST Employee
Feb 23, 2026 4:32 PM UTC

Hi,

Btw, did you look to use 2 x DDR4 16-bits 16Gbits (as on STM32MP257F-EV1) ?
Might offer more manufacturer choices and so lower price or better availability (LPDDR4 32-Gbits single-rank is almost limited to Micron as far as I know).

Furthermore, DDR4 timings are usually slightly more robust than LPDDR4 (at the expense of more power rails and PCB terminations).

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
DMårtAuthor
Lead
Feb 23, 2026 8:32 PM UTC

Thank you @PatrickF ! I did not know that!

By the way! I think you should try Kingstons memories. They seems to be single rank and 32-bit density.

I will look at DDR4! Perhaps it might be a 4 GB DDR4 that fits my board.

Edit:

I look up the prices for DDR4...more expencive than LPDDR4! And only 16-bit density size.

So I'm staying at LPDDR4! 

The Kingston B3221PM3BDx might look interesting!

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
PatrickF
ST Employee
Feb 24, 2026 6:58 AM UTC

You should try to ask Kingston directly, seems they could be OK.
Sometimes memory manufacturers make their own tests and publish results (e.g. here).

For our DK and EV boards, we will probably not change as there is long term agreement with Micron (which allow us to sell boards at decent price).

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent