Get ready for the STM32 Summit 2026 | Online, November 3
Join conversations with your peers and ST experts. Explore the full potential of STM32 microprocessors for your embedded design.
Most recent activity
I've tried using WSLg into windows 10 to start a project using the STM32cubeide but it fails. The ide is launched but those not automaticaly download stuff, but manualy do. If click new project, target selector animation goes and then I have this message "STM32 target or STM32Cube example selection is required". So can't select mpu. etc...What is the simplest way to start dev :full linux machinevirtual machineWSLg /w10 should workThx for any help.
We use the STM32MP157CA and the STM32CubeIDE and let the code generator generate a confiuration with the required modules. In our case the SPI1 on the pins (PZ0,PZ1,PZ2). The generated functions provide the initializations for the SPI1. Unfortunately the SPI1 does not work for us in normal operation mode. If we call the HAL_SPI_Transmit(...) function after the initialization we get a SPI timeout. On the oscilloscope we see no clock on the spi clock line. We also noticed that when we use the engineering mode for the M4 the SPI1 works. If we change the SPI to the SPI5 (also generated with the code generator) everything works in normal operation mode and in engineering mode. How can we use the SPI1 in normal operation mode on the M4?
I'm trying to test the low power modes (I don't care about the current at this point). I start the Next I run this:cd /usr/local/Cube-M4-examples/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo_wakeup fw_cortex_m4.sh start echo enabled > /sys/devices/platform/soc/4c001000.mailbox/power/wakeup echo "*delay" >/dev/ttyRPMSG0 systemctl suspendThe CPU never goes into CStop mode. DMESG reports the following:[ 4665.621976] unbind driver hci_uart [ 4665.884144] PM: suspend entry (deep) [ 4665.900196] Filesystems sync: 0.013 seconds [ 4665.905556] Freezing user space processes ... (elapsed 0.001 seconds) done. [ 4665.913002] OOM killer disabled. [ 4665.915975] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done. [ 4665.923519] printk: Suspending console(s) (use no_console_suspend to debug) [ 4665.933455] dwc2 49000000.usb-otg: suspending usb gadget configfs-gadget [ 4666.063929] stm32-dwmac 5800a000.ethernet eth0: Link is Down [ 4666.065574] stm32-dwmac 5800a000.ethe
..
Hi everyone,I'm interested how can someone backup rootfs, vendorfs etc and later use that to flash via the STM32CubeProgrammer? Is using the dd good way to do it?Best regards,Nenad
We are using the STM32MP15 ecosystem 2.1.0 and buildroot build flow for a custom board. The custom board uses the FMC peripheral to connect to three FPGAs using an SRAM/PSRAM interface. We have successfully implemented this interface on the CA7 side by writing a custom kernel driver, but would now like to move this function to the CM4. After using CubeMX to move the peripheral to the CM4, there is an error in the generated device tree for the kernel, specifically there is a missing symbol “m4_fmc�? in the generated device tree.I looked at the STMicro kernel repos on GitHub at the in-tree stm32mp157-m4-srm.dtsi file for both ecosystem 2.1.0(v5.4-stm32mp1-r2.1) and 3.0.0 (v5.10-stm32mp1-r1) and there is no definition for “m4_fmc�? in either version.Does this mean that the FMC for the STM32MP15x is not yet supported by HAL? Or just an oversight?Thanks,Mark Carlin
When exiting out of standby mode through RTC,Wakeup pins or PON Key in all the cases System stops at : INFO: SP_MIN: Preparing exit to normal world.Here is the complete log :[ 32.488278] usb33: supplied by vdd_usb#echo mem > /sys/power/state [ 37.576569] PM: suspend entry (deep)[ 37.587289] Filesystems sync: 0.008 seconds[ 37.591188] Freezing user space processes ... (elapsed 0.001 seconds) done.[ 37.597870] OOM killer disabled.[ 37.601128] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.[ 37.608535] printk: Suspending console(s) (use no_console_suspend to debug)NOTICE: CPU: STM32MP157C?? Rev.ZNOTICE: Model: SBS MOBIOINFO: Reset reason (0x810):INFO: System exits from STANDBYNOTICE: BL2: v2.2-r2.0(release):NOTICE: BL2: Built : 10:03:06, Apr 15 2021INFO: Using crypto library 'stm32_crypto_lib'INFO: BL2: Doing platfo
Could you please explain me why ST support is so slowly... I'm starting with STM32MP1xx MPUs hoping, that ST support will be fast and specific. But currently answer for even simple (and stupid) questions need to be wait for unpredictable time...We need to read hundred pages with inconsistent information even for simplest steps like compiling TF-A or U-BOOT.We spent a lot of time designing custom MP157 module, It's forking fine except qspi-nand and nobody could help me... There is simple question - why qspi nand flash connected according to Getting started guide is not working. Hardware seems no problem - at least FlashID read ok. There are two sample board with exactly same symptoms... Why you can't provide simple step-by step manuals:compiling TF-Acompiling U-BOOTFlashing with USB?Event your README.HOW_TO.txt have stupid mistakes like TFA_DEVICETREE instead of TF_A_DEVICETREE.May be I need to pay money for support? Please give wallet address to pay.Dealing with Allwinner MCUs I had su
Helllo i configurated my Device tree so i a can use my USART3 as a serdev. But when i run "cat /proc/tty/driver/stm32-usart". i can see my serial port but my RTS pin is missing. I configurated my device tree like this:&usart3 { pinctrl-names = "default", "sleep", "idle"; pinctrl-0 = <&usart3_pins_c>; pinctrl-1 = <&usart3_sleep_pins_c>; pinctrl-2 = <&usart3_idle_pins_c>; uart-has-rtscts; status = "ok"; ethernet { compatible = "st,stm32_usart_net"; local-mac-address = [ A0 B0 C0 D0 E0 F0 ]; };};So But if i remove the ethernet part it shows the RTS port. Why is that happening?
A quick grep through the latest and greatest release shows this:$ grep -r STM32MP157C-DK2 . | grep machine ./meta-st/meta-st-stm32mp/conf/machine/stm32mp1-disco.conf:#@DESCRIPTION: [EXAMPLE] STM32MP157C-DK2 board ONLY with Trusted boot and SDcard support ./meta-st/meta-st-stm32mp/conf/machine/stm32mp1-disco.conf:M4_BOARDS = "STM32MP157C-DK2" ./meta-st/meta-st-stm32mp-addons/conf/machine/examples/stm32mp1-disco-mx.conf.sample:#@DESCRIPTION: [STM32CubeMX-EXAMPLE] STM32MP157C-DK2 board ONLY with Trusted boot and SDcard support ./meta-st/meta-st-stm32mp-addons/conf/machine/examples/stm32mp1-disco-mx.conf.sample:CUBEMX_PROJECT = "mx/STM32MP157C-DK2/my-demo/DeviceTree/my-demo"So I am wondering if/how it's possible to have a kernel/device tree/rootfs which is not signed.My ideal setup grabs (unsigned) kernel/device tree from tftp and passes to the kernel the kernel command line to boot over nfs (unsigned as well).If this possible at all here with an unsigned kernel/device tree/rootfs?If so, c
I recently attended and intro course to the STM32MP1, which was very informative. Subsequently, in considering possible applications, I have questioned wither the STM32 MPUs are suitable for use in functional safety systems as a processor for the execution of safety critical software, e.g. in an automotive, avionics or medical system.The use of Linux on the A7 side of things make it very difficult to use this for safety critical real time software and clearly the M4 is more appropriate anyway. However, as I see it, the M4 is effectively a co-processor with critical parts of the M4 and associated peripherals controlled by the A7 side which means that M4 cannot be adequately segregated from the A7. I understand that some peripherals can be assigned solely to the M4 and protected from access from the A7 but the A7 still controls important related aspects such as clocks and regulators. Furthermore, the A7 must bring up the chip and load and start the M4.This is a similar problem to running
Hi, ST :)In addition to https://community.st.com/s/question/0D53W00000pUh4gSAC/tfa-and-uboot-custom-compile-failsCould you plese explain me what is the reason for such error:dfu_fill_entity_mtd: Memory layout (/0x10/1*122Me) not supported!while downloading flash content with CubeMXProgrammer.I've built a core image with bitbake st-image-core command (hope I'm correct here) and got UBI image with size 116Mb (121896960b). I'm expecting it can be fitted to a UBI partition that has size 0x07a00000b = 127926272b. Please refer to nand partition table below. spi-nand flash size is 128Mb.TF-A and u-boot was manually build during duscussion mentioned with link above.Here is .tsv file:#Opt Id Name Type IP Offset Binary- 0x01 fsbl-boot Binary none 0x0 ./tf-a-stm32mp157a-stm32mp151-dk1-mx-usb.stm32- 0x03 fip-boot Binary none 0x0 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.binP 0x04 fsbl Binary(2) spi-nand0 0x000000 ./tf-a-stm32mp157a-stm32mp151-dk1-mx-nand.stm32P 0x05 fip1 Binary sp
C $> sudo apt-get updatePC $> sudo apt-get install corkscrewPC $> git config --replace-all --global core.gitproxy "$HOME/bin/git-proxy.sh"PC $> git config --add --global core.gitproxy "none for <MyPrivateNetworkDomain>" (optional, for example .st.com or localhost)PC $> echo 'exec corkscrew <MyProxyServerUrl> <MyProxyPort> $* $HOME/.git-proxy.auth' > $HOME/bin/git-proxy.shPC $> chmod 700 $HOME/bin/git-proxy.shPC $> echo '<MyProxyLogin>:<MyProxyPassword>' > $HOME/.git-proxy.authPC $> chmod 600 $HOME/.git-proxy.authI'm following above commands but when execute "echo 'exec corkscrew <MyProxyServerUrl><MyProxyPort> $* $HOME/.git-proxy.auth' > $HOME/bin/git-proxy.sh" it says git-proxy.sh not found
Hey there, I am trying to increase the RPMSG buffer size to 1024 on the STM32MP1 for the last couple of days. The A7 side seems to be working fine but the M4 side seems to struggle with the vdev declaration on the device tree. On the A7 side: virtio_rmpsg_buss.c#define MAX_RPMSG_NUM_BUFS (1024) #define MAX_RPMSG_BUF_SIZE (1024) #define RPMSG_RESERVED_ADDRESSES (2048) #define RPMSG_NS_ADDR (53)stm32mp15xx-dkx.dtsi:vdev0buffer: vdev0buffer@10044000 { compatible = "shared-dma-pool"; reg = <0x10044000 0x10000>; no-map; };On the M4 side: rpmsg_virtio.h* Configurable parameters */ #ifndef RPMSG_BUFFER_SIZE #define RPMSG_BUFFER_SIZE (1024) #endifThe user-space can see and send messages to the RPMSG channel but when debugging the M4 part I get what to seems to be a memory allocation error (gdb) 0x1000b47e in MAILBOX_Poll (vdev=0x10020f70) at ../OPENAMP/mbox_ipcc.c:105Any ideas or advice will be highly appreciated.
Hello on my serdev when i set it up the transmition complete is not set:stm32-usart 4000f000.serial: transmission complete not setI configurated my device tree like this:&usart3 { compatible = "st,stm32-uart", "st,stm32f7-uart", "st,stm32h7-uart"; pinctrl-names = "default", "sleep", "idle"; pinctrl-0 = <&usart3_pins_b>; pinctrl-1 = <&usart3_sleep_pins_b>; pinctrl-2 = <&usart3_idle_pins_b>; uart-has-rtscts; status = "okay"; ethernet { compatible = "st,stm32_usart_net"; local-mac-address = [ A0 B0 C0 D0 E0 F0 ]; current-speed = <38400>; };};So in my system it shows up like this:/sys/devices/platform/soc/4000f000.serial/serial0/serial0-0drivermodaliasof_nodepowersubsystemueventThe probe methode of my serdev_device_driver looks like this:struct stmuart *stm;u32 speed = 115200;int ret;stm = devm_kzalloc(&serdev->dev, sizeof(*stm), GFP_KERNEL);stm->serdev = serdev;spin_lock_init(&stm->lock);INIT_WORK(&stm->tx_work, stmuart_tran
When you create a project, CORE_CM4 symbol is added to properties by default.However, if you look at stm32mp1xx_hal_rcc.h, the CORE_CM4 area is still disabled. Is it a bug? Can I ignore it and use it? Or please tell me how to solve it.
Hi, Everybody!Referring to this issue:https://community.st.com/s/question/0D53W00000oVNtqSAG/qaudspi-spinand-flash-device-tree-for-tfa-and-ubootPatrickF suggested to manually configure U-BOOT for my board. I have downloaded tf-a sources patched it, of course installed and configured SDK and trying to do all according to it's README.HOW_TO.txt file.As I have my specific DT I need to specify it in makefile parameters:README.HOW_TO.txt has this example:make -f $PWD/../Makefile.sdk TFA_DEVICETREE=stm32mp157c-ev1 TF_A_CONFIG=trusted ELF_DEBUG_ENABLE='1' allBut in fact TFA_DEVICETREE var-name should be TF_A_DEVICETREE. Is this correct?Then, file format. We have .stm32, also .fip file format avaialbleI can compile both .stm32 tf-a and u-boot, but u-boot fail to start with following error:NOTICE: CPU: STM32MP157DAB Rev.ZNOTICE: Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX boardINFO: Reset reason (0x14):INFO: Pad Reset from NRSTINFO: PMI
Hello, my EVB is based on STM32MP151A SoC. The situation we are facing is that sometimes, the FSBL gets stuck and we would like to recover from it. i.e. reflash some Known Good FSBL. As the FSBL in that situation is kinda functional, the device will not fallback to boot from Serial. On the other hand, as the FSBL is itself stuck, any SW based solution to do so is irrelevant. Ideally, we need some external mean to force a serial boot, either from the STCube programmer, or the JTAG, or the like. As this seems like a very likely problem to appear during dev, there must be some classical solution to it, unfortunately, i couldn't find out a way from all the docs I could read. Is that known to anybody ? Thanks, Jacques
I'm trying to edit the device tree of the distribution but there is no .dts or .dtsi files in all the distribution package directories. The only way I found to experiment modifying the device tree is doing it with developper package (I modified stm32mp157c-dk2.dts) but I now must add it to the distribution and I'm still not able to force bitbake to generate any dts file.How can I do it.Thank you in advance.
Is there any reason why M4 is reset multiple times when entering debug mode in STM32CubeIDE? Is this normal?For example, in the case of an application that toggles GPIO, GPIO defaults to low while entering debug mode, then toggles, then goes low and toggles again. When entering debug mode completely, GPIO stays low and then toggles. (Original operation)It doesn't matter whether it completely enters debug mode and works, but it seems that m4 is reset several times while entering debug mode. I want to know why and is this normal?
My STM32MP157F-DK2 is powered by 5V 3A PSU. but at the boot up time, always it displays the warning ***************************************************** WARNING 500mA power supply detected ** Current too low, use a 3A power supply! *******************************************************At the end of the boot process, I do see following display as well:root@stm32mp1:~# [ 33.112323] usb33: supplied by vdd_usb[ 33.114843] vref: supplied by vdd[ 33.118045] vref: disabling[ 33.120724] vdda: disabling
for the STM32MP157C board
I have successfully build st-image-weston using Distribution-Package.Now I want to add libmodbus to st-image-weston.I refer to the wiki page below.https://wiki.st.com/stm32mpu/wiki/How_to_integrate_an_external_software_package1) I checked the libmodbus recipe in the path below.And I am using the meta-oe layer containing libmodbus.But I can't find libmodbus in the target.Why doesn't rootfs include libmodbus?layers/meta-openembedded/meta-oe/recipes-extended/libmodbus2)I tried to add libmodbus by executing the command below.The following error occurs.how to fix it?echo 'IMAGE_INSTALL_append += "libmodbus"' >> ../layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bbappendbitbake st-image-weston -c cleanall bitbake st-image-westonNOTE: Started PRServer with DBfile: /home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-03-31/build-openstlinuxweston-stm32mp1/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 35363,
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.