When I used the SD card connected to the STM32MP157C-DK2 board without rewriting it, the apt-get command did not work properly.
However, after rewriting the image of the starter package according to the wiki and trying it, the apt-get command became available and pip was installed correctly with the command you taught me.
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
When you mention "in my environment", could you elaborate more ?
The command I listed should be run on the board (not on your PC). If you are running a custom board, please provide more information as in that case this is not anymore a 'starter package'.
I'm not specialist on SW, I just copy the command which was working to install few python packages on my DK2 having latest starter package (Ecosystem v3.0.0, using Linux kernel 5.10).
Assuming you are using a DK1/DK2 board, maybe worth to first populate the latest starter package on the SD-card (board are shipped with starter package, but depending on manufacturing date, maybe not the latest one).
Note also that using "apt-get install python3-pip" will install 'pip' (as you wanted for), but also some 'compile' tools which are not intended to be supported on the target. This mean some very specific python package which need compilation during install might not be usable.
Regards.
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
When I used the SD card connected to the STM32MP157C-DK2 board without rewriting it, the apt-get command did not work properly.
However, after rewriting the image of the starter package according to the wiki and trying it, the apt-get command became available and pip was installed correctly with the command you taught me.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent