Question
Production mode STM323CubeIDE / ST-Link v2 / DFU - Settings?
I work on Windows and use the STM32CubeIDE 1.6.1. I want to program and debug the M4 part, On the A7 part Linux is working.
My current state is, that The A7 is in Bootloader mode and the DFU per USB is connected and shown in Windows (Gerätemanager) as USB device. There is no serial port.
In the debug settings STM32CubeIDE require a serial port.
With STM32CubeProgrammer USB1 connects and seems to work
At the end of the day I want to create and debug a M4 program.
Thx
Steffen
.