Skip to main content
MEige
Associate II
Jun 15, 2021 6:45 PM UTC
Solved

"ums 0 mmc 0" doesn't work

Hello,

I can't use the "ums" command via terminalprog (minicom)

Message is always

"STM32MP> ums 0 mmc 0

UMS: LUN 0, dev 0, hwpart 0, sector 0x0, count 0x1dacc00

Please connect USB cable. "

After 60 seconds: "USB cable not detected. Command exit."

Communication via minicom/ST-Link and ETH works.

STM32MP> usb start

starting USB...

USB0:  USB EHCI 1.00

scanning bus 0 for devices... 2 USB Device(s) found

scanning usb for storage devices... 0 Storage Device(s) found

System is buildroot, an older one and a version with kernel 5.8. No difference.

I can't find the mistake.

Marc

This topic has been closed for replies.
MEige
MEigeBest answer
Associate II
Jun 16, 2021 3:16 PM UTC

Hello Olivier,

the missing and a wrong USB cable was the problem. One of the USB cables is for charging/power supply only. And that cable was connected to the OTG.

The datalines of such cables are not connected inside. This type of cable is cheaper to manufacture. It's a commone trap (Many Type B cables suffer from this problem also). The problem is solved.

Thank you for your help.

Marc

2 replies

OlivierK
ST Technical Moderator
Jun 16, 2021 8:34 AM UTC

Hello MEige (Community Member)

Do you use a custom board or an ST board? If you use an STM32MP157C-DK2 board, after "STM32MP> ums 0 mmc 0" just plug an USB OTG type C cable as mentioned to open an USB mass storage device in U-boot. What happens when you do so?

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MEige
MEigeAuthorBest answer
Associate II
Jun 16, 2021 3:16 PM UTC

Hello Olivier,

the missing and a wrong USB cable was the problem. One of the USB cables is for charging/power supply only. And that cable was connected to the OTG.

The datalines of such cables are not connected inside. This type of cable is cheaper to manufacture. It's a commone trap (Many Type B cables suffer from this problem also). The problem is solved.

Thank you for your help.

Marc