Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hello ST,For our project, we would like to use STM32WB09KE chip as a Bluetooth MCU and would like to establish communication with the HOST MCU ex:- Stm32H5.Do you have any protocol, how we can make communication both ways from the Main MCU to enable the Bluetooth stack and send advertising parameters during the run time and get the response back to the host?Because, as a individual project - we can create an application for ble chip and run it independently, but in this case we would like to control the BLE chip from the host mcu by sending requests.We can use UART/SPI for this purpose, but in detail do we need to send the ACI commands or HCI commands for enabling the BLE stack on the BLE chip?IF you have an example, please provide us.Thanks & RegardsPT
Hello,When I add the BLE stack to the STM32WB35CEU6A, I notice that the RTC and timer settings don’t work correctly. With the BLE stack enabled, I can’t get accurate time information from the RTC and timer, or there are inconsistencies in the timing. Is there something I might be overlooking in the STM32CubeMX settings? What specific settings should I pay attention to for stable operation of both RTC and timer with BLE?Thanks!
Hello, I'm a beginner in hardware design for STM32 MCU wireless. I usually get detailed information about component value recommendations in the datasheet or application note. But in STM32WL33, I get unclearer information than in other MCU wireless documentation like STM32WL5 or STM32WB55. Here is the application circuit from the STM32WL33 datasheet; there is no component value recommendation. I have several question1. what is L1 and L2 recomendation value?2. I want to use this MCU for 433MHz or 868MHz, so what value recommendation for matching network components?3. Why in the application circuit there is no RF switch? In AN5407 and MB1720 docs (STM32WL_QFN48_4Layers_Ref_Board) I found that using RF switch.
HI Team,We are using the STM32WB controller for our project, in that we are using the I2C1 for to communicate with Eeprom Module.Can anyone explain how to configure/Calculate the Exact Timing Register value. If we have any sample calculator for different I2C Speeds along with other register settings it is very helpful to us.Currently My Register value: hi2c1.hi2c1.Init. Timing = 0x00000E14, for which I2C speed it is calculated we are not understanding. Regards,Srinivas.V
I am currently working with the STM32WB55RGV6 microcontroller, which has a total of 1 MB of Flash memory. However, after generating a project using STM32CubeMX, I noticed that the Flash memory file only indicates 512 KB of available memory.Could you please provide clarification on how the remaining memory is allocated among different sections? Understanding the memory organization would be greatly appreciated.Thank you for your assistance.Thanks and RegardsSarthak Malik
Hello,Does anybody knows - are 4 wires enough for programming: STM32F411CEU6 module JP5 of the NUCLEO-WB55RGGND <---- T_VDDSWSCK ??? SWOSWDIO <---- SWCLK3.3V <---- SWDIO ??? NRST &nb
My STM32WB5MMG application interfaces with a GPS receiver. Ideally, what I would like to do is to update the RTC date/time every time I get a timepulse signal from the GPS, so that the RTC date/time is always as close as possible to GPS time. However, my application also uses ST's HW timer server, and when I update the RTC date/time, it seems as though this also resets timers in the HW timer server, so that those timers do not trigger when expected.Is there a way to update the RTC without interfering with HW timer server timers?Thank you!
Hello,What should I do to record BLE traffic (data send and received) between STM32WB55 and PC?
Hello, Iam trying look for low budget chip for my application, Can you guide if stm32wl33 will work for lorawan communication to send temp. data
I have a P-NUCLEO-LRWAN3 and I have downloaded the I-CUBE-LRWAN expansion software.Using the project "STM32CubeExpansion_LRWAN_V2.1.0 \ Projects \ NUCLEO-L073RZ \ Applications \ LoRaWAN \ LoRaWAN_AT_Master \ STM32CubeIDE \ LRWAN_NS1" and following the procedure indicated on the file "readme.txt" on the VCOM port I cannot send and receive anything. I also tried to use the "LoRaWAN_End_Node / STM32CubeIDE" project but there is no project related to my SX1278 model. Instead the Gateway works perfectly. I've read all the existing documentation but can't get it to work. What i can do?ThanksEdit: by enabling DEBUGGER_ON in "sysconf.h" I can see this but I can't send AT commands
Algumas das minhas plcas quando faço a gravação do BLE não consigo comunicação com a USB do meu computador para fazer a gravação do meu firmware. Translation: When I record the BLE I cannot communicate with my computer's USB to record my firmware in some boards of mine. 9:26:07 : UR connection mode is defined with the HWrst reset mode09:26:07 : ST-LINK SN : 50FF6D06778854543533116709:26:07 : ST-LINK FW : V2J45S009:26:07 : Board : --09:26:07 : Voltage : 2.63V09:26:07 : SWD freq : 4000 KHz09:26:07 : Connect mode: Normal09:26:07 : Reset mode : Software reset09:26:07 : Device ID : 0x49509:26:07 : Revision ID : Rev Y09:26:07 : Debug in Low Power mode enabled.09:26:07 : UPLOADING OPTION BYTES DATA ...09:26:07 : Bank : 0x0009:26:07 : Address : 0x5800402009:26:07 : Size : 96 Bytes09:26:07 : Bank : 0x0109:26:07 : Address : 0x5800408009:26:07 : Size : 8 Bytes09:26:07 : UPLOADING ...09:26:07 : Size : 4 Bytes09:26:07 : Address : 0x5800408009:26:07 : Read progress:09:26:07 : Data read
Hi Everyone! So yeah, as the title says, while designing the PCB, we forgot to ground RF_Out and ANT_IN pins of STM32WB5MMGH6T6, datasheet says we should have, because there is no external antenna. We have noticed it when we tried to run our codes to connect Bluetooth but nothing worked. So I am not sure if it is the reason and if it is the reason, is it possible to take the BLE module off with hotair and short circuit unconnected pads to neighboring GND pads?
Hi,I use the BLE_p2pServer example as a basis and would like to forward the transmitted data directly to the UART1 interface. My idea would be to use here (in p2p_server_app.c) a HAL_UART_Transmit_DMA() function, but I fail to access the data due to an incorrect type conversion. case P2P_SERVER_LED_C_WRITE_NO_RESP_EVT: /* USER CODE BEGIN Service1Char1_WRITE_NO_RESP_EVT */ if(p_Notification->DataTransfered.p_Payload[1] == 0x01) { // HAL_UART_Transmit_DMA(huart, pData, Size); ... here i want to insert the UART transmission funkction BSP_LED_On(LED_BLUE); LOG_INFO_APP("-- P2P APPLICATION SERVER : LED1 ON\n"); P2P_SERVER_APP_Context.LedControl.Led1 = 0x01; /* LED1 ON */ } if(p_Notification->DataTransfered.p_Payload[1] == 0x00) { BSP_LED_Off(LED_BLUE); LOG_INFO_APP("-- P2P APPLICATION SERVER : LED1 OFF\n"); P2P_SERVER_APP_Context.LedControl.Led1 = 0x00; /* LED1 OFF */ } /* USER CODE END Service1Char1_WRITE_NO_RESP_EVT */ break; In p2p_server.h are the
Using the latest SM32Cube_FW_WL_V1.3.0 and the lorawan middleware.For MAC v1.0.4 the devnonce and other parameters needs to get persisted to the flash. From what I see this happens when LmHandlerNvmDataStore is called.But from the looks of it, this is never called? I assume I am missing a file somewhere!?Any idea where and when this function is getting called?
I'm trying to program a P-Nucleo WB55 USB Dongle (PCB number MB1293C) with the BLE_TransparentModeVCP example. Using STM32 Cube Programmer: 1. Load FUS V1.20.0 - stm32wb5x_FUS_fw.bin at 0x803A0002. Load BLE Stack V1.- stm32wb5x_BLE_Stack_full_extended_fw.bin at 0x80110003. Load BLE_TransparentModeVCP_reference.hex (from P-NUCLEO-WB55.USBDongle directory) at 0x800000 I get a single green LED on the board and it appears as a COM port on the PC, but STM32CubeMonitor-RF is unable to connect to it. Any suggestions?
Hello!I am having issues with firmwares on the P-Nucleo-WB55. I started from blank code from CubeMX using AzureRTOS/ThreadX with an added layer of CMSIS and took inspiration from the HeartRateFreeRTOS sample (as it uses CMSIS too). I am currently using the BLE/ZigBee FF dynamic firmware as the project will include communication with ZB devices later on. The ZB stack is not initialized.I refactored some of the code from the sample and have been able to see all the proper exchanges on the SHCI/HCI layers being successful: getting the firmware version, enabling the C2, resetting HCI, setting the default PHY, configuring various settings (public address, IR/ER, TX power level), enabling GATT then GAP, updating the device name and appearance, setting the IO capabilities and the authentication requirements.Starting advertisement begins with `aci_gap_set_not_discoverable`, which fails (error 0xC/not allowed) as expected as the device is not discoverable by default.The next call is to `aci_gap
Hello,I am working with the STM32WB5M module and encountering an issue with Zigbee connections between the coordinator (coord) and an end device. The end device successfully reconnects and resumes communication upon waking up from the stop mode. However, if there is a power loss while the end device is in stop mode, it fails to reconnect after the power is restored. I have implemented a filter in the coordinator's code to detect disconnections, but it seems that this filter only detects disconnections when the end device is not in stop mode. When the end device is in stop mode, the filter fails to detect any disconnections. Could you provide guidance on how to ensure the end device can reliably reconnect to the coordinator after a power loss during stop mode? Any suggestions on modifying the filter or any other settings would be greatly appreciated.
I'm working on a project using the STM32WB55 Nucleo Board with the Zigbee_APS_Coord example. I need this specific example because my application communicates at the APS level and doesn't use ZCL.My application also requires a custom encryption key, and we don't use or support install codes. The system works by having the coordinator create a network with a known, configurable extended PAN ID, to which all router devices (no end devices, only routers) connect. Communication is then established using the custom encryption key.I’m providing this background because I’m unsure if I’m misconfiguring the Zigbee_APS_Coord example for my coordinator. My goal is to allow my existing non-STM32 routers to connect to the STM32WB55 Nucleo Board acting as a coordinator. If anyone has insights or can point out potential issues, I'd appreciate the help.FWIW, the routers already connect and work perfectly fine with my existing non-STM32 coordinator. I'm just trying to substitute the non-STM32 coord
The STM32WB1MMCH6TR module has a BOOT0 pin that is pulled high on the MB1868 "B-WB1M-WPAN1" board through (what appears to be) a non-populated resistor. Without this resistor the BOOT0 input to the module is floating. Does the module pull the signal down internally or is the BOOT0 input to the STM32WB15CC on the module left floating? Is there a design guide document for using the STM32WB1MM? So far I've been using the bare chip documentation and the B-WB1M-WPAN1 board as a guide. I do have the STM32WB1MMC datasheet (DS14096 - Rev 7 - August 2024) but there aren't a lot of details.
I have an unusual question. The storage temperature range for an STM32WL is stated as: -65 to +150 °C.We are looking at doing some particular tests at high temperatures for radiation exposure recovery, so some questions if anyone knows:1. If we put the chips in an oven at 140 °C, powered off, for 6 months is there a likely hood of FLASH data loss ?2. If the FLASH does lose data, I assume some factory settings could also be lost ?3. Is it possible to reprogram the factory settings and the internal ROM code if this gets messed up ?4. Would the STM32 still be accessible via the SWD interface even if the internal settings/FLASH is messed up ?
HelloWe are working on a product using the STM32WLE5JC MCU. The features a magnetic switch that generates interrupts (specifically a low to high transition) which is meant to wake up the MCU from STOP2 mode. What is the ideal way to do this? We have few free GPIO pins. Could we use any GPIO with an external interrupt or does the switch need to be connected to dedicated wakeup pin?
Hi,I am currently playing with the NUCLEO-WBA55 board with the BLE_p2pServer_ota example.During the advertising process, I got this raw data with the BLE scanner on my phone. I mean that the 0x30 is the ID for STMicroelectronics, but what is behind it? Can someone explain to me what 000010080E12AAB is?
Hello,I want to activate UART1 interrupt directly through code in STM32CubeIDE, without using the .ioc file. UART1 is already active, so I just need to add the necessary lines to enable the interrupt.In the stm32wbxx_it.c file, I defined the interrupt handler as follows:void USART1_IRQHandler(void){/* USER CODE BEGIN USART1_IRQn 0 *//* USER CODE END USART1_IRQn 0 */HAL_UART_IRQHandler(&huart1);/* USER CODE BEGIN USART1_IRQn 1 *//* USER CODE END USART1_IRQn 1 */}In the stm32wbxx_it.h library, I declared the prototype as void USART1_IRQHandler(void);. However, I am still not able to receive data using the HAL_UART_Receive_IT function.
Hi , is it possible to get the RX sensitivity of the STM32WLE5JCI6 in other LORA conditions then mentioned in the Datasheet ? our LORA parameters are:PER=1%BW= 20.8Khz to 125KhzSF= 7 to 11split RF paths for RX and TX using RF SWITCH Thank you,Viola
Hello,I am trying to use WB55 as a Zigbee device on HomeAssistant. I have made some progress so far, and I can use it as an OnOff switch on HomeAssistant and report my switch status in real-time to HomeAssistant.At first, I added WB55 to HomeAssistant and it worked very well. I modified the client to server based on the demo, so it changes the OnOff state every second, and I can see its status changes in real time on HomeAssistant. But if I restart the device, I won't see any status changes again when WB55 is reconnected to HomeAssistant. I didn't do anything in HomeAssistant, reconnecting looks completely automatic.I provided the source code I modified and its logs. I hope to receive an answer.Thank youWeng
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.