Skip to main content
ledi001
Associate III
Oct 5, 2024 10:55 AM UTC
Solved

BLE_p2pServer example with STM32WBA55 - How can i forward a payload tu UART?

Hi,

I use the BLE_p2pServer example as a basis and would like to forward the transmitted data directly to the UART1 interface. My idea would be to use here (in p2p_server_app.c) a HAL_UART_Transmit_DMA() function, but I fail to access the data due to an incorrect type conversion.

 

case P2P_SERVER_LED_C_WRITE_NO_RESP_EVT:
 /* USER CODE BEGIN Service1Char1_WRITE_NO_RESP_EVT */
 if(p_Notification->DataTransfered.p_Payload[1] == 0x01)
 {
 	// HAL_UART_Transmit_DMA(huart, pData, Size); ... here i want to insert the UART transmission funkction
 BSP_LED_On(LED_BLUE);
 LOG_INFO_APP("-- P2P APPLICATION SERVER : LED1 ON\n"); 
 P2P_SERVER_APP_Context.LedControl.Led1 = 0x01; /* LED1 ON */
 }
 if(p_Notification->DataTransfered.p_Payload[1] == 0x00)
 {
 BSP_LED_Off(LED_BLUE);
 LOG_INFO_APP("-- P2P APPLICATION SERVER : LED1 OFF\n"); 
 P2P_SERVER_APP_Context.LedControl.Led1 = 0x00; /* LED1 OFF */
 }
 /* USER CODE END Service1Char1_WRITE_NO_RESP_EVT */
 break;

 

In p2p_server.h are the typedef structures as follows:

 

typedef struct
{
 uint8_t *p_Payload;
 uint8_t Length;
} P2P_SERVER_Data_t;

typedef struct
{
 P2P_SERVER_OpcodeEvt_t EvtOpcode;
 P2P_SERVER_Data_t DataTransfered;
 uint16_t ConnectionHandle;
 uint16_t AttributeHandle;
 uint8_t ServiceInstance;
} P2P_SERVER_NotificationEvt_t;

 

Can someone tell me how I can access the data correctly?

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Oct 7, 2024 4:19 PM UTC

Hello @ledi001 

The USART1 on the BLE_p2p Server example is configured and reserved for trace and debug. I suggest you use another API to send your payload.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Oct 7, 2024 4:19 PM UTC

Hello @ledi001 

The USART1 on the BLE_p2p Server example is configured and reserved for trace and debug. I suggest you use another API to send your payload.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ledi001
ledi001Author
Associate III
Nov 1, 2024 4:36 PM UTC

Hello @STTwo-32 

now, i have implementet USART2. It seems that the example BLE_p2pServer_ota works with an operating system? For me, it is very difficult to find out where i can insert my user code.

If, for example, I want to forward certain data to a UART2 interface via DMA after a connection has been established, where is the right place to insert a HAL_UART_Tx_DMA transmission function in the code?

In the example provided, the function to check the payload is queried in the p2p_server_app.c file:

if(p_Notification->DataTransfered.p_Payload[1] == 0x01)
 {
 BSP_LED_On(LED_BLUE);
 LOG_INFO_APP("-- P2P APPLICATION SERVER : LED1 ON\n"); 
 P2P_SERVER_APP_Context.LedControl.Led1 = 0x01; /* LED1 ON */
 }
 if(p_Notification->DataTransfered.p_Payload[1] == 0x00)
 {
 BSP_LED_Off(LED_BLUE);
 LOG_INFO_APP("-- P2P APPLICATION SERVER : LED1 OFF\n"); 
 P2P_SERVER_APP_Context.LedControl.Led1 = 0x00; /* LED1 OFF */
 }

Is this the right place to insert a HAL_UART_Tx_DMA transmission function?

STTwo-32
ST Technical Moderator
Nov 1, 2024 4:41 PM UTC

Hello @ledi001 

This is a new question. 

Could you please close this post by selecting a best answer to the original post. And open a new thread on the ST Community with maximum details. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.