Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
I am a newbie in ST boards/products.I am using the NUCLEO-WL55JC board. I found an example to try. However, I can not work with it.After I open the example, I choose "Debug As: STM32 App". It is uploading the code, and the debugger connects... I can go step by step until DBG_Init() function in SystemApp_Init() function. Then, DBG_Init() tries to change my debugger pins behaviors. Then, "Target is not responding, retrying..." message appears in the console.What should I do?
..
HiMe and my team designed a custom PCB containing a STM32wb55cc and needed it to be connected with BLE with an application made by ourself. Unfortunately, even if ou board is functionning pretty well with STM apps like with STM32 BLE toolbox for Android for example, with our own app made on App Inventor we can't manage to establish a connection between our microcontroller (the server) and one of our cellphones with the app (the client). We went through a lot of topics in ST Community forum and didn't seem to see the same problem somewhere else. We also went through some workshops provided by STM over the BLE function but we didn't find any solution.If you need more details about our project feel free to ask.We hope we were clear enough about our issue.Best regards
Bluetooth Mesh Rapid Prototyping workshop using the STM32WB5MM-DK
Hi,I am using a STM32WB5MMG module and want to use FreeRTOS in combination with BLE.For ease of programming I am using CubeMX to set everything up. My goal is to have BLE up and running to be able to connect it to a Client. FreeRTOS is being used to communicate with a LTE Modem and several sensors.Currently I am stuck on getting the device to boot up properly.Without the stm_wpan part enabled in CubeMX my code is working fine, but as soon as I enable it, the code gets stuck after power up.I am basically using the BLE_HeartRateFreeRTOS example but added my code to the default taskReally appreciate any help !!Thanks in advance/* USER CODE END 4 */ /* USER CODE BEGIN Header_StartDefaultTask */ /** * @brief Function implementing the defaultTask thread. * @param argument: Not used * @retval None */ /* USER CODE END Header_StartDefaultTask */ void StartDefaultTask(void *argument) { /* USER CODE BEGIN 5 */ app(); /* Infinite loop */ for(;;) { osDelay(1); } /* USER CODE END
I followed the series of video "STM32WB Getting Started" with my P-Nucleo-WB55 board. During the 5th video "Heart Rate Monitor", I flashed the BLE_HeartRate project into my board and since this I have this message :"Target no device foundError in initializing ST-LINK device.Reason: No device found on target"I'm on Linux but I tried to do the same thing on Windows and the same error occured. I tried with an other P-Nucleo-WB55 board and I did the same manipulation and the same error occured. I let you screenshot of my errorsNow, I can't flash and run a new code on my two boards. What can I do to reset the Firmware of the board or to solve my problem whereas I can't flash any code on it ?Thank you
I just loaded version 2 of the AT slave firmware on my B-L072Z-LRWAN1 discovery kit and noticed that the current measured over JP3 which heads to the MCU oscillates between 2.5mA and 2.9 uA every 50 milliseconds. When I flashed the device with older firmware I do not see this. how do I stop this oscillation? Is this a bug in the firmware or a feature of something else?
Good Day.I have created a board and some program easily through SWD port and some struggle. The error i am getting In STM32CubeProgrammer is:---------------------------------------------08:35:51:413 : Reconnected !08:35:51:413 : Success with Time elapsed during Reconnect: 4314 ms08:35:51:413 : UPLOADING OPTION BYTES DATA ...08:35:51:414 : Bank : 0x0008:35:51:414 : Address : 0x5800402008:35:51:414 : Size : 104 Bytes08:35:51:414 : Reading data...08:35:51:414 : r ap 0 @0x58004020 0x00000068 bytes Data 0x000000AA08:35:51:414 : OPTION BYTE PROGRAMMING VERIFICATION:08:35:51:414 : Expected value for Option Byte "nSWboot0": 0x0, found: 0x108:35:51:414 : Option Byte Programming failed08:35:51:415 : Failed to set nSWboot0=0 nboot1=1 nboot0=1---------------------------------------------------------------------------------------------I am trying to load stm32wb5x_FUS_fw_1_0_2.binto start address 0x080EC000on new stm32wb55RGEven when trying to download a Hex file to program space 0x8000000---------
i'm using P-NUCLEO-WB55i try to update bootloader using stm32wb wiress stack updater.I saw the link below and set up the hardware for bootloader.https://visualgdb.com/tools/STM32WBUpdater/connecting/When I connected the usb, I could see DFU in FS Mode in Device Manager. And i saw the link below and downloaded ble stack.https://visualgdb.com/tools/STM32WBUpdater/However, an error occurred while downloading. The DFU mode is then invisible to the device manager, and ST-link is not attached.I think the bootloader was downloaded and it was erased when an error occurred.How can I get the P-NUCLEO-WB55 back to its original state?
In testing my LoRa design at 868 MHz on the STM32WL with a digitally compensated TCXO I witness a significant jump in frequency when (what I assume is) a micro-jump of the TCXO occurs. The specification rate this as maximum 300ppb which equates to worst case 260Hz.What we see is receive bit errors and CRC failures every time this jump occurs during transmission, something that does not occur when using traditional analog compensated TCXO.Presumably this has something to do with the CSS (de)modulation. What I was wondering is firstly if this is known issue, and secondly if there was some setting that may allow me to limit or filter the transmit/receive signal and improve or eliminate this effect.
Hello,I build a network that have some coordinators(FFD) and few nodes(RFD) by using;Dev-kit: STM32WB55 NucleoSW: Mac_802_15_4_FFD (from STM32Cube_FW_WB_1.11.0)I want to send a message that will be received by all nodes and all coordinators nearby. As I know it is called broadcast message. I found there are few default defines in example SWs like below in 802_15_4_mac_types.h/** @brief Defines the broadcast PAN ID */#define g_BROADCAST_PAN_ID_c 0xFFFF/** @brief Defines the broadcast PAN ID */#define g_BROADCAST_ADDRESS_c 0xFFFFBut there is no usage for these defines. Is there anything that explaining how to use broadcast message on MAC 802.15.4?Also I tried few different PAN_IDs and adresses but there is no receiving data that I sent.Thanks for any help.
I want to connect to the WB55 USB Dongle with CubeMonitor-RF to scan for my BLE peripherals.I followed the connection guide and flashed the BLE_TransparentModeVCP firmware to the dongle. I also installed the VCP driver under windows. The dongle appears as "STMicroelectronics Virtual COM Port (COM3)" in the device manager.But it still is not responding to a connection request from the CubeMonitor. Is there anything left I could have forgotten to do or set up? Do you have any advice how I will be able to finally connect to the USB dongle?
Hi,Using the P NUCLEO WB 55 with STM32WB .Encountered with below code, regarding HSE tuning, in workshop tutorial. A reference was given to An5024.This code does not exist in my example project, BLE Heart Rate RTOS, generated with STM32Cube 6.2.0 , FW_WB V1.11.0.Should I add it manually? Will this benefit my current working environment above?Code:/* 1 */ #include "otp.h" /* 2 */ #warning “Following code is valid only for P-NUCLEO-WB55 boards and should be reimplemented depending on the target HW and HSE capacitor tuning value storage location.“ OTP_ID0_t * p_otp; /* Read and use HSE_Tuning from OTP */ p_otp = (OTP_ID0_t *) OTP_Read(0); if (p_otp) { LL_RCC_HSE_SetCapacitorTuning(p_otp->hse_tuning); }
Hello,Depending on the datasheet of the STM32WB55 MCU, there is an external resistor for the oscillator circuit. In many Nucleo board schematics, it is not used. The datasheet says that the resistor is to avoid overdriving current. How can I decide that overdriving or do I have to limit the current? Does not the MCU limit the current? The schematic in the attachment is from the STM32WB Nucleo Board.Thank you,Batuhan
Hello everyone,I'm new here, but already made a few developpment on a ST32F7 chip, but now have a question about USB and virtual COM.Is it possible to use the second USB port of the NUCLEO board to make a virtual COM and manage communication with a PC ? I mean, without using STLINK USB port.If so, could you please explain how to do that, and if there are some example and application notes I can find ?Hoping someone may help me and give some recommendations.Have a nice day,KindlyPatrick
Hi everyone,Currently I am using Mac_802_15_4_FFD (Coordinator) application on STM32WB Nucleo board (FUS v1.1.2 & stm32wb5x_Mac_802_15_4_fw.bin flashed). Everything works perfectly. Nodes were connected and sends messages to coordinator succesfully.But I want to use this example on STM32WB USB Dongle. I flashed FUS v1.1.2 & stm32wb5x_Mac_802_15_4_fw.bin FWs on USB dongle and I downloaded Mac_802_15_4_FFD example on USB dongle. Seems everything working until FFD MAC APP - Association Requested step but there is no RECEIVE DATA : HELLO COORDINATOR & RECEIVE DATA : DATA FROM NODE messages on USB dongle. Seems like there is a connection problem on USB Dongle.I am suspect about it may cause from MCUs. Because there is STM32WB55RGV6 on Nucleo and there ise STM32WB55CGU6 on USB Dongle. Is flash addresses should be different for stacks?What should I do to run Mac_802_15_4_FFD application on STM32 USB dongle?
Hi everyone :)I'm at the first steps of building a Lora application with STM32WLE5C8 MCU. While using CubeMX to generate the code, and after defining the pinout of the chip, connectivity, and LORWAN in middleware, I opened the project in CudeIDE and tried to build it, I got :make: *** [makefile:79: TEST3.elf] Error 1 TEST3 C/C++ Problemregion `FLASH' overflowed by 484 bytes TEST3 C/C++ ProblemTEST3.elf section `.rodata' will not fit in region `FLASH' TEST3 C/C++ ProblemI still didn't start writing the Lora application, I wanted to make sure that the generated files are working correctly.I tried to make the same settings with STM32WLE55 (which has more flash and ram) and the building process seems to work just fine!Is there anything I can do to still be able to use the STM32WLE5C8 MCU?I'm new to STM32 MCU :D thanks a lot
In this doc searching for the keyword MSK I come across the following:"MSK and GMSK RX/TX with BR from 1.2 to 300 Kbit/s and TX only with BR from 0.1 to 1.2 Kbit/s""The (G)MSK and BPSK modems only supports transmission""The FSK modem with a bit rate above 1.2 kbps and a frequency deviation equal to a quarter of the bit rate, allows the MSK modulation to be used in both receive and transmit."" This MSK modulation is only available in transmit mode"The question is can I use GMSK for receive?
Hello All; I use an example code "Zigbee_OnOff_Client_Router" for Nucleo-STM32WB and "Zigbee_OnOff_Server_Coord" for Dongle-STM32WB when my coordinator lose then come back. My rounter can't send any message to coordinator. Could you please advice me?Thank you,Best regards.
We are designing a PCB based on the below products.We need the project files for the following boardsB-L475EIOT01A2C - Discovery boardNUCLEO-WL55JC - End nodeP-NUCLEO-LRWAN2 - GatewayWe are using Altium Designer. If the files are in different format, we can import them in to Altium. RegardsShaun Thirukonda
Hello,I would like to use a reset circuit with a push-button for STM32WB55 MCU. The datasheet of the MCU gives a diagram which is uploaded to the attachment. As I understand, I use just a push-button and a capacitor. VDD and pull-up resistor is involved internally. But, in many example schematics which is published by ST shows that there are a pull-up resistor and VDD connection externally. And sure, the circuit is connected by an active-low signal. So, I need a VDD with a pull-up resistor. The question is that whether I have to use a VDD connection with a pull-up resistor in the reset circuit or not necessary. Thank you,Batuhan
STM32WB. Code based on BLE heart rate example.Created a characteristic that supports both Read and Notification.Would like to update the characteristic value without sending a notification to the user. How can I do that?Thanks.
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.