Question
GMSK RX/TX
In this doc searching for the keyword MSK I come across the following:
"MSK and GMSK RX/TX with BR from 1.2 to 300 Kbit/s and TX only with BR from 0.1 to 1.2 Kbit/s"
"The (G)MSK and BPSK modems only supports transmission"
"The FSK modem with a bit rate above 1.2 kbps and a frequency deviation equal to a quarter of the bit rate, allows the MSK modulation to be used in both receive and transmit."
" This MSK modulation is only available in transmit mode"
The question is can I use GMSK for receive?