Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hello,We are using STM32WB15CCY6TR in our design. From Datasheet page 1 says "Available integrated passive device (IPD) companion chip for optimized matching solution (MLPF-WB-01E3)". However, the MLPF-WB-01E3 datasheet does not mention STM32WB15..So, can we use MLPF-WB-01E3 with STM32WB15CCY or is there a better solution?Thank you.
The STM32WB examples only show up on the STM apps and not on the phone or PC Bluetooth scan lists. What determines how the BLE advertises to a public like list?
..
I want to know whether any option bytes should be set before doing global erase for STM32wb chip. After the initial 0x44 and 0xBB, the device doesnt respond to global erase command (0xFFFF).
Using an STM32WB5. Using the ADC for some slow periodic measurements. Its working fine. Then added in STOP0:LL_PWR_SetPowerMode( LL_PWR_MODE_STOP0 )The ADC does not recovered on STOP exit. Value of:hadc->Instance->ISRis causing a hang in:HAL_ADC_PollForConversion() in stm32wbxx_hal_adc.cValue is 0x03 whereas before STOP mode it was 0x0F.Tried to do aHAL_ADC_DeInit()Followed by:MX_ADC1_Init()either before going into STOP mode or after. Either way results in ISR goes to 0 and still hangs. Doing a Sleep,LL_LPM_EnableSleep()instead of a STOP and ISR value is good and no hangs.Any suggestions for getting STOPx to work with ADC?
I'm using the STACK "stm32wb5x_Mac_802_15_4_fw.bin"on the STM32WB55 and in principle it works correctly.The problem is that after a few hours and after having been working correctly it seems that the cortex-M0 does not answer to the cortex M4 and I get blocked.The only way to make it work again is turning off and on the STM32WB55.I attach some code where you can see that when doing the RESET the return is MAC_ERROR instead of MAC_SUCCESS.When this error occurs I have tried to execute the functions:HAL_Init();Tune_HSE();SystemClock_Config();But it is still blocked. What can I do in this situation to unblock and start working without turning off and on the microcontroller?
In the wiki ( https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_FUS ), it is said:Interfaces that can be used to communicate with FUS are:System bootloader (USB DFU and USART): provides ready-to-use commandsSWD (FUS_Opeartor): provided by ST inside the STM32CubeProgrammer tool and offers ready-to-use commands.Userapplication on CM4: can be developed by the user based on STM32WB CubeFW examples (and in the future using Open Bootloader integrating FUS_Operator)Does the example that shows how to access FUS from user application actually exist ? I did not see any such example in STM32Cube_FW_WB_V1.13.0. or its patches (up to 1.13.3).I want to find a way to update the wireless stack in the field (no SWD, USB or UART, only our own bootloader with access to a user-accessible SD card).Best,Nicolas
Hi everybody,I want to design a custom PB for the STM32WB10 with the PCB antenna design from AN5129. As described in the document there is a keep out area for the antenna where no GND plane should be placed. My question about this:If I keep this space free for the antenna, can I place components with a GND plane outside without having a cut in PCB? Or is there any interference if I do this?The picture shows my antenna with keep out area and I want to place something left and right to this area.
I am currently working with the STM32WBMMG discovery board.Initially, I powered the board through USB STLink(CN11), and was able to download the p2pserver program. Everything works perfectly. But if I power this board using an external power 3.3V as the red box shows. I am no longer able to find the Bluetooth signal. I am sure the external power can provide enough current. Could someone please help me understand why? Thank you.
Hi, I am using VREF to calculating VDD. VDD = 3.3V but VREF = 3.0V. What wrong? (I use __LL_ADC_CALC_VREFANALOG_VOLTAGE() macro helper to calculate Vref). Does anyone have any tips what the issue might be? Thank.
Hello ST,During the provisioning in mesh network a node address assigned by PROVISIONER. which is going to be stored in LPN node memory. -----------------Debug Trace-----------BLEMesh_PbAdvLinkOpenCb - PB-ADV Link opened successfullyBLEMesh_PvnrDataInputCallback - Device Key: d4 ac c7 95 da 3c 8a 1d b7 dc d6 a0 50 3f fa a9BLEMesh_PvnrDataInputCallback - App Key: e3 c5 54 9d d1 19 bf 00 56 80 9a 54 6a 54 e1 04BLEMesh_PvnrDataInputCallback - Node Address Assigned = 3Device is provisioned by provisioner----------------------------------------------------------i want to delete this "Node Address Assigned = 3" from the LPN memory without system reset. so i can reuse this number again from provisioner side. Best RegardsDeepak Aagri
I can not find an Resource that describes the funktion of the RF Wakeup. Im using an STM32Wb5m, so a dual-core with Application and Network core. In my understanding the "RF Wakeup" is used to wakeup the network core if an signal is coming from the radio - but im not using any Power management options, so the network core should run always and should not need any wakeup. What am I missing or for what is the "RF Wakeup" clock necessary?I configure it in my example to use the BLE radio. Without this RCC Config the radio does not work. RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0}; PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RFWAKEUP; PeriphClkInitStruct.RFWakeUpClockSelection = RCC_RFWKPCLKSOURCE_LSE; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) { ret = UTILS_ERR; }
I have congigured it as picture, when i use dfu mode.I can't find usb port. When i use usb dongle, I can download well by dfu mode.
Not sure if this is the right place to post about CubeMX issues, but I'm having issues replicating the STM32WL55JC1 PingPong example. What I'm doing is trying to mimic every setting that exists in the example project (because it works), but some options are not actually changeable for me.First example is here:https://i.gyazo.com/46cebf0b8e0474d6480bd82d7e154085.pngOn the right, all visibility boxes are unchecked. But in the project I'm trying to recreate the example in, I can't uncheck any of the visibility (static) boxes. It just won't let me:https://i.gyazo.com/fdbf32a95e3c9bc8f0c5031f6c70749d.pngSecond thing is in my new project, cubemx refuses to generate any bsp files. So while in the example project I have the proper BSP files:https://i.gyazo.com/935b6558b46ce70fcf1bc5664b50d254.pngMy new project doesn't have anything:https://i.gyazo.com/8262c8d5b3e15d0a99f31d7d17be4b09.png(Notice the lack of a BSP folder)Both projects also match the SubGHz_Phy middleware section exactly:https://
Hi guys, I have any questions about OTA BLE using STM32WB.I didn't understand this area circled in red (vídeo: "STM32WB Getting Started Series: Part 7, Over-the-Air (OTA)"):1) This space of memory is used to store the new user application or new ble stack or new FUS, right? But, if the new user application has a big memory, what will happen?2) When the update happens, is the new application placed in this area circled in red and then the old application memory is deleted and then the new application is placed in memory space 0x08007000?3) Can I change the position 0x08007000? (I have the application that has 600Kb of memory and I think that It's needs to increase the memory space). 4) As I need to increase the memory, I will have to change the Magic Keyword to another memory location, is this possible?5) What will happen to the free memory (circled in red) if I change the position of the magic keyword?
I have a custom board using the STM32WB55RCV6, I am able to generate a project that advertises the correct Bluetooth name, but I cannot connect to it. I have looked at several projects online and compared my STM32CubeMX IOC file to theirs and I do not see anything that would prevent me from connecting to the device. Any help would be much appreciated.
I 'am new to STM32WL & CAN protocol interfacing! I'm currently working with the STM32CubeMX platform & some examples are given for CAN interfacing for other variants of STM32 MCUs.But there is no CAN interfacing option available in STM32WL. So I'm unable to use the respective HAL libraries.Can anyone help me, that whether STM32WL will support CAN interfacing? If so, please share the steps to follow!Thanks in advance!
Hello ST microelectronics support team.I'm developing an IOT application using the STM32WLE5CC for gas measurement. To measure the pulses I'm thinking of using the LPTIM, but I have a doubt.In topic 26.4.14 of the RM0461 reference manual, I became aware of two ways to reset the counter, synchronous and asynchronous mode. My question is what happens to the value of the counter, when the MCU undergoes a reset, for example a reset caused by the Watchdog.I understand that after undergoing a reset, the LPTIM will be unconfigured, but in case there is no interruption in the power supply to the MCU, would it be possible that after restarting, the LPTIM will be able to continue counting from the previous value?Best Regards.
Hi,Is there any side effects of changing the RF Frequency of the Lora Modem during runtime.Radio.SetChannel(RF_FREQUENCY);Can this be used to change the frequency at runtime? Thanks
It's a board I've been using for a while, and I'm struggling loading a new stack onto it.Here are the steps I've executed:1/ powercycle2/ start FUS3/ delete image4/ powercycle5/ start FUS6/ get FUS info: FUS_IDLE | FUD_NO_ERROR | Version=1.1.1.0 | stackversion=1.13.3.2 | FUS opeatorver = 3.1.07/ erase memory to load the stack (stack full basic v1.13.3.2, address @0x080D0000)8/ firmware upgrade of the stack (with verify download enabled, and first install (tested without too))9/ ERR_IMG_NOT_FOUND.The weird part is that after a firmware delete and a powercycle, the fus still report the current stack version being v1.13.3.2. However, after checking with a getfwinfo, I get the stack_type == 0. And the SFSA is 0xF4, so only the FUS is protected, leaving the whole Flash writable for the image (which has been verified!)Can you advise?
I am using the LoRa Development board B-L072Z-LRWAN1 and it has got STM32L072CZ microcontroller and want to write FUOTA service using LORAWAN
error: no stm32 target found Stlink is ok ,i can download program to another board. As manual's configuration, I configure MB1355C(P_NNUCLEO_WB55), I can't enter dfu mode. But the usb dongle is ok. So i think usb driver is ok.There is a 'FAIL.TXT' . The content is 'The interface firmware FAILED to reset/halt the target MCU'. I browsed through many posts , no body can solve. When i use stm32cubeprogrammer, the error is always ' no stm32 target find'. When i refresh stlink, note' STLINK error(DEV_CONNECT_ERR). I hold reset and download, it failed. I connect boot0 to 3.3V, it failed too.I don't how to continue. Does the chip(stm32wb55rgv6) is broken?If I confirm the chip is broken, I give it up immediately.It's too torturous:face_with_tears_of_joy: .
Hi,I have designed two PCBs that use STM32WLE5C8U6. I am experiencing range problems. The communications does not exceed 15 meters of range. What is the expected range? Below is what I use to initialize the radio. I have an R0 so that I switch between LP and HP. I tried both configurations switching the R0 for various "#define TX_OUTPUT_POWER" values in 14 - 22 range. I checked with a scope to see the RF_CTRL pin of the switch goes high while transmitting. Also I measure around 1.5V in VR_PA pin. The component values I used are the same as the LP configuration in schematic provided by ST. For antenna I used a commercially sold 433MHz spiral copper antenna, also tried a custom antenna made of wrapping a transformer coil around a cylinder.Any ideas for increasing the range is appreciated. Only a 50m range would be enough for me.Regards#define TX_OUTPUT_POWER 20 /* dBm */ #define LORA_BANDWIDTH 0 /* [0: 125 kHz, 1: 250 kHz, 2: 500 kHz, 3: Reserved] */ #define LORA_SPREADING_FA
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.