Skip to main content
Deepak.Aagri
Associate III
May 20, 2022 9:29 AM UTC
Solved

How to remove past Low Power Node(LPN) assigned address without system reset in Mesh Network?

Hello ST,

During the provisioning in mesh network a node address assigned by PROVISIONER. which is going to be stored in LPN node memory.

-----------------Debug Trace-----------

BLEMesh_PbAdvLinkOpenCb - PB-ADV Link opened successfully

BLEMesh_PvnrDataInputCallback - Device Key: d4 ac c7 95 da 3c 8a 1d b7 dc d6 a0 50 3f fa a9

BLEMesh_PvnrDataInputCallback - App Key: e3 c5 54 9d d1 19 bf 00 56 80 9a 54 6a 54 e1 04

BLEMesh_PvnrDataInputCallback - Node Address Assigned = 3

Device is provisioned by provisioner

----------------------------------------------------------

i want to delete this "Node Address Assigned = 3" from the LPN memory without system reset. so i can reuse this number again from provisioner side.

Best Regards

Deepak Aagri

This topic has been closed for replies.
Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
May 25, 2022 8:56 AM UTC

Hello,

The only way to delete the  "Node Address Assigned = 3" is to unprovisione the provisioner node and provision again the network.

Best Regards

1 reply

Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
May 25, 2022 8:56 AM UTC

Hello,

The only way to delete the  "Node Address Assigned = 3" is to unprovisione the provisioner node and provision again the network.

Best Regards