Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
I am using P-NUCLEO-LRWAN3 and I have re programmed the sensor board (NUCLEO-L073RZ + LRWAN_NS1) using the STM32CubeExpansion_LRWAN_V2.1.0.I am getting TxTimeout and JOIN FAILED and I can’t execute any AT commands?
..
Hi,I'm Using stm32wb5mm-dk with I2S mic to capture audio and using TAS2563 I'm playing the captured audio. The data from the mic is transmitted and played using DMA. Now I want to transmit the I2S mic data using BLE. I used notification method using sequencer. On the other side using python i receive the data and convert it to wav. I found that in my audio signal I'm getting noise. Can anyone help me with this or suggest a good way to do this(transmitting the mic data over BLE).Thanks in advance.
Hi, I want to develop a basic Zigbee end device.After having successfully programmed a STM32WB55 Nucleo with the example Zigbee_OnOff_Server_Distrib, I tried to use CubeIDE to setup from scratch my own device. I am unable to set CFG_DEBUG_TRACE, as it is set in the provided OnOff example.I join my .ioc project file.Why don't you provide .ioc file for each example?Thanks in advance for your answers.
Would like to update the ble stack of stm32wb55 to 1.15.Do old commands from stack 1.13 are supported?And which parameter describes the stack version:APP_DBG_MSG("Wireless Firmware version %d.%d.%d\n", WirelessInfo.VersionMajor, WirelessInfo.VersionMinor, WirelessInfo.VersionSub); APP_DBG_MSG("Wireless Firmware build %d\n", WirelessInfo.VersionReleaseType); APP_DBG_MSG("FUS version %d.%d.%d\n", WirelessInfo.FusVersionMajor, WirelessInfo.FusVersionMinor, WirelessInfo.FusVersionSub); Thanks!
I connected my STM32WB5M DK with USB DFU mode according to manual and description.When i want to read or write the opt area over the cli and i got the error:Error: OTP programming is currently not supported on MCU devices What does it mean it is currently not supported? I saw in other post it was working in other versions?
But I am not able to disconnect. Can someone please help me with how to disconnect from the server?
We made custome PCB board using STM32WB5MMG. We tried (489) BLE Security with STM32WB - 04 Simple BLE application generated from CubeMX - YouTube, and also we followed repository example too. We enabled the necessary settings which is mentioned above video but weI didn't get BLE name.
Using a sample example from your database code.Compatible with stack 1.15.0 (that is the stack I am running)STMicroelectronics ST-LINK GDB server. Version 7.1.0Copyright (c) 2022, STMicroelectronics. All rights reserved.Starting server with the following options: Persistent Mode : Disabled Logging Level : 1 Listen Port Number : 61234 Status Refresh Delay : 15s Verbose Mode : Disabled SWD Debug : Enabled InitWhile : EnabledWaiting for debugger connection...Debugger connectedWaiting for debugger connection...Debugger connectedWaiting for debugger connect
I have a board P-NucleoWB55 and I'm trying to acquire a signal with external clock, very similar to uart, I tried with usart in slave mode without succcess, I tried with spi slave without success.Now I'm trying to trigger a DMA transfer with a timer and clock source ETR.I'm following this thread but the code use old api and I don't understand how start the timer.I configured TIM2 Clock Source ETR2 and Counter Period, DMA TIM2_UP.I read the AN4666 but I don't understand very well the example.I tested this code: HAL_TIM_Base_Start(&htim2); HAL_DMA_Start_IT(&hdma_tim2_up, GPIOB->IDR, (uint32_t)buf, sizeof(buf));I receive interrupt for timer but not for dma.Thank you for suggestions
Hello Community,I have made a custom board for the LoRa application for both P2P as well as LoRaWAN modes. The reference for the RF network I referred to is "Highband High Power" from the MB170 schematic. The frequency I am making this module is EU868 and high power. Below are the images of the MB170 and my board RF network. While testing my board with Nucleo-WL55JC1 in P2P mode, the error is coming in receive mode. Also in transmission, when I transmit some message at receiving node (Nucleo-WL55JC1) RXP2P ERROR message is shown. Are there any changes in the RF network value that will give me a fruitful result?
In datasheet, pin 43 as PB0 and pin 44 as PB1. However, it is reversed on the module.
Hello,I'm trying to put the STM32WB55 into standby mode and eventually wake it up using wakeup pin 1 (PA0), but it wakes up directly after the HAL_PWR_EnterSTANDBYMode() is executed. After that, I checked the PWR->SR1 and it had BLEWUF bit set, but I don't understand why because I have enabled only WAKEUP_PIN1 source. The second core is running full BLE stack and there are no interrupt flags pending at the time when I enter standby mode. I also clear all PWR->SR1 flags before entering standby mode.Many thanks for help
I am fiddling with a STM32WB5M discovery kit.This kit includes a QuadSPI external NOR FLASH chip and i need to understand this in order to make early design choices. Could the DMA access that external FLASH memory space?I didnt try it yet, but my limited understanding of how DMA magic works is telling me it wont work because QSPI is in the way... am i wrong?is there any way to include external FLASH/RAM thats accessible by DMA?
I could not find a definite answer on the STM32WBx5 reference manual.I am setting the LPTIM to generate a periodic interrupt by configuring the ARR register, say to 1 millisecond period. Occasionally, I need to reprogram the ARR with a longer period, e.g. 2 seconds, and then I put the system in Sleep/Stop mode. On exit from sleep, I am reprogramming ARR to the original 1ms period.I seem to end up in situations where the CNT register is higher than ARR (the 1ms value), e.g. CNT=10, ARR=7, even though CNT was lower when ARR was reprogrammed. I still get the interrupt though, and CNT seems to reset at some point.This seems to become more likely with higher prescaler values (CFGR.PRESC).
Hi, I try to start a a continuous waveform (CW) from the STM32WB radio using theaci_hal_tone_start command from the DTM suite. I execute the following commands:hci_reset( );HAL_Delay( 10 );aci_hal_set_tx_power_level( 1, tx_pow );aci_hal_tone_start( RF_Channel, offset);which all return success. At that point the ble advertisements stop so it is doing something, but I do not seem to be getting the CW.Am I missing some call to eg 'activate; DTM ? Or something else I might be doing wrong ? (I looked at the PER testbench code, but did not see anything special in the start_TX function of that codebase, there the same steps are done except of course the different last call to start transmitting packets)ThanksBram
* JLink Info: Device "STM32WB55VG" selected.JLink info:------------DLL: V7.66d, compiled Jun 21 2022 17:00:22Firmware: J-Link Ultra V4 compiled Sep 24 2021 16:41:09Hardware: V4.00Feature(s) : RDI, FlashBP, FlashDL, JFlash, GDB * JLink Info: Found SW-DP with ID 0x6BA02477* JLink Info: Failed to power up DAP* JLink Info: Found SW-DP with ID 0x6BA02477* JLink Info: DPIDR: 0x6BA02477* JLink Info: CoreSight SoC-400 or earlier* JLink Info: Scanning AP map to find all available APs* JLink Info: AP[0]: Stopped AP scan as end of AP map seems to be reached* JLink Info: Iterating through AP map to find AHB-AP to use***JLink Error: Could not find core in Coresight setupError: Flash Download failed - Target DLL has been cancelledHow can I fix it?
Hi,For stm32wb flash operations we have to implement diagram described in AN5289, page 36. How about option bytes access? Do we have apply the same approach, with semaphores etc? Or we just can use regular HAL functions? Best,Mateusz
My expectation was that a pin-interrupt using EXTI will lead to wakeup times just slightly longer than the wakeup delays named in the datasheet (below 10µs), but what I see is this (falling edge on yellow finally reached the ISR on the magenta rising edge :(This was measured using an STM32WB55 waking from STOP2.How is this delay explained and can I shorten it while still using stop-mode?EDIT:I tested the reaction from standby mode via a wkup pin as well and it's even a bit faster! (different project so no reverse edges by design)
I am having similar issues with STM32WL54 with boot pin pulled up to 3.3V, it was initially working but suddenly stopped responding. I have tried connecting via a STLink using CubeProgrammer c2.12.0 and STLink Utility v4.6.0.0. Additionally, I have also tried connecting to Jlink as well but STM32 failed to connect. 12:54:42 : Error: No STM32 target found! 12:54:50 : ST-LINK SN : 53FF6D065056705449132081 12:54:50 : ST-LINK FW : V2J40S7 12:54:50 : Board : -- 12:54:50 : Voltage : 3.16VI have assumed that somehow I killed the STM32 because I can connect to another board (same hardware) with the same setup ( both Jlink and STLink v2 connects). Did anyone see similar issue and manage to find a root cause ?
Hello,I have thought to use FreeRTOS with the Bluetooth stack with STM32WB family MCU but it appears it is not possible by the STM32CubeMX if you want to build your custom service.Then, I have to use the SEQUENCER but I have no idea how to use it..... Is there any literature or manual or application note which explains how to use it? ThanksMaurizio
it's returning 0x82.Can someone please help me with this?
The datasheet of the STM32WB5MMG BLE module describes the placement of the module, as well as recommendations for the ground plane on the right side to the module:- The module should be placed in the top left corner- The ground plane should be kept free and provided with vias. My question:What influence does it have on the antenna performance if the board on which the module is mounted has a similar width like the module? I.e. that the board ends directly behind the module (on the left and right side)?Similar to this board:Other electronic components would be placed under the module in the red zone.Or like the Arduino Nano33 (but without the pins next to the module): Thank you very much :)RegardsBenjamin
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.