Skip to main content
BPeet.1
Visitor II
Jan 26, 2023 5:32 PM UTC
Question

STM32WB55: DTM/aci_hal_tone_start not activating

Hi,

I try to start a a continuous waveform (CW) from the STM32WB radio using theaci_hal_tone_start command from the DTM suite. I execute the following commands:

hci_reset( );

HAL_Delay( 10 );

aci_hal_set_tx_power_level( 1, tx_pow );

aci_hal_tone_start( RF_Channel, offset);

which all return success.

At that point the ble advertisements stop so it is doing something, but I do not seem to be getting the CW.

Am I missing some call to eg 'activate; DTM ?

Or something else I might be doing wrong ?

(I looked at the PER testbench code, but did not see anything special in the start_TX function of that codebase, there the same steps are done except of course the different last call to start transmitting packets)

Thanks

Bram

This topic has been closed for replies.