Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hello,I am using the STM32WB55 P-Nucleo dev board to try and send a data packet from the development board to a mobile app. I assume to use P2PServer for this and have figured out how to advertise and make a connection. Where I am stuck is setting up the service and characteristics to send a fixed size data packet over BLE. Can anyone help me understand how to do this? Thanks so much in advance.
The Interface of the Library (ble_mesh.h) in the STM32WPAN layer seems not up to date, some functions does not work (like BLEMesh_SetRemotePublication) and the descriptions are outdated.The return value of some functions are misleading/wrong, e.g. the function BLEMesh_SetRemotePublication() will return an MOBLE_RESULT_FAIL when the subscription and publication address of the elements are not equal, but the message will be send anyways.Is there a Debug function for the library blob except the "libBle_Mesh_CM4_GCC_DEBUG.a" file ?We would like to get the raw data the library will send for each message for example, but the debug output does not print this information.Is there an additional description only for the interface except the ble_mesh.h?Will this library blob get a rework?Thanks
We are the company Oko Icare Solutions Pvt. ltd.need WPC certifications for developing our device we are using your Bluetooth module of 511-STM32WB35CEU6A this module we have brought from mouser electronics.pls provide WPC certificates for the same.
..
Hi,I am trying to flash basic Led blinking code. During the flashing, I have seen the error which is attached with this forum. I have double checked the connections.Details of the board: LoRa-E5 Dev Board which has STM32WLE5JC.Debugger: Segger JlinkIDE: STM32CUBEIDE Please do the needful.ThanksMahesh
Regarding P/N: STM32WB55 in a WLCSP100 package:Q1: When VBAT is not in use, can I connect it to GND?Q2: When VDDA is not in use, it must be connected to VDD, but is it still requires a 10 nF + 1 μF capacitors?Q3: If VDDA is not in use, can I connect VREF+ to GND?Thanks!Nir
I'm starting to use the NUCLEO-WB55RG dev board but can only find a 'databrief'. Is there somewhere I can find a more detailed 'datasheet'? Something that shows which pins are connected to what on the board? Hopefully some address mapping as well for embedded C applications. TIA
Hello ST-Community,I have two NUCLEO64 STM32WL55JC1 development boards and am trying to get the LocalNetwork example up and running. A build can be easily generated from the LocalNetwork_Concentrator in the CubeIDE and transferred to the board. On the other hand, the LocalNetwork_Sensor shows a malfunction. The build cannot be completed successfully because the includes "demo_package_format.h" and "version.h" fail. When examining the firmware package manually, the files could not be found either.Is the error due to an incorrect procedure on my part, or were the required ST include files incorrectly not provided in the firmware package?Attached is a screenshot of the error message in the STMCubeIDE.I use the following software:STM32CubeIDE 1.11.2STM32CubeMonitor 1.5.0STM32Cube MCU Package for STM32WL series V1.3.0
Hi Guys,I have problems reading. I have followed the STM32WB Workshop on stm32wb (using mx version 5.4.0). Now i'm trying to read but all examples seem to only use notifying and writing.I have the following char created and added some default value.aci_gatt_add_char(SvcHandle, UUID_TYPE_128, &uuid16, 1, CHAR_PROP_READ | CHAR_PROP_WRITE_WITHOUT_RESP, ATTR_PERMISSION_NONE, GATT_NOTIFY_ATTRIBUTE_WRITE | GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP, 10, 0, &(AlarmThresholdHandle)); uint8_t pData[1] = {59}; aci_gatt_update_char_value(SvcHandle, AlarmThresholdHandle + 1, 0, /* charValOffset */ 1, /* charValueLen */ pData); Within server app handler it enters this case when im reading, and found the right handler. This is the part where i get lost, what to do next? I implemented the following but that does not work.case EVT_BLUE_GATT_READ_PERMIT_REQ: { aci_gatt_read_permit_req_event_rp0* attributeToRead; attributeToRead = (aci_gatt_read_
Hi, am working on a STM32WL55 solution that has both Hi power (RFO_HP) and Low power (RFO_LP) circuitry included (like that of the WL55 Nucleo PCB, either one of which is used at a time). Am at a component placement situation where the VR_PA signal line has to physically cross over RFO_HP signal line but on different layers. Would it be advisable to route the VR_PA connection from the feedback noise filter network on a separate layer cutting across the RFO_HP line, in perpendicular to each other? Components are only on one side of the board as overall finish has this limitation. Thank you.
Hi, I'm using the CM4 core to receive the data and store it in the SD card, once the FATFS only works on this core. Furthermore, I want to send this data via LoRa, but it only works on the other core (CM0Plus). How can I share this information between them? Any article or guidance is welcome. Other thing that occured to me is that I can just have the same code running in both cores (only with the respective parts). For example, activate ADC for both cores and declare the same variables and pins. Is that possible? If it is, is it worth it, or it's better to share the data between them?
Hi,I have a project where im using the STM32WB5MM-DK to develop code to act as a ble P2P client. I have the development board setup as a P2P client and the code is working fine. but when introducing the code to initialize the onboard OLED screen my Bluetooth scanning seems to not function anymore.Am I missing something with interrupts or Systicks?Any help would be much appreciated,Thanks,Chris
I would like to implement UHF transmission with QPSK modulation using the STM32WL. The required data rate is slow, so direct control of modulation may be possible if the transceiver peripheral cannot achieve it natively. Has anyone managed this, or tried it, or have any suggestions on approaches to try?
Hello,Can anyone help me on how to receive characters from STM32WB55 to the USB DONGLE as a receiver to show the ADC values. Or send the values via BLE Gatt to an android application using the inbuilt BLE services in STM32WB55.The material offered are too shallow especially the USB Dongle.Thank you.Regards,M.E
We are using STM32WB55RE in our application. we are trying to achieve ~10uA current consumption in sleep. But, 22uA(stable for 10min) immediately after entering sleep. After 10min current consumption start decreasing eventually to 14uA in next 60min. Why the current consumption start decreasing after 10min and how to achieve minimum stable current consumption immediately after entering sleep?
I have used UART example code for P-NUCLEO_WB55 board to check it's UART.Now i want to share that project to another team memberBut if i just Copy paste project folder to other file location than it gives me compilation errors of Few files missing.I have also tried to Export that project by Clicking File->Export than also i was not able to build that project.Let me know solution of this.
I am using the nucleo-WB55RG board. The problem is that it's my first time using BLE, but I don't know how to configure it to use Bluetooth as an advertising mode. I've seen a lot of data, but I don't know. Please tell me...
hello,I am using a NUCLEO-WL55JCX and I have been using the LoRaWAN_End_Node application found within the STM32Cube_FW_WL_V1.3.0 package.I would like to use the ioc file to generate a clean project and then develop a custom application.I read the readme file but it did not help me, after copying in a diectory the ioc file I open it and it creates me a project that on stm32cube is not possible to open.What are the steps I can take to handle the project properly?
Hi Guys,I'm working with a P-NUCLEO-WB55 traying to implement an OpenThread network. I'm using the latest stable software package (1.15.0) with STMCubeIDE.I found some problem browsing response from the otDnsClientBrowse function. In particular, in the callback, otDnsBrowseResponseGetServiceName return OT_ERROR_NONE but no data on the label (param. 1) is filled.I tryed to initialize all the buffer to 0 and, after the call, the data is still 0.I share the code in here to reproduce the problem:otIp6Address otLocalMLEIDAddress; void _CP_DNS_BrowseCallback(otError aError, const otDnsBrowseResponse *aResponse, void *aContext){ #define LBL_LEN 255 aError = aError; otError record_not_found = OT_ERROR_NONE; char label[LBL_LEN]; char svc_name[LBL_LEN]; uint16_t index = 0; otDnsServiceInfo s_info; otDnsBrowseResponseGetServiceName(aResponse, svc_name, LBL_LEN); if (aError == OT_ERROR_NONE){ while(otDnsBrowseResponseGetServiceInstance(aResponse,
I currently need a simple string to double/float function. For this I use atof() or strtod(). However whenever I call these functions the BLE advertisement stops and I cannot further connect to the WB.Does someone have the same problem?
I have a STM32WLC1 board with 2 processors. I would like to develop a LoRa based Project that uses both cores. However the example code of Lorawan-Endnode found here:[link removed because newest members cannot add links]uses only one core and has an annoying folder structure. CubeIDE hides the INC and src folders, displays ALL *.h files somewhere else and makes it hard to create a new .h file without bypassing the IDE and creating it in fileexplorer. Also the way the folders are structured makes it harder to work with GIT.My plan is to start a new project in cubeIDE with the STM32WLC1 selected as a project start. This gives me a skeleton with two main files. one for each core. Now i can add files and folders the way that fits my workflow. How ever the IOC is missing and i would love to be able to use it since it is the main reason for me to use cubeIDE in the first place.So basically i want to rework the Example project but with my own Folder Structure from 'scratch' but somehow load i
I'm currently having problems with the code generated by CubeMx for the RTC on my STM32WL MCU. Indeed, after generating the code and building the project, there are errors in the timer_if.c file. Each time the rtc handler is used, it says that the reference to "h" (which is the name of the handler generated by CubeMx) is unknown. The problem disapears when I rename the handler and call it "hrtc", which is the same name as the rtc handler generated in the main.c file. Does anyone know where the problem comes from?Thank you !ML
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.