Skip to main content
Taxara
Associate III
Apr 3, 2020 7:44 AM UTC
Solved

Basic ble reading for STM32WB

Hi Guys,

I have problems reading. I have followed the STM32WB Workshop on stm32wb (using mx version 5.4.0). Now i'm trying to read but all examples seem to only use notifying and writing.

I have the following char created and added some default value.

aci_gatt_add_char(SvcHandle,
 UUID_TYPE_128, &uuid16,
 1,
 CHAR_PROP_READ | CHAR_PROP_WRITE_WITHOUT_RESP,
 ATTR_PERMISSION_NONE,
 GATT_NOTIFY_ATTRIBUTE_WRITE | GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP,
 10,
 0,
 &(AlarmThresholdHandle));
 
 
 uint8_t pData[1] = {59};
 aci_gatt_update_char_value(SvcHandle,
 AlarmThresholdHandle + 1,
 0, /* charValOffset */
 1, /* charValueLen */
 pData);

    

Within server app handler it enters this case when im reading, and found the right handler. This is the part where i get lost, what to do next? I implemented the following but that does not work.

case EVT_BLUE_GATT_READ_PERMIT_REQ:
 {
 aci_gatt_read_permit_req_event_rp0* attributeToRead;
 attributeToRead = (aci_gatt_read_permit_req_event_rp0*)blue_evt->data;
 
 if(attributeToRead->Attribute_Handle == AlarmThresholdHandle + 1)
 {
 
 uint8_t pData[1] = {5};
 
 retval = aci_gatt_update_char_value(SvcHandle,
 AlarmThresholdHandle + 1,
 0, /* charValOffset */
 1, /* charValueLen */
 pData);
 
 }
 returnValue = SVCCTL_EvtAckFlowEnable;
}

Once i passed here i cant trigger any new events anymore.

I would like to see some examples of reading or get some feedback on which steps to preform to read successfully.

Thanks in advance,

This topic has been closed for replies.
JSHAR.1890
JSHAR.1890Best answer
Associate II
Apr 9, 2020 7:59 AM UTC

Read request must always be completed with

(void)aci_gatt_allow_read(read_permit_req->Connection_Handle);

 switch(event_pckt->evt)
 {
 case EVT_VENDOR:
 {
 blue_evt = (evt_blue_aci*)event_pckt->data;
 
 switch(blue_evt->ecode)
 {
 	case EVT_BLUE_GATT_READ_PERMIT_REQ:
		{
 		read_permit_req = (aci_gatt_read_permit_req_event_rp0*)blue_evt->data;
			if(read_permit_req->Attribute_Handle == (aTemplateContext.TemplateReadClientToServerCharHdle + 1))
			{			
				memset(MsgResponse, 0x22, 87);
				ReadCount++;
		 HAL_GPIO_TogglePin(LED1_GPIO_PORT, LED1_PIN);	
				(void)aci_gatt_allow_read(read_permit_req->Connection_Handle);	
				#if 1
				aci_gatt_update_char_value(aTemplateContext.TemplateSvcHdle,
				 aTemplateContext.TemplateReadClientToServerCharHdle,
				 0, /* charValOffset */
				 87, /* charValueLen */
				 (uint8_t *) MsgResponse);	
				 return_value = SVCCTL_EvtNotAck;
				#endif
			}
			break;
 	}

for example: See the code snipped below that I worked and found useful:

5 replies

Remi QUINTIN
ST Technical Moderator
Apr 9, 2020 7:47 AM UTC

​You may have a look at  the blood presure project  here:

STM32Cube_FW_WB_V1.5.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_Peripheral_Lite

The related characteristic has a READ property.

JSHAR.1890
JSHAR.1890Best answer
Associate II
Apr 9, 2020 7:59 AM UTC

Read request must always be completed with

(void)aci_gatt_allow_read(read_permit_req->Connection_Handle);

 switch(event_pckt->evt)
 {
 case EVT_VENDOR:
 {
 blue_evt = (evt_blue_aci*)event_pckt->data;
 
 switch(blue_evt->ecode)
 {
 	case EVT_BLUE_GATT_READ_PERMIT_REQ:
		{
 		read_permit_req = (aci_gatt_read_permit_req_event_rp0*)blue_evt->data;
			if(read_permit_req->Attribute_Handle == (aTemplateContext.TemplateReadClientToServerCharHdle + 1))
			{			
				memset(MsgResponse, 0x22, 87);
				ReadCount++;
		 HAL_GPIO_TogglePin(LED1_GPIO_PORT, LED1_PIN);	
				(void)aci_gatt_allow_read(read_permit_req->Connection_Handle);	
				#if 1
				aci_gatt_update_char_value(aTemplateContext.TemplateSvcHdle,
				 aTemplateContext.TemplateReadClientToServerCharHdle,
				 0, /* charValOffset */
				 87, /* charValueLen */
				 (uint8_t *) MsgResponse);	
				 return_value = SVCCTL_EvtNotAck;
				#endif
			}
			break;
 	}

for example: See the code snipped below that I worked and found useful:

Taxara
TaxaraAuthor
Associate III
Apr 9, 2020 2:01 PM UTC

Exactly where i was looking for, thanks!

MKolo.2
Associate II
Mar 1, 2023 8:25 AM UTC

Hello,

I just read your post on how to send message usi g BLE in STM32. Can you please help me know where I can include my alue so that I may be able to send using BLE. Thank you in advance.

Regards,

M.K

BScha.2
Visitor II
Nov 26, 2020 9:16 PM UTC

Thanks, thats it...... and my Problem is past now ....