Skip to main content
PMato.1
Associate II
Feb 23, 2023 8:13 PM UTC
Question

I'm using two sx1272mb2xas Lora modules, I want to create a point to point communication with stm32l0xx, but how can I get access to the compatible libriries? I have tried libraries from mbed but they show errors in my code, I need help please

..

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Feb 23, 2023 9:28 PM UTC

You can use LRWAN libraries, or the original SEMTECH ones.

I built my point-to-point based on the Ping Pong Examples, from LRWAN 1.1.3, but you're basically using the Radio library, and it's call backs via the main() loop.

https://www.st.com/en/embedded-software/i-cube-lrwan.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PMato.1
PMato.1Author
Associate II
Feb 24, 2023 5:09 AM UTC

Thank you, I actually used these libraries but everytime I copy them in my code, they bring errors, how did u add them into your project, if you could help me with the semtech libraries, the better. Thank you so much ​