Skip to main content
NirAlon
Associate III
Feb 22, 2023 1:07 PM UTC
Solved

STM32WB55 WLCSP100 Power supply connections when not in use.

Regarding P/N: STM32WB55 in a WLCSP100 package:

Q1: When VBAT is not in use, can I connect it to GND?

Q2: When VDDA is not in use, it must be connected to VDD, but is it still requires a 10 nF + 1 μF capacitors?

Q3: If VDDA is not in use, can I connect VREF+ to GND?

Thanks!

Nir

This topic has been closed for replies.
Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
Mar 1, 2023 12:14 PM UTC

Q1: VBAT to VDD

Q2: Not necessary the 10nF + 1uF

Q3: Yes, customer can connect to GND

2 replies

Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
Mar 1, 2023 12:14 PM UTC

Q1: VBAT to VDD

Q2: Not necessary the 10nF + 1uF

Q3: Yes, customer can connect to GND

NirAlon
NirAlonAuthor
Associate III
Mar 2, 2023 9:11 AM UTC

Thanks a lot!