Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
I am trying to load the p2p server example and noticed my Nucleo-WB15CC doesn't do any bluetooth communication. I can run normal user code just fine (LEDs, GPIO etc.) but CPU2 doesn't seem to do anything.When I try to start FUS, I get this:When I try to read the FUS version, I just get this:Here is the output of some STM32ProgrammerCLI commands:.\STM32_Programmer_CLI.exe -c port=SWD -fusopgetversion FUS Operator Version : v3.1.0 fusopgetversion command execution finished .\STM32_Programmer_CLI.exe -c port=SWD -fusgetstate FUS_STATE_IDLE getFUSstate command execution finished .\STM32_Programmer_CLI.exe -c port=SWD -startfus Reconnecting... Reconnected ! Error: FUS_STATE_ERR_UNKNOWN: Unknown error Error: Fus is not yet running, try again .\STM32_Programmer_CLI.exe -c port=SWD -startwirelessstack Error: FUS_STATE_ERR_UNKNOWN: Unknown error Error: startwirelessStack Operation Failure! Please, try again.\STM32_Programmer_CLI.exe -c port=SWD -fwdelete 
ACI_HAL_GET_LINK_STATUS will give an Array of link status (eight links).My question is how do I do operations on specific links of my choice?e.g., start an advertisement on a specific link. reference AN5270 -
Greetings,I have a question regarding the reference design MB1389-WL55JC-highband-E02_Schematic (https://www.st.com/content/ccc/resource/technical/layouts_and_diagrams/schematic_pack/group1/2e/e5/94/2a/d7/46/48/57/MB1389-WL55JC-highband-E02_Schematic/files/MB1389-WL55JC-highband-E02_Schematic.pdf/jcr:content/translations/en.MB1389-WL55JC-highband-E02_Schematic.pdf).The MCU has two RF outputs, one for high power and another for low power. Both outputs connect to an RF switch through identical filter schematics, but with different component values.I have a few questions. If these filters are frequency-related, why do the values differ when both ports are supposed to output the same frequency? I simulated both schematics for the 800-900MHz range (attached), and the difference is only 1 dBm.Could you please advise on why the components in each filter scheme are different?Additionally, the MCU datasheet's Sub-GHz radio characteristics section states that "All RF impedances matched using ref
(1) Are there any experience for a data exchange via bluetooth between two STM32WB1MMC-parts? (2) How can I use a STM32WB1MMC together with a STM32F411 board? Are there any experiences? (3) How can I create a data exchange between two STM32WB1MMC? (4) Are there documentations, tutorials or further sources? It is my first use of STM32WB1MMC... Thank you in advance.
Hello,I have STM32WB5MM-DK evaluation kit and I am trying to get example Zigbee_OnOff_Client_Router working. I updated FUS (v. 1.2.0) and Zigbee FFD (v.1.18.0). Example do not work, I get an error "Fatal Error" on terminal and display:[M4 APPLICATION] APP_ZIGBEE_Init[M4 APPLICATION] **********************************************************[M4 APPLICATION] WIRELESS COPROCESSOR FW:[M4 APPLICATION] VERSION ID = 1.18.0[M4 APPLICATION] **** Fatal error = ERROR Unknown (Err = 0)I debugged application and I found that error comes on this point (stm32_seq.c)/* Execute the task */TaskCb[CurrentTaskIdx]( );Any idea, what could be wrong? I tested all other zigbee examples also and all have the same error. I am using latest Stm32CubeIde.
I have a problem with my wireless stack which was fixed by unplugging and pluggin back in my NUCLEO-WB55. Everything was working well for many months, but I recently tried downloading the ST example project BLE_DataThroughput (from the STM32Cube_FW_WB_V1.18 package via the dialog in STM32CubeIDE). Since then, the program would get stuck because the Wireless stack was not started, then I tried starting the stack manually in STM32CubeProgrammer and it would start but then get stuck at getting a response from the Wireless stack. Wireless Firmware version 1.16.0 Wireless Firmware build 4 FUS version 1.2.0 >>== SHCI_SUB_EVT_CODE_READY >>== SHCI_SUB_EVT_CODE_READY - FUS_FW_RUNNING This is the output of BLE_DataThroughput first, where the FUS is running but the Wireless stack is not. Wireless Firmware version 1.16.0 Wireless Firmware build 4 FUS version 1.2.0 >>== SHCI_SUB_EVT_CODE_READY >>== WIRELESS_FW_RUNNING >>== DBGMCU_GetRe
We are using B-L072Z-LRWAN1 Discovery kit for testing the range of LORA network. We have purchased 2 numbers of B-L072Z-LRWAN1 Discovery kits. We are using the factory default firmware provided with the kits. We have observed that the kits can communicate with each other only upto 100 meters. But as per the kits datasheet, we should get ranges of up to a dozen kilometers. We are testing the devices in city environment.Are we doing anything wrong?Is there any way to get the range as specified in the kit datasheets (over ranges of up to a dozen kilometers)?Kit 1 is powered with USB connector CN7.Kit 2 is powered with three AA 1.5V batteries. (SB37 removed to release the RESET).
I am a new developer on STM32WB10 and I do not succeed to drastically decrease power consumption in standby mode. Commands for main CPU in order to lower consumption seems to be OK but the CPU2 for BLE seems to be always active.LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN) does not work while CPU2 is running but I cannot find the way to stop the CPU2. I read that hci_reset could help but it is not the case.Please help me about the sequence to use in order to properly stop CPU2 and decrease power consumption.
Hello everyone,I'm seeking your guidance regarding the substitution of 0402 inductors with 0603 in the NUCLEO-WL5JC MB1389 high band schematics (https://www.st.com/resource/en/schematic_pack/mb1389-wl55jc-highband-e02_schematic.pdf). In the RF section of the schematics, there are 0402 (highlighted in Red inside attached sheet) power inductors from Murata. I have chosen the replacement in 0603 (highlighted Blue) accordingly. However, only two inductors have slightly lower specifications (highlighted in gray-red). I would appreciate your advice on whether the specifications of the selected inductor would be suitable for this application. (LQW15AN3N6C10 -> LQW18AN3N6D00 and LQW15AN3N0B00 -> LQW18AN3N0C8ZD)
Hello,I am using STM32WB55RW (MCU) + muRata module(LBAD0XX1SC-DM) in my custom HW.X-CUBE-CELLULAR expansion package is available for STM32Cube but its contain example project for L4 series (STM32L462REY6TR).Can you please share sample code if anyone has done with WB55 series?OrAny guide/note like how to convert L4 series example for WB55? Thanks.
When I run the application, all three LEDs are toggling in cyclic fashion and according to the note, this is an error condition. I checked the message from serial port and I am getting the following[0m[M4 APPLICATION] WIRELESS COPROCESSOR FW:[0m[M4 APPLICATION] VERSION ID = 1.12.0[0m[M4 APPLICATION] **** Fatal error = ERROR Unknown (Err = 0)What could have gone wrong? Also, is there any way the application can know what RF stack is currently loaded into the M0 controller. Thank you for your time.
Hello,during testing Zigbee_OnOff_Client_SED example, hard fault in time of joining network happen, when logging with ZB_LOG_MASK_LEVEL_3 or higher is configured. With ZB_LOG_MASK_LEVEL_2 or lower example works fine.Hard fault analyzer report PRECISERR with BFAR 0x280027. Origin seems to be in the ZbLogPrintf (see attached screenshot with stack). Because it's library, it's out of my range. Depth, lqi, pjoin values are reported weird. See next log. Any suggestion, except keeping log mask level low?Thanks, Slavomir Tomascik ZIGBEE Application Init StackLayers Init (startupMode = 3) Adding endpoint 17 (0x11), profile = 0x0104, mem = 108 ********************************************************** Network config : CENTRALIZED END DEVICE Application Flashed : Zigbee OnOff Client . Channel used: 14. Link Key: ZigBeeAlliance09 Link Key value: 5a 69 67 42 65 65 41 6c 6c 69 61 6e 63 65 30 39 Zigbee Extended Address : 0x000000000000000lX Clusters allocated are: OnOff Client on Endpoint
Hi,I'm having an error after powering the MCU, it looks like the CPU2 with the BLE stack it's not restarting.The error occurs when I stop advertising, the BLE status is APP_BLE_IDLE and I turn off the board.When I power-up the board and do the BLE initialization process, the CPU2 looks like it's not answering to the commands. If a software reset occurs with BLE status equal to APP_BLE_IDLE, the systems starts correctly. How can I tell the CPU2 to reset?Best,Pablo
Hello, testing Zigbee_OnOff_Client_SED on P-NUCLEO-WB55. Sources are from version 1.18.0, same as installed stm32wb5x_Zigbee_FFD_fw.bin. Almost no changes to source files except modification channelmask to WPAN_CHANNELMASK_2400MHZ.After a while (random inteval) device send following debug message, and device can't find network anymore:[M0] [0;92m[00007009.694][LLD] !! ip802154_lld_exitSleep() FAILED : LLD state before 2 - time before 2714719056 - sleepTimeStatus 1 - wakeUpStatus 149 - default state after 99 (1) - LLD state after 2 Does anybody have a clue? Any suggestion?Thanks. More from log file:[0;92m [M0] [0;92m[00006358.738][PLATFORM] nwk_scan_req : MLME-SCAN.request (wpan0): type=1, page=0, mask=0x07fff800, dur=4[0;92m [M0] [0;92m[00006362.963][PLATFORM] nwk_handle_scan_conf_rejoin : Error, could not find a parent to rejoin.[0;92m [M0] [0;92m[00006641.946][PLATFORM] nwk_dataconf_watchdog_timer : Error, never received MCPS-DA
Hello, I would like you to help me to communicate two microcontrollers (The B-L072Z-LRWAN1 Discovery kit LoRa/Sigfox module (Murata) using Lorawan, I was researching and looking at some libraries that were an expansion for Lorawan. But I don't know how to use them. I was trying to get the USART to work but I couldn't get it to transmit information. I don't know if anyone knows where I can start. Also if I need to use the libraries to communicate the microprocessors or if I can communicate without using the libraries, thanks.
Hello,Can someone tell if BLE stack in STM32WB chipset support QUUPPA application ? I expect it is the case for the latest STM32WBA?Thanks
Hey, everybody!I looked at the Release Notes for the STM32WBxx Copro Wireless Binaries and kind of did everything according to the manual.stm32wb5x_FUS_fw.bin -> 0x0809A000, tm32wb5x_Zigbee_FFD... -> 0x0804C000. However, after flashing the controller behaves unstable and sometimes shows FUS_ERROR, FUS_NOT_RUNNING. And after a repeated attempt to read FUS everything normalizes. Then I tried to use the example ZigBee_OnOff_Server_Coord, but nothing is transmitted via UART and there is no connection with the working Nucleo STM32WB55RGV6. The channels are set up correctly and I think it's ZigBee not working and I messed up something with the FUS. Also WB Commands are now unavailable to me.
Hi,it is ok to call hci_user_evt_proc function (STM32WB), from an interrupt, for example SysTick_Handler ?Best,s.mateusz
Hi all,Im trying to load the stack onto the custom board. I've done it for both Nucleo board and dongle. I use Nucleo board with SWCLK, SWDD, RST, GND, 3V3. I think Ive managed to program FUS as it shows the correct number and it starts. Ive been trying to program the stack for a long time, with different configuration, but no luck. Every single time it is unsuccessful. A weird thing is that it shows the stack number 1.18 but Im almost 100% that it wasn't successful. I have followed the tutorials, datasheets, yt videos and nothing. I can program that mcu, it blinks leds etc. But I cant use Zigbee. Please, help me.
Hello, I'm Marco, HW developer.Scenario: two Nucleo WB15CC transmit both a sawtooth into the Nucleo WB55 USB dongle with BLE protocol. With a proper SW we can see the two sawtooth in the GUI. The Nucleos WB15 should be replaced with custom HW with small size and few components.Omitting details I can say the HW is not working with the same firmware, so I need to test the HW in other way.Can you suggest me something to test BLE transmission and if the mcu is running?The firmware is written with Keil and debug is not running properly for some reason, and I don't have enough SW skills, so I need a more simple way to see if mcu is transmitting data.Thanks
Hello guys, I have this situation where when I use the LoRa protocol in my application, the RTC stops working and vice-versa. Anyone have an idea of what could be causing it and the solution for the problem?
I'm working on a BLE application which uses a pair of BLE characteristics to transfer packets of data (similar to a cable replacement service). I believe I have followed the recommendations in AN5289 8.6.9 to mazimize throughput.When I read packets from the STM32WB device from a PC, using the 1M PHY, I get a transfer rate of about 40 kB/s, which seems pretty good. Looking at the transfer in Wireshark, I get the capture attached here as "read.7z".However, when I write packets to the STM32WB device from a PC, I get a transfer rate of about 2 kB/s. The Wireshark capture for this transfer is attached as "write.7z".On the central side, I'm using a TP-Link USB500 Bluetooth adapter and a Python script using Bleak for the BLE interface. I've run the script both on Windows 10 and on Ubuntu 22.04 with the same results.On the device side, I'm using an STM32WB5MMG with a custom CRS profile.Looking at messages when the connection is being established, the adapter requests an MTU of 527, and the STM
Hi there, I explored the attribute reporting topic based on my initial question, which you can find here: [link]. I gained a better understanding of how the feature operates.Currently, in my setup, the Client pretends to be a Zigbee End device, and the Server acts as a Zigbee Coordinator with simulated or dummy RMS Voltage and Current values. I've configured Attribute Reporting on the End Device side (Client). So, whenever there's a change in attributes on the Server side (Coordinator), it reports to the Client. (Check the attachments for the Client and Server applications.) #1 Objective:My goal is to have the Zigbee Coordinator (acting as the Client) fetch Voltage and Current attribute data from the Zigbee End device (acting as the Server). Despite trying various combinations, I faced challenges and haven't succeeded.I would be grateful if you could take a look at my attachments and offer suggestions on how to move forward to accomplish #1. Could you also pr
Hello , I'm using the Nucleo-WL55JC1 in my project as Gateway and End-devices.The SW Works well and it communicate properly, but i have problem with the RANGE between the Gateway and the End-device.Know when I change the Antenna I can communicate with 300metres as range , but i like to achieve more distances like 1Km or +Actual SW Params :SP = 12TxPower = 22dbBandwidth = 125khz.How can I increase the range , in SW or HW side ?Thank you in advance.
Hello,I'm interested in using one of the STM32WL chips for a telemetry board. I need this board to be as small as reasonably possible. I am trying to decide on a way to program it and (optionally) have a way for it to connect to a laptop via usb. Ideally, I would be able to use on USB port for both firmware updates and serial communication, but it appears that the STM32WLE5C8U6 doesn't support DFU. What would be the most optimal (spacewise) solution to both program and USB interface with the STM32WLE5C8U6? I am fine adding a USB to UART or any other necessary chips. Also, what is the most compact solution for only exposing a programming interface (no USB needed) / what is the minimum surface area needed to be able to program the chip using the STLINK?
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.