Question
B-L072Z-LRWAN1 Discovery kit lora range issue. Range of less than 100 meters.
We are using B-L072Z-LRWAN1 Discovery kit for testing the range of LORA network. We have purchased 2 numbers of B-L072Z-LRWAN1 Discovery kits. We are using the factory default firmware provided with the kits. We have observed that the kits can communicate with each other only upto 100 meters. But as per the kits datasheet, we should get ranges of up to a dozen kilometers. We are testing the devices in city environment.
Are we doing anything wrong?
Is there any way to get the range as specified in the kit datasheets (over ranges of up to a dozen kilometers)?
- Kit 1 is powered with USB connector CN7.
- Kit 2 is powered with three AA 1.5V batteries. (SB37 removed to release the RESET).