Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hello Developers, In our product, we currently have a RAK3172 module interfaced with STM32L4 controller. I am able to use both LoRa P2P and LoRaWAN communication using the AT command sent to the RAK chipset from host, through UART interface. Now i would also like to add sigfox functionality in my application. But by default RAK3172 chipset doesn't support Sigfox. So for adding sigfox functionality, i have to port the stm32wl AT Slave example for RAK3172 and add the AT commands for LoRa communication firstly, as AT Slave doesn't provide AT cmd for LoRa communication. So currently i am stuck, thinking where my AT cmds for P2P/LoRaWAN recieved by RAK module (STM32WLE) will be stored such that RAK perform the desired AT cmd task. Is there any register where it's written ? I would like to have better understanding of how i can add command like that of RAK in AT Slave example and the module executes it properly.
I do everything as decribled here:-stm32u5 program with ble at client code-on stm32wb I update fus, stack and program BLE_AT_Server_reference.hex from STM32Cube_FW_WB_V1.17.0When i try run app @teraterm i see:Start of the STM32WB5M module AT example.Run ST BLE sensor application on your smartphone and connect to you device.Press user button:- once to notify a value.- twice to toggle the BLE service.--------------------------------------------TX: ATRX: OKTX: AT+BLE_SVC=1RX: OKBut my iphone ST BLE Sensor app(i also try android) dont find any device, i don't know why, I also try ST Ble Sensor Classic app and this don't help (I don't know which one i should use).
Hi team, Warm GreetingsI am using STM32WB55RG6VTR controller in our battery operated product development. We are enabling the sleep mode in the controller to test the current which is around 10mA but it is supposed to be around 40uA if all peripherals are enabled. Moreover, our requirement is to have the sleep current less than 10uA.So, I would like you guys to give us some suggestions on the maintaining the specified sleep current mentioned in the datasheet and also options to disable the in-Built SMPS Power to reduce the overall current consumption in sleep mode of the controller.PFA of the test code Zip file for your reference.Your quick response to this query would be highly appreciated. Thanks & regardsDarshan R
Hi all,I have a setup where many devices need to to respond to a message on 868MHz from a sender. At the moment I am using random delay to space the responses but I will like to use the RadioIsChannelFree() function.Do anyone use this function? Is it a recommended way for avoiding transmission collision and if so are there good example on how to properly utilize this function?Ola
Hello community,Currently, I have Lorawan gateway: p-nucleo-LRWAN1 and Lorawan node: B-L072Z LRWAN1.I'm looking forward to suggestions from you, which company gateway and node will be better than this current gateway and node. with current devices, I'm facing data rate as well as long-distance communication. In the current node when I fill a 242-byte buffer and try to transmit data it only transmits data at SF7 and SF8 and not at SF9,10,11,12. At this SF I'm getting empty packets. And at distance of 50 meters only from gateway SF turns from 7 to 12.Thank you.
I encounter the following error when connecting STM32WB15 to ST-Link V2.Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authenticationonly VDD,GND, and SWIO and SWCLK pins connected..package is ..UFQFPN48what is problem..?
Hello,I have been getting into BLE applications with the stm32wb55 nucleo development board. I am currently developing my application over the BLE p2pServer app. I have modified the program such that the P2PS_Send_notification() method keeps sending a sensor data in a loop. however when i measure the data rate, it is somewhere around 4500bytes/sec. This was consistent with the results I got when I tested the Data Throughput app, and when i pressed SW2 the data throughput changed to around 40000 bytes/sec (these values are still way lower that what other people have experienced but I will get to that later as 40000 bytes/sec is good enough for me at the moment). However, when I tried to change the PHY to 2M on my application, the results were exactly the same. The wireless stack version is 1.18.03 and I have followed all steps mentioned in AN5289 section 7.8 and section 8.6.9 but nothing worked for me and my data rate is still at around 4500 bytes/sec. Any help would be greatly apprecia
Hello everybody, I am currently building a STM32 BLE software and in this software I got a very long custom loop. My problem is I want to continously check whether there is data received with BLE, if there is, process the data, and return to main loop. How can I do that? Sincerely,Yusuf.
Hi, I'm developing a BLE P2P application to exchange data. I have encountered a problem while debugging. The status for the BLE when turn on is APP_BLE_FAST_ADV, but when I restart the debug sessions the status is APP_BLE_IDLE. It looks like the CPU2 and th stack it is not restarting with the debug restart session, only when power up. When I'm not debugging the application, it works well, I can scan the BLE device. But, when I want to restart the BLE discovering process (due to scan timeout, or I have canceled the discover process), it is not working, the status reamains as APP_BLE_IDLE. Thanks,Pablo
Hi! :waving_hand:I have programmed a STM32WB5MMG with the SBSFU + OTA + User app. The SBSFU is able to start the user app with no problem, and the user app is able to start the OTA app.The problem comes when starting the update process. With STM32CubeMonitorRF there is no problem: the device is updated to the new version of the user app. However, when the operation is performed with the ST BLE Sensor app (iOS), the image is sent (100%), but the OTA does not restart to install the new user app and the 100% message does not disappear from the mobile app.With the normal OTA (without SBSU) I have been able to update the versions of the user app with the mobile application.My question is if STM32CubeMonitorRF and the mobile application ST BLE Sensor manage differently the OTA procedure (if so, to know these differences to be able to implement them in our mobile application where the updates will be done in production), or if it is a bug of the mobile app when managing sfb files.Best regards
Hello,We are using STM32WB55CEU6 in one of our project and we are facing the issue in BLE. We checked all the powers and soldering related things, everything looks fine. But BLE is not able to advertise.Also, from the firmware side the same code is working in Nucleo board.We used 2450AT18B0100001E Antenna and DEA162450BT-1298A1 Filter.Let me know if the Circuit has any issue.Below I am attaching the Schematic File for MCU section.Thank You.
Hi,I just want to know whether STM32WB5MMG module supports LE Audio since it has Bluetooth LE 5.4. If it supports can anyone help how to do it.Thanks and Regards,LR.2
I use STM32WB sample code to build project and need to know BLE client address from BLE server during connecting request. if is possible, could you please point me what API or data structure I can study. thank you.best regards,Langston
Hi :) I am trying to port the Bluetooth Firmware of B-L475E-IOT01A STM32L4 Discovery Kit provided by ST to BlueNRG-M2SA BLE Module. But failing to communicate. Is firmware compatible across both Bluetooth Modules?
I am using STM32wl55jc1 nucleo board using subghz_phy_per application provided by "en.stm32cubewl-v1-3-0 SDk" using FSK Trying to communicate with efr32fg23 silabs rf module withe same rf freq is this communication is possiable if yes recommend any configuratuons/applications. Thank You
Hello,I am using STM32WB55RE (MCU) in my custom HW and sdk "STM32Cube_FW_WB_V1.16.0".I want to get debug log using SWD. (I am using ST-LINK/V2)I have created test project for testing swd logging.I followed below video link while creating test project.Link: https://www.youtube.com/watch?v=Efgp34LbkLUCan you please check my project configuration? and help me to fix it.Thanks,
Hello, I'm trying to use STM32WLE5CCU6 MCU as a radio module transceiver.I have followed the MB1874_LowPower reference design down to it's 0.7 mm substrate thickness.I connected the internal MCU RF power supply pins required like in the reference design and made sure i connected both of oscillators. I made sure to connect the necessary solder jumpers as well especially for the internal power supplies.However I can't seem to be able to run the MCU as neither a transmitter or receiver. But when the program reaches the line of code Radio.Rx() I can not communicate with MCU anymore via STM32 debugger. So I can't run my MCU with this program.How do I fix this problem? Any help is appreciated.
HI Madam Sir, Had anyone tried to port the cable replacement sample included in the Firmware package to STM32WB55CC? This MCU has different pins and FLASH sizes.Thank you.Ian C Mosquera
Hello!I'm currently trying to get two B-U585I-IOT02A (STM32U585AI) boards to communicate with UART over BLE. I'm using the BLE_CableReplacement example project (STM32Cube_FW_WB_V1.13.3/Projects/P-NUCLEO-WB55.Nucleo/Applications/BLE/BLE_CableReplacement) as a starting point, as these boards are essentially supposed to replace physical communication wires. The STM32U585AI boards have a STM32WB5MMG Bluetooth module on-board, but I have not been able to find a way to flash the wireless coprocessor binaries onto it. The release notes do not include procedures for flashing the STM32U585AI boards. I'm also missing the Firmware Upgrade Services button on the left-hand menu of the STM32CubeProgrammer GUI despite being updated to the latest STM32CubeProgrammer version. I apologize in advance if these are novice-level questions - I've only just started using the STM32 ecosystem (~1-2 weeks at this point), so thank you for bearing with me!To summarize, here are the questions I have:How do I flash
I have an STM32WB design using I2C to get 6 bytes from a BMI0888 every 50ms (triggered by an external interrupt). The interrupt sets a flag in my main loop to go get the data. The devices first requires you to write the desired register, then read the 6 bytes. If I use back to back calls to HAL_I2C_Master_Transmit followed by HAL_I2C_Master_Receive, it works great. See figure 1 below. That will happen every 50ms. I am now trying to do this using the interrupt versions of the functions. If I try and use HAL_I2C_Master_Transmit_IT and HAL_I2C_Master_Transmit_IT. I again use flags to inform my main loop what to do. The external interrupt flags the loop to perform the transmit, then the HAL_I2C_MasterTxCpltCallback informs the main loop to perform the receive, and then HAL_I2C_MasterRxCpltCallback tells the main loop the data is ready. I get all of these interrupts, however the data isn't actually read
Hello,I want to be able to perform OTA updates of nodes in a bluetooth mesh network. Therefore I want to add a service and a characteristic to the existing BLE connection between a proxy node and a smartphone/PC. Currently, only the mesh provisioning service (UUID 0x1827) is present on the STM32WB using the example program BLE_MeshLightingPRFNode for the STM32WB55.Could you please provide some guidance on how to add an additional characteristic to a BLE connection of a mesh node?I've tried to add an additional service using the functions aci_gatt_add_service(...) and aci_gatt_add_char(...) to add a characteristic. I've tested calling these functions from different places in the program flow. Calling these functions before MESH_Init(...) in Middlewares/.../mesh.c or after MESH_Init(...) both didn't work. If someone has a suggestion how to do it, I would be very grateful. Thanks
Curious regarding using ACI_GAP_SET_AUTHENTICATION_REQUIREMENT to change the fixed pin after already using a different pin key for a previous connection. Would that work? Any bad consequences?
Hi can MCU STM32WL33 - QFN32 work with the balun BALF-SPI-01D3? Where can I find the solution on 2-layer PCB (for 868MHz)? // for Antenna johanson 0868AT43.. regards zbyno
Hello community, I am trying to read a characteristic before each advertisement on BlueNRG-2 devboard. I started from the example BLE_Sensor_Demo, I adapted the services and characteristics. I want to use a characteristic as a flag. When characteristic is 1, I send data in my eddystone advertisement payload, when 0, I don't. For this, I need to read the characteristic before advertising. I guess I need to do that in my App_Tick, but I don't know with what function. Can someone give me support please ? Gaétan
I created a custom application using the code from the BLE_THREAD_DYN example and the v10.0 FW BLE_THREAD_DYN stack. The BLE works fine but the thread stack goes down after a few minutes. The main differences between my code and the example is that I converted the code to use FreeRTOS but I preserved most of the logic and structure. Upon initial system power on, the stacks both initialize and go up just fine with the device meshing with my existing thread network. However, after a few minutes the device disconnects from the thread network and the node never reconnects but the BLE remains active. I'm troubleshooting the issue but any breadcrumbs on how to converge on the problem more quickly would be much appreciated. Update 3/3/2021 @ 1:50PMWithin the initialization of both stacks, I commented out the BLE initialization and only ran with the Thread stack active using the v10.0 BLE_THREAD_DYN firmware. The issue persisted with the Thread stack going down after a few minutes -- the amoun
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.