Skip to main content
Associate
Feb 5, 2024 3:18 PM UTC
Solved

STM32WB15 cannot connect stlink v2

I encounter the following error when connecting STM32WB15 to ST-Link V2.

Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

only VDD,GND, and SWIO and SWCLK pins connected..

package is ..UFQFPN48

what is problem..?

 

This topic has been closed for replies.
ErdinccaBest answer
Associate
Feb 13, 2024 5:58 AM UTC

i solved this problem... Proble is SW Fequency... Low frequency is working..

Thanks..

6 replies

TDK
Feb 5, 2024 3:35 PM UTC
  • Is this a custom board?
  • Are you using STM32CubeProgrammer? Does it output the target voltage? Is that voltage as expected?
  • Are you using a genuine programmer? Link to it.
"If you feel a post has answered your question, please click ""Accept as Solution""."
ErdinccaAuthor
Associate
Feb 6, 2024 5:46 AM UTC

yes customboard. i use stm32cubeprogrammer. output voltage 3.3v. original stlink v2 use.. 

TDK
Feb 6, 2024 2:31 PM UTC

Perhaps a schematic error. Perhaps a hardware error.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
Feb 5, 2024 3:49 PM UTC

@Erdincca wrote:

If your product embeds Debug Authentication,


Does it?

If 'yes':

 


@Erdincca wrote:

please perform a discovery using Debug Authentication


did you do that?

 


@Erdincca wrote:

only VDD,GND, and SWIO and SWCLK pins connected..


Have you tried adding Reset?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ErdinccaAuthorBest answer
Associate
Feb 13, 2024 5:58 AM UTC

i solved this problem... Proble is SW Fequency... Low frequency is working..

Thanks..

Andrew Neil
Super User
Feb 13, 2024 9:14 AM UTC

@Erdincca  Good to hear it's solved.

Now please mark the solution - so that others who come here with the same problem can find it.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.