Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
STM32WB55RGV MCU is in use, and BLE_HeartRateFreeRTOS example is under review. In the example of BLE_HeartRateFreeRTOS, it was confirmed that the STOP2 mode function was included, but I don't know the Stop mode entry conditions.And I wonder if I can set the BLE ad timeout in the BLE_HeartRateFreeRTOS example.Or let me know if you have any documentation that explains this example in detail...This is because I want to know information such as current consumption in STOP2 mode.
I am using the p-nucelo-lrwan3 and I have been using the i-cube-wl project and i did some changes to the region and to the activation mode but it doesn't join the network can any body help me with it
I'm trying to create a new ZigBee network frame for STM32WB55RG Zigbee 3 and DIGI Zigbee 3, but it's not working,My request is :How to configure Zigbee network step by stepHow to set unique PAN-IDHow to set 64 bit MAC addressHow to send and Received data thought ZigBee 3
Hi, I am trying to measure the power consumption of my NUCLEO-WL55JC2.In the user manual here Is what I found : Jumper JP1, labeled I_SoC, is used to measure the STM32WL microcontroller consumption by removing thejumper and by connecting an ammeter. Their location in the power structure is shown in Figure 19.JP1 ON. STM32WL is powered with 3V3 voltage (default)JP4 OFF. An ammeter must be connected to measure the STM32WL current. If there is no ammeter, the STM32 is not powered. Normally, only one jumper is used to connect the ammeter. However, when I try to put connect an ammeter in the JP1 or JP4 I don't see any current and can't run my code in the stm32cubeIDE.Does anyone have an idea of where should I connect the ammeter and how to proceed?Thanks for your time
Hello ST community, I am leading a project at university and I would like to make a communication between two STM32WL55JC1 cards using the LoRa protocol without a gateway. I'm not very familiar with STM32CubeIDE and any help would be much appreciated.The aim is to recover data from an accelerometer that will be transmitted by a serial communication to the first STM32 card and then make a wireless communication to recover the data on the other card. First of all, I would like to know if I can make a communication between two LoRa device without using a gateway. Thanks for your answers. Jules.
Good morning,I am building a system with stm32 wl55jc1 to count water flow with a pulse flow meter.So I created two internal clocks in stm32 one to create a time window and the other that counts each pulse received from the sensor. At the trigger of the first clock I check how many pulses the second clock counted and get the instantaneous flow rate.I put an LED in parallel with the signal to visually see the pulses. The problem is that the count the clock makes and the pulses I see do not match.I would like to ask for some documentation on the input voltage and so that I can design my RC circuit as best I can (as I am convinced that the problem is electrical). thanks for your time, greetings Roberto
I have been getting warnings similar to the following when I link with LinkLayer_BLE_Full_lib.a and stm32wba_ble_stack_full.a. output.axf is the executable elf file. objdump is from Ubuntu 23. objdump -g 'output.axf' > 1.txtobjdump: Warning: Invalid length 0xc000000 in FDE at 0x30cadThe PDE problem causes a problem with Segger Ozone. It is unable to unwind the call stack and warns "ELF data section 'debug.frame' has an unexpected byte size".I don't get the warnings when I use LinkLayer_BLE_Basic_lib.a and stm32wba_ble_stack_basic.a. Ozone doesn't have an unwinding problem with the basic versions.Is there a known way to use LinkLayer_BLE_Full_lib.a and stm32wba_ble_stack_full.a without causing an invalid FDE.I am using STM32Cube_FW_WBA_V1.2.0, Nucleo-WBA52CG, Ubuntu 23, and arm-gnu-toolchain-13.2.Rel1-x86_64-arm-none-eabi.
Hi A previous version of a product used STM32G071x8/xB in conjunction with external radio transceiver (SPSGRF-915). The team has used SPIRIT middle ware for radio functions. A newer version has migrated to STM32WLE5/E4xx which has inbuilt radio and I see collateral on ST website usong Sub_GHZ radio middleware Is there a way SPIRIT can be used directly on the new STM32WL MCU ? ThanksPavitra
Hi,I am using aSTM32WB55Wireless Firmware version 1.17.2Wireless Firmware build 1FUS version 1.2.0As described by AN5270 2.5.6. an ACI_GATT_UPDATE_CHAR_VALUE must fire an ACI_GATT_NOTIFICATION_COMPLETE_EVENT if the characteristic was created with GATT_NOTIFY_NOTIFICATION_COMPLETION mask.I am using the BLE_Custom example to which I added a service. I could not find any setting to enable this notification with CubeMX at the STM32_WPAN section.I added the mask manually, but I never got this event!The function aci_gatt_notification_complete_event_process (defined in ble_events.c) was never called as well.I need to send multiple indications and I want to use this event to determine when the next indication can be sent.I receive an ACI_GATT_SERVER_CONFIRMATION_EVENT but in this case the parameter is a connection handle instead of a handle to a characteristic. What do I have to do to receive the ACI_GATT_NOTIFICATION_COMPLETE_EVENT?Best regards,Christian
In my design I left the exposed pad in Stm32wb55rg VFQFN68 package. when I try to flash the device using st link , iam getting error "target not found". I am check the design and found i left the epad (69th pin) floating. Does this cause any issue ?. Please help me out here .thanks @Amel NASRI .
I am attempting to use the https://github.com/stm32-hotspot/stm32wb-matter-device-over-thread/ repo to connect a STM32WB5MMG-DK to an Amazon Alexa acting as a border router, using the Alexa app. The device always fails to connect, outputting the serial log that I have attached. I am using the recommended firmware (stm32wb5x_BLE_Thread_ForMatter_fw.bin)I have also been unable to commission using the CHIP-TOOL and Raspberry Pi 5 border router.
Hi,I have made an application on that needs to enter shutdown/standby mode on the STM32WB10 MCU.I have successfully made it enter the shutdown mode, and I can wake it back up again.However, when it wakes up, it does not get any response from CPU2.It is as if the task "shci_user_evt_proc" is never called in a way that allows it to call "APPE_SysUserEvtRx()" in app_entry.cAs a result I only have Bluetooth when the MCU is started the first time from a power cycle. The current version of my application enters standby/shutdown after 10s of no user interaction.After wakeup, it enters HardFault_Handler() when it attempts to enter shutdown again.This happens when it attempts to send the command for disabeling the advertising (which i suspect is obvious, since the CPU2 is not responsive).Below is a screenshot of the stacktrace and the line that causes the hard fault.I suspect this is caused by my code not doing something the way it should, but I cannot figure out what it should do, or when
Hello! We are a bit stumped here. We have a product that we are testing at 65C and it seems that the bluetooth connection keeps dropping at this temperature (Connection timeouts). We are running from a 32K LSE and 32M HSE crystals. All our parts are confirmed to be good to 80C. There seems to be a host of other various issues that pop up at this temperature. Ive tried setting the LSE drive to HIGH and increasing the flash latency, but it does not seem to impact the behavior. Any ideas?
..
I use STM32WL RTC Alarm as low power mode timer for achieve ms level accrancy and any duration sleep. System will convert sleep time to Alarm time before enter low power mode. I have tested different sleep time, verified convertion result is correct but system will always wakeup by Alarm advance 1 second than Alarm time. below is my RTC init and Alarm Setting Code:```cvoid MX_RTC_Init(void){ /* USER CODE BEGIN RTC_Init 0 */ /* USER CODE END RTC_Init 0 */ RTC_TimeTypeDef sTime = {0}; RTC_DateTypeDef sDate = {0}; RTC_AlarmTypeDef sAlarm = {0}; /* USER CODE BEGIN RTC_Init 1 */ /* USER CODE END RTC_Init 1 */ /** Initialize RTC Only */ hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = RTC_PREDIV_A; hrtc.Init.SynchPrediv = RTC_PREDIV_S; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE; hrtc.Init.OutPutPolarity = RTC_OU
Hi ST experts.I used the pingpong sample code to test RSSI and SNR. I set SF=12, BW=62.5Khz.I used SX1261 calculator tools to calculate, under this condition, its RSSI can reach -140dBm.But during my actual test, our RSSI reached -120dBm and the SNR was unable to receive data after it reached -20dBm. This is a module we designed ourselves. Is this normal behavior?
Hi everyone !I'm really new to STM32 and everything that goes around... I want to communicate with a SIMCOM A7670E with my NucleoWB55RG and UART1. I'm using PB6 and PB7 for USART1_TX and USART1_RX. But these pins (I kept the jumpers) are also connected to TX_STlink and RX_STlink right? That's why I can print on a tera term terminal what is happening on the UART right? (I followed a tutorial with no explenations that's why I'm not sure). My question is : is it a problem if I connect PB6 and PB7 on RX and TX of my 4G module? Maybe it will cause a conflict?Thanks a lot!
I am trying to test the SUB GHZ interface on STM32WL5xxU7. Is there any starter code without reliance on Nucleo boards that I could use to start with? Or are there steps how to do this with Low level drivers ?
I have done following configuration for RTC:static void MX_RTC_Init(void){/* USER CODE BEGIN RTC_Init 0 *//* USER CODE END RTC_Init 0 *//* USER CODE BEGIN RTC_Init 1 *//* USER CODE END RTC_Init 1 *//** Initialize RTC Only*/hrtc.Instance = RTC;hrtc.Init.HourFormat = RTC_HOURFORMAT_24;hrtc.Init.AsynchPrediv = CFG_RTC_ASYNCH_PRESCALER;hrtc.Init.SynchPrediv = CFG_RTC_SYNCH_PRESCALER;hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;if (HAL_RTC_Init(&hrtc) != HAL_OK){Error_Handler();}/* USER CODE BEGIN RTC_Init 2 *//* USER CODE END RTC_Init 2 */}With prescalers set as:#define CFG_RTC_ASYNCH_PRESCALER (0X7F)#define CFG_RTC_SYNCH_PRESCALER (0XFF) The system is clocked with 32 MHz HSE.I configured timer server to have periodic wakeups every 10 mins:HW_TS_Create(CFG_TIM_PROC_ID_ISR, &Wakeup_mgr_Id, hw_ts_Repeated, Set_Wakeup_Task);HW_TS_Start(Wakeup
Hello,Like "BLE_AT_Server" example, is there a similar example of "802.15.4_AT_Server" for 802.15.4 RF MAC Mode Transceiver for STM32WB5MMG modules?
Dear team!,I have a problem with STM32WL55JC1 board.I loaded the "LoRa End Node Dual Core "project and it works very well.Then I made a project from scratch, with Dual core checkbox checked.Before initialising any module, I built both projects and downloaded the exported elf files.Then I tried an example to test the IPCC but I found that the CM0 is no longer able to start from its default address.I've made a full chip erase using STProgrammer CUBE and loaded the "LoRa End Node Dual Core "project binaries to the board. But CM0Plus is not working. I've entered a debug session. I found that CM4 is working normally but CM0Plus after releasing it by CM4, it goes to 0x FF FF FF FE. I double checked the linker file for CM0Plus and it looks the same as the default example. I brought a brand new kit, loaded the "LoRa End Node Dual Core "project and it works fine. I checked the Flash Option Bytes from the working kit and compared with the died one and they were the same.I hav
Hi,I'm working with an ST50H based on STM32WLE5 series MCU. Here's the product: https://www.st.com/en/partner-products-and-services/acsip-st50h.html. I would like to be able to flash the device using pyOCD or OpenOCD. However, after installing the STM32WL series support for pyOCD, pyOCD ask me to select a target and I'm seeing these devices. I tried each of these resulting in a "critical No ACK received error".I would like to know the exact name of the STM32 used in ST50H. I asked Acsip for the exact name and they do not tell me more than STM32WLE5.Did you have examples or documentation about flashing an STM32WL series MCU with pyOCD?Thanks!Alexandre
Hello,I'm currently developing a Zephyr application and want to use the STM32WB55 chip. For evaluating I use the ST Nucleo WB55RG board. The device is configured as a Bluetooth peripheral using the Zephyr v3.6.0 host stack and the stm32wb5x_BLE_HCILayer_fw.bin firmware V1.18.0 for the controller.Issue:Once a central connects to the device, the following warning and error messages are logged: <wrn> bt_hci_core: opcode 0x2016 status 0x3a <err> bt_hci_core: Failed read remote features (-16) The opcode corresponds to the OCF defined in the Bluetooth Core Specification 5.3, Vol. 4, Part E, Chapter 7.8.21 (LE Read Remote Features command).The controller return status indicates "controller busy". Debugging the issue, I found that a delay of 500ms between connecting and requesting the remote features in most times prevents the error.Steps to reproduce:Build and flash the peripheral example from the Zephyr sources.Connect to the deviceError message is logged
HelloI've been recommended the product by the ARROW sales manager, but I'm not getting any documentation or technical help. I'm new to st product and ble.Below are the features I want.1. If you don't do anything for a certain period of time, you will be in sleep mode, and if you receive a wake-up message through wireless communication, you will wake up.2. The button allows you to turn on or off the low power mode.3. Can it operate on low power by default unlike item 2?4. How do I do broadcast communication, not pairing?What else should I refer to to to implement the above features?
Excuse me, how can we establish a Bluetooth connection between stm32wb55 as an observer and other broadcasting devices on CubeMX? The current CubeMX can only implement WB as a broadcaster to connect to the app, which is not the pattern required in my project. Please give me a good suggestion, thanks !
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.