Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
I am using Zigbee for wireless communication using Zigbee_OnOff_Router_NVM as a reference. The problem I am currently facing is that if I turn off the Router for a long time, it may take about 20 seconds for the data to reach the Coordinator the next time it is started. What can I do to reduce the time it takes to reconnect? Help me.
Hi ST Support Team,I am reaching out regarding an issue I have encountered while attempting to utilize USB CCID functionality on the STM32WB55 MCU. Recently, I integrated the CCID driver from the following link into my project.https://github.com/STMicroelectronics/stm32_mw_usb_device/tree/master/Class/CCIDFollowing the integration, I successfully configured the USB device, and my system(windows PC) can now detect the STM32WB MCU as a smart card reader.However, upon further testing, I encountered an unexpected behavior: when attempting to communicate with the smart card reader using a Python script, the STM32WB USB port is detected as a Virtual COM port rather than a smart card reader. As a result, I am unable to establish communication with the MCU via script.I am reaching out to kindly request your assistance in resolving this issue. Could you please provide guidance or solutions to ensure that the STM32WB MCU is correctly detected as a smart card reader and able to communicate w
Hello, I am developing a device using STM32WL chipset.I'm currently taking the FCC certification test, but it failed in R.S.E (Radio spurious emmision), so I've been reviewing it for 3 weeks.There was an FCC certification logo on the STM32WL Ev-kit, so I searched for the FCC ID and found a test report like the attached file.If you look at page 23, it says "Final measurement detector: CISPR Average". Is the AVG value measured by CISPR correct?The device we are developing is in a situation where Peak passes in the FCC R.S.E section, but fails in AVG.Since our device only had a difference between Peak and AVG of 3 to 4 dBuV/m, we asked the certification company to measure it using CISPR.However, I received a reply from the certification company that they only measure CISPR below 1GHz.Please help.thank you
Appreciate pointer to simpliest example for STM32CubeWL sequencer.Specially "Task registration and execution" and "Wait for an event and set event" to do the below sequence. I have AN5406 and reading.....read temperature sensor, transmit on STM32WL5JC Lora, sleep, wake up on end_of_tx, set timer to nnn seconds, sleep, wake up and repeat. TIA
Which ST Link programmer is best for STM32WL5JC (Lora MCU) for advanced debug facility (still reading, ??trace, monitor??)TIA
How to setup debug session with C breakpoint, stepping, variable read/write, etc. (and advanced facility like monitor, etc. I am still reading...)TIA
I use stm32wb5x_BLE_Stack_full_fw.bin v1.13.2 on STM32WB5MMG.The installation address is 0x080CF000.What happens if I write the stack to the wrong address (0x080C7000, the install address for v 1.13.0).In my board, it looks work fine. Is there any concern or limitation?
Hello, I'm STM F/W Beginner .Recently, I was tasked with a project to implement BLE with the Stm32wb MCU.As a result of referring to Example such as Heartrates or P2PServer Projects, I could successfully send Data to a mobile phone by Nucleo Board.However, I still can't receive and handle Data with my board.Is there any example I can refer to?
Hello all, I made custom PCB board with STM32WB5MMG in my project. I have confirmed that the SWD pins are working and Code is Debugging ok.I have also set up HSEM, IPCC, RCC, RTC, RF, STM32_WPAN required but I can't detect the Bluetooth.Iam using STM32CUBEMX V6.8.1 and STM32CUBEIDE V1.12.1Firmware package version is 1.16.0 (STM32Cube_FW_WB V1.16.0) .
Good morning,I am using an STM32 WL55JC1 starting from the end node example.I am unable to figure out in the code how to set how long or how many tries it makes before it stops trying to connect to the gateawy.Could you please point me to this information?Thank you very much,Roberto
i set fido related services and characteristics using cube mx for stm32wb55 development board why i am not getting any value in my coustum event handler.
Hi ,I'm trying to Perform OTA update using ST BLE ToolBox ,I have programmed my STM32WB5MMG with the OTA binary.The problem comes when starting the update process. With ST BLE Sensor there is no problem: the device is updated to the new version of the user app. However, when the operation is performed with the STM32 BLE ToolBox app (iOS), the image is sent (100%), but the OTA does not restart to install the new user app and the 100% message does not disappear from the mobile app.Andriod version of ST BLE ToolBox is working properely and the device is updated to the new version of the user app.So , ST BLE ToolBox (Android version) and ST BLE Sensor (IOS version) are working properely .ST BLE ToolBox (IOS version) has a problem that the image is sent (100%), but the OTA does not restart to install the new user app and the 100% message does not disappear from the mobile app.IOS Version 17.4.1ST BLE ToolBox IOS version 1.2.6Best regards and thanks for yo
@ST Community @STTwo-32 @Tinnagit @Tesla DeLorean 1) I have done few changes from "#define LORAWAN_DEFAULT_CLASS CLASS_A" to "#define LORAWAN_DEFAULT_CLASS CLASS_C" in the "lora_app.h" file and I also changed "#define DISABLE_LORAWAN_RX_WINDOW 0" to "#define DISABLE_LORAWAN_RX_WINDOW 1" in "lorawan_conf.h . Is there are more settings to do to operate this boards in Class C?2) Is there anyone who's working on class C with Wl55JC1/L072Z LRWAN1. I have went to community and they are not able to work on class C with Wl55jc1. After few settings and some has suggest to set up the LoRaWAN server to tell the device to switch to class C, and i'm able to understand how to setup server?If you have any information to operate these Board in Class C, do guide me.Looking for your guidance.Thank you
Hello.I have encountered an issue during the migration from STM32WB5MMG to STM32WB1MMC.When I generate the default code using CubeMX with STM32WB1MMC, no errors occur. However, when I try to transfer the code I was using with STM32WB5MMG to STM32WB1MMC, errors arise. Of course i have undergone the migration from STM32WB5MMG to STM32WB1MMC. Below, I'll outline my current situation. During compilation with IAR, I ran into an error. Upon checking the source size via the map file, it appears as follows: After examining the RAM size, it seems that the capacity of SRAM1 is less than 12K. I believe this shouldn't cause a compilation error.What actions can I take to address this issue?
Do I need to set the net impedances of differential pair from RFI_P and RFI_N to 50ohm?
Hi.I'm using stm32wb55 MCU.ADC is running in continuous mode with 6 channels using DMA for the results. I want to use analog watchdog interrupt on just 1 channel that is on rank 2.I have 2 problems, first the interrupts occured only for the channel in rank 1. I tried replacing the channel in rank 1 and the watchdog always considered only rank 1 channel. Second, I'm using 12 bits resolution and I checked RES bits are set to 00, but from what I tested it looks like the value triggers the watchdog is right shifted by 4 bits, for example if data received is 2116(0x844), low threshold needs to be set to more than 132(0x84) to trigger the interrupt.Does anyone had any of these problems or have any idea how to solve it?Any help will be appreciated.Thanks
1) Class A for Unicast.Class B synchronous transmission (thanks to beacon) for Unicast or Multicast.Class C for continuous transmission for Unicast or Multicast.According to this details will Class C will give little bit more data rate then Class B?2) I have done few changes from "#define LORAWAN_DEFAULT_CLASS CLASS_A" to "#define LORAWAN_DEFAULT_CLASS CLASS_C" in the "lora_app.h" file and I also changed "#define DISABLE_LORAWAN_RX_WINDOW 0" to "#define DISABLE_LORAWAN_RX_WINDOW 1" in "lorawan_conf.h . Is there are more settings to do to operate this boards in Class C?3) Is there anyone who's working on class C with Wl55JC1/L072Z LRWAN1. I have went to community and they are not able to work on class C with Wl55jc1. After few settings and some has suggest to set up the LoRaWAN server to tell the device to switch to class C, and i'm able to understand how to setup server?Thank you in advance.
Hello,I am developing a custom board with the STM32WB55RGV6 Chip and an on-board PCB antenna. The document is for a 2-layer PCB and I am needing to do a 4-layer PCB. I don't completely have the recommended stack-up, but altium shows its very close to 50Ohms. Will this work?
Hello developers,I am currently developing all in one AT Slave firmware for STM32WL, which can handle both lorawan and sigfox AT commands. I have tested both AT Slave example of Sigfox and LoRaWAN one by one and it's working as expected. When i open the .ioc file of this examples (AT Slave LoRaWAN and Sigfox) in CubeMX, i can see it doesn't allow to enable the Sigfox/LoRaWAN middleware in LoRaWAN/Sigfox example. So i would like to know how i can enable both the middleware in same firmware, so that my master device can leverage the use of both technologies (LoRaWAN & Sigfox ) in the same chipset.
I've prepared a small device firmware for a STM32WB35CEU7Ait's only providing battery service and debug infos on serialI've tested it on a P-NUCLEO-WB55 loaded with stm32wb5x_BLE_Stack_full_fw.bin1.19.02 stack loaded @0x080CE000 and it works wonderfully even if .ioc file is based on STM32WB35CEU7A and not on WB55on debug serial all startup is complete :[app_entry.c][APPE_SysUserEvtRx][362] Wireless Firmware version 1.19.0[app_entry.c][APPE_SysUserEvtRx][363] Wireless Firmware build 2[app_entry.c][APPE_SysUserEvtRx][364] FUS version 1.2.0[app_entry.c][APPE_SysUserEvtRx][366] >>== SHCI_SUB_EVT_CODE_READY[app_entry.c][APPE_SysEvtReadyProcessing][452] >>== WIRELESS_FW_RUNNING[app_entry.c][APPE_SysEvtReadyProcessing][476] >>== DBGMCU_GetRevisionID= 2003[app_entry.c][APPE_SysEvtReadyProcessing][481] >>== DBGMCU_GetDeviceID= 495[app_ble.c][APP_BLE_Init][333] Success: SHCI_C2_BLE_Init command[app_ble.c][Ble_Hci_Gap_Gatt_Init][715] ==>> Start Ble_Hci_Gap_Gatt_
Hi,I am writing a client/server application for STM32WB55. Server behavior is ok. On client side, I connect to a peripheral and try to send 32 bytes packets every 100 ms on peripheral's RX characteristic using aci_gatt_write_without_response function. MTU is set to 156. Nevertheless most of the time the function return with error code 0x64 (insufficient resource). The application is connected to 1 peripheral only, no advertising. I didn't find any helpful information.Any idea? Any orientation for investigation?Thanks, Jacques
What is the correct way to configure PLL in clocks for the BLE_HEAR_RATE_FREE_RTOS example ? So that sleep is maintained?
Hi,For our embedded Zigbee wireless application, we want to use the ST Zigbee stack.Per design, we want to avoid the use of dynamic memory allication. Per default, the ST Zigbee stack internally seems to use malloc for memory allocation. The ST application note AN5500 describes a way to let the application provide its own preallocated memory using the function ZbMemConfig(). However, this functions seems not to exist. - Has anyone managed to use the Zigbee stack with pre-allocated memory and prevent the stack from using malloc?- Is there an example provided by ST? Thanks in advance!Lukas
Hello Developers,I am currently testing Sigfox AT slave example from STM32Cube_FW_WL_V1.3.0 on STM32WL nucleo board. I already have 5 set of ID,KEY,PAC values from sigfox build for testing purpose. But when i am running sgfox at slave example, i am uunable to set id and pac values usinthe AT command. So can anyone please tell how can i set ID, PAC info in STM32WL using AT Slave.
I want to connect my NUCLEO board via bluetooth to a RN42 bluetooth module. The RN42 recieves sensor data from an adruino and needs to send it wirelessly to my STM board. How can i go about connecting the two?
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.