TODAY | STM32 Summit 2026
Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.
Most recent activity
Hi,I've been trying to port the STM32H753 SBSFU project to the STM32H735G-DK.The bootloader fails in SFU_BOOT_Init due to failing SE_Init().This is the result of __IS_SFU_RESERVED() failing it's test: 0x08008A00 < 0x08008061 < 0x0801FFFF (SB_REGION_ROM_START < __get_LR() < SB_REGION_ROM_END).As you can see the LR register value is outside of the expected range.Does anyone have an idea why this could be the case?Thanks!
..
I would like to use the RNG of the H743ZI2. The provided example works, but on a new project I can't get it work, The CPU clock is configured to 400MHz just like in the example./* RNG Initialization */ if (HAL_RNG_DeInit(&hrng) != HAL_OK) { /* DeInitialization Error */ Error_Handler(); } /* Initialize the RNG peripheral */ if (HAL_RNG_Init(&hrng) != HAL_OK) { /* Initialization Error */ Error_Handler(); }uint32_t rnd_number; void main() { while (1) { status = HAL_RNG_GenerateRandomNumber(&hrng, &rnd_number); if (status != HAL_OK) { Error_Handler(); } } }
I want to apply Read Protection to the STM32L552CCT6 .If you execute HAL_FLASH_OB_Launch(); after setting Read Protection, reboot does not work.Read Protection is applied only when the power is physically rebooted.I want Read Protection to be applied as ST reboots after executing HAL_FLASH_OB_Launch();.Below is the code I used.----------------------------------------------------------------------------------------------------------------------------///* Unlock the Flash to enable the flash control register access *************/ HAL_FLASH_Unlock(); ///* Unlock the Options Bytes *************************************************/ HAL_FLASH_OB_Unlock();OptionsBytesStruct.RDPLevel = OB_RDP_LEVEL_1; OptionsBytesStruct.OptionType = OPTIONBYTE_RDP;if(HAL_FLASHEx_OBProgram(&OptionsBytesStruct) != HAL_OK) { /* Error occurred while options bytes programming. **********************/ } else { /* Generate System Reset to load the new o
Background:I am working on a project that uses the STM32H7B0 processor on a custom board. The firmware is loaded by ST SBSFU bootloader STM32CubeExpansion_SBSFU_V2.4.0. I have used 2_Images_ExtFlash example as a template, and our firmware is stored an 8 pin external flash. The external flash part we are using is 4MByte and by EON EN25QH32B.In addition to using SBSFU I am also using Keil MDK RTOS-v2. In one of the tasks, the STM32H7B0 is operating as an I2C slave device communicating with an I2C master controller that does not support clock stretching.If load and run firmware with the debugger and without bootloader everything works fine.Problem:The problem I am having is that when the firmware is loaded by SBSFU the I2C communications between the master controller and the STM32H7B0 does not realiable run at 400KHz but works fine with 100KHz. The STM32H7B0 processor is running at 240MHz.
HiWhat is the maximum Stack and Heap size of a STM32G474VE with the SBSFU Bootloader 2 Image version?In the icf file the settings are at 0x400 and 0x200 which is really low./*-Sizes-*/ define symbol __ICFEDIT_size_cstack__ = 0x400; define symbol __ICFEDIT_size_heap__ = 0x200;
Hi,In static HAL_StatusTypeDef CRYP_TDES_Process(CRYP_HandleTypeDef *hcryp, uint32_t Timeout){ uint32_t temp; /* Temporary CrypOutBuff */ uint16_t incount; /* Temporary CrypInCount Value */ uint16_t outcount; /* Temporary CrypOutCount Value */ /* Enable CRYP */ __HAL_CRYP_ENABLE(hcryp); /*Temporary CrypOutCount Value*/ outcount = hcryp->CrypOutCount; /*Start processing*/ while((hcryp->CrypInCount < (hcryp->Size/4U)) && (outcount < (hcryp->Size/4U))) { /* Temporary CrypInCount Value */ incount = hcryp->CrypInCount; /* Write plain data and get cipher data */ if(((hcryp->Instance->SR & CRYP_FLAG_IFNF ) != 0x0U) && (incount < (hcryp->Size/4U))) { /* Write the input block in the IN FIFO */ hcryp->Instance->DIN = *(uint32_t *)(hcryp->pCrypInBuf
The STM32H733VGH6 datasheet specifically mentions "Bootloader with security services support (SFI and SB-SFU)," while the STM32H723VGH6 does not. Does that mean that I can't use encrypted firmware on the STM32H723VGH6?I tried to do some research, but it is hard to decipher what are hardware versus firmware requirements.
HelloIn chapter 22.4.9 of RM0434 Rev6 is stated:Counter: a 32-bit big-endian integer that is incremented each time a blockprocessing is completed. The initial value of the counter must be set to 1.Why can be the initial value of the counter not be set to 0 (as far as I know it is possible in standard)? Is this a bug?Best regardsPaul
Hi All,I am using SBSFU to load my firmware which is running from external flash. The firmware works but seem to be experiencing speed issues on the I2C communications.In an attempt to solve this issue, I am would like to, at start-up copy the code that is placed at 0x90000000 to RAM and run but not sure how to do this.Regardsooni
Hi,I find the new chip STM32G0B1 from STM32CubeMX.And I want use this chip with SBSFU 2_Images.But I can not find the STM32G0B1 project from the X-CUBE-SBSFU v2.4.0.Is STM32G0B1 compatible with X-CUBE-SBSFU v2.4.0 ?How do I use STM32G0B1 with SBSFU 2_Images?Could you help me?Thank you.
During the workshop itself, I had some problems with some of the example files not having correct access rights to allow the workshop changes to be made.We worked around that during the workshop.Now I have just come back to the STM32Cube IDE; it started up with the last 2 workshop projects still open (as would be expected). But when I tried to close these projects, I got the following errors: It seems that the whole workshop folder tree was installed with only 'Read' access for Users: Giving 'Full Control' stopped the problems:Hopefully this will be of help if anyone else is having the same problem.But the question remains: why did the stuff get installed with these inappropriate settings?This is on a standalone Win10-Pro.
HelloThe crypto HAL driver ( function CRYP_SetKey in file stm32wbxx_hal_cryp.c ) of the STM32WB accesses the key as "array of uint32_t" (lines 2919 etc): hcryp->Instance->KEYR3 = *(uint32_t *)(hcryp->Init.pKey); hcryp->Instance->KEYR2 = *(uint32_t *)(hcryp->Init.pKey + 1U); hcryp->Instance->KEYR1 = *(uint32_t *)(hcryp->Init.pKey + 2U); hcryp->Instance->KEYR0 = *(uint32_t *)(hcryp->Init.pKey + 3U);thus the key and nonce must be swapped by customer software. This is not compatible with openssl generated key nor STM32 crypto library usage on other STM32 mcus (could be declared as bug). The "CRYP_DATATYPE_8B" byte swapping only applies to cipher and plain buffer.Better would be: hcryp->Instance->KEYR3 = __REV( *(uint32_t *)(hcryp->Init.pKey) );
I converted code from one of the example from sbsfu for stwinkt1 board.This converted example is for 2 image and working fine on serial port.As far as i get for 2 image example configuration will like,SBSFU s;ot+1 active slot + 1 DWL slot + swap area.When i download new firmware,Encrypted image is downloaded in DWL slot and on next reset it decrypted and swapped with active slot image so after installing new firmware result will be like,before swapping,Active slot-image(decrypted) 1.0.0DWL slot -image(encrypted) 1.0.1after swapping,Active slot-image(decrypted) 1.0.1DWL slot -image(decrypted) 1.0.0is this understanding correct?can i roll back to older version once new one is installed(like from 1.0.1 to 1.0.0)? can i choose any slot as active firmware image?Second question is ,In stm32 based project is partial firmware update is possible. I mean if we consider stm32 based project than most of the time once controller is finalized than hal layer and lower
I have some code that removes a "secure area" on STM32H75x by so called "regression" from RDP level 1 to level 0, which causes full erase.(Actually this code is based on example very kindly provided by ST support) void EraseAll(void) { uint32_t flashUserOpt; printf("Launching erase all process. Requires RDPL1 already set\n"); __HAL_FLASH_CLEAR_FLAG_BANK1(FLASH_FLAG_ALL_ERRORS_BANK1); HAL_FLASH_OB_Unlock(); FLASH->OPTSR_PRG = 0x13BEAAF0; /* RDP level 0 */ FLASH->PRAR_PRG1 = 0x80000FFF; /* No PCROP */ FLASH->SCAR_PRG1 = 0x80000FFF; /* No secure area */ FLASH->WPSN_PRG1 = 0x000000FF; /* No WRP */ OBLaunchWithCheck(); HAL_FLASH_OB_Lock(); } void OBLaunchWithCheck(void) { HAL_StatusTypeDef error; if ((error=HAL_FLASH_OB_Launch()) != HAL_OK) { printf("HAL_FLASH_OB_Launch failed. HAL_ERROR: %d Error code : %8.8x ...\r\n", error, pFlash.ErrorCode); printf("Flash->SR1: 0x%8.8x\r\n", FLASH->SR1); } }The erase usually (*) works, but after a power
I am trying to create a mechanism of verification where I sign a file on the PC save it to a disk on a key device and then verify it by the MCU after saving it to internal flash.The PC is doing the signing process and the MCU should only do the verification process.On the PC side I sign the image with the pkcs1_15.sign() function from the pycryptodome library. On the MCU is the public key is saved as modulus and exponent in the following format:unsigned char RSAKeyModulus[] = { // Offset 0x00000000 to 0x00000158 0x30, 0x81, 0x9F, 0x30, 0x0D, 0x06, 0x09, 0x2A, 0x86, 0x48, 0x86, 0xF7, 0x0D, 0x01, 0x01, 0x01, 0x05, 0x00, 0x03, 0x81, 0x8D, 0x00, 0x30, 0x81, 0x89, 0x02, 0x81, 0x81, 0x00, 0xD6, 0x35, 0x43, 0x7C, 0xC9, 0x22, 0x18, 0x16, 0xF5, 0xE9, 0xB9, 0x29, 0x51, 0x80, 0x3F, 0x1D, 0xC0, 0x94, 0xCF, 0x91, 0x0D, 0x38, 0x6E, 0x83, 0x51, 0x22, 0x52, 0xC0, 0x8D, 0xBD, 0xD3, 0x21, 0x68, 0x52, 0x50, 0x39, 0x79, 0xC6, 0x6D, 0x19, 0x9B, 0xFE, 0x61, 0xDF, 0xFA, 0xB3, 0x7E, 0xE1, 0x71, 0xA9,
I'm trying to port the SBSFU to STM32H735. I started from the project for the NUCLEO-H753ZI.I get errors in sfu_fwimg_core.c on FW_INFO_TOT_LEN but where is this defined?A simple grep -r turns up nothing.Thanks!
We are evaluating if we can use the STM32WLE5, to interface to existing devices .A critical factor is the expected endianness of the data. I have seen no reference in the docs if this can be set, so I have provided an example message and would like to know if this can correctly interpreted by the STM.The following sequence defines the values of bits 'in the air' as recorded on an oscilloscope. The most left bit is the first bit transmitted.10101010 10101010 10101010 10101010 These are the 4 preamble bytes. Byte value is 0x55 with LSBof each byte transmitted first00110011 01010101 00110011 01010101 These are the 4 Sync bytes 0xCC 0xAA 0xCC 0xAA in sequenceof transmission, with LSB of each byte transmitted first01000000 10000000 00000000 The first byte is the Variable Length : Value is 0x02, LSBtransmitted first. The data bytes are 0x01, 0x00, LSBtransmitted first01110100 11110110 The CRC is computed on the 3 bytes above. The CRC value is 0x6F2EThe LSByte of the CRC is sent first, LSB of
Hello,one question (or feature request):I try to use the STM32 crypto library (v1.3.1 software implementation) on STM32WB. I activated the RNG and CRC but the calculated results (encryption/decryption, cmac) are not ok. Are there other things to do?Is there an hardware implementation using directly using the AES/PKA peripherals of STM32WB? Or will be there a new version of the library package?As I understood, there are only examples to use directly HAL drivers. It would be great, if the crypto library (executing on AES/PKA hardware) would be optimized using LL drivers...Is there a user manual "how to use crypto lib on STM32WB"?Best regardsPaul
Hello,I want to calculate the CRC (32 bit) of image at post build and insert it in a known location in the image.In order to do it I should perform the following steps:a) Definition of placeholder in linker script fileb) Post build steps: b.1) Calculation of image CRC (32 bit) b.2) Insert it into the placeholderThe reason of 32 bit is to use the STM32 HW CRC calculation for checking the CRC.The post build steps can be performed by IELFTOOL.Can anyone help?Yacob Hassidim.
HiI want to use the Cryptographic peripheral on the above nucleo board, in the following way.Serial message from embedded board-->H745 crypto engine-->wireless transmission-->Decrypt packet on remote x86 laptopAnd the reverse direction tooSo clearly i will need a way to duplicate the AES/DES flavor implemented on the H745 on an X86.Is there a reference C code that would give the same output on x86 (assuming the symmetric keys are exchanged during a binding process)
Hi!I'm triying to set the CRC-16-IBM: X16+X15+X2+1, but CUBEMx does not allow it. In fact, I cannot introduce any polynomial.Is it a CUBE issue? How can I introduce the CRC-16 IBM polynomial ?Thank you
HelloIn STM32 Crypto Library, there are function "AES_CMAC_Encrypt_Init", "AES_CMAC_Encrypt_Append" and "AES_CMAC_Encrypt_Finish" to calculate the authentication code of a plain text.How can this be done on STM32WB using the CRYP peripheral (HAL driver) ?Best regardsPaul
We are evaluating if we can use the STM32 to interface to existing devices. The critical fator is the expected endianness of the data. I have seen no reference in the docs if this can be set, so I have provided an example message and would like to know if this can correctly interpreted by the STM.The following sequence defines the values of bits 'in the air' as recorded on an oscilloscope. The most left bit is the first bit transmitted.10101010 10101010 10101010 10101010 These are the 4 preamble bytes. Byte value is 0x55 with LSBof each byte transmitted first00110011 01010101 00110011 01010101 These are the 4 Sync bytes 0xCC 0xAA 0xCC 0xAA in sequenceof transmission, with LSB of each byte transmitted first01000000 10000000 00000000 The first byte is the Variable Length : Value is 0x02, LSBtransmitted first. The data bytes are 0x01, 0x00, LSBtransmitted first01110100 11110110 The CRC is computed on the 3 bytes above. The CRC value is 0x6F2EThe LSByte of the CRC is sent first, LSB of byt
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.